NI LabVIEW Community
  • Products & Partners
  • Dev Tools
  • NI LabVIEW Community
  • More
  • Cancel
NI LabVIEW Community
NI Forum goal: learn OO LabVIEW
  • Blog
  • LabVIEW Challenge Blogs
  • Forum
  • Documents
  • Quiz
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NI LabVIEW Community to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 134 subscribers
  • Views 2007 views
  • Users 0 members are here
  • RoadTest
  • mcc172
  • labview
Related

goal: learn OO LabVIEW

Jan Cumps
Jan Cumps over 3 years ago

I made a LabVIEW driver for a DAQ. The sampling mechanism is always the same:

  • one flow starts the DAQ, tells it to sample data, retrieves that data and queues it. In a loop. This is called the Producer Loop in LabVIEW lingo
  • a second flow reads data from that queue and shows / stores / processes it. They call that the consumer loop

image

The top loop - the producer - is always the same. This is the flow that tells the DQ to send samples, then retrieves the sampling data and enqueues it. I know how to turn that into an object (and have done that - will be released later).

I want to make the Consumer Loop OO

I want to focus on the bottom loop: the consumer. That one is application dependent. What do I do with that data?
In my examples, I have implemented several incarnations of that pattern:

  • a simple flow that retrieves one channel and shows its data on a virtual scope screen
  • a flow that samples two channels
  • a flow that collects x samples and does a FFT
  • a flow that collects x samples and calculates acceleration data from it
  • a combination of those.

I'd like to use LabVIEW's OO mechanisms to provide a simple implementation. And allow the user to inherit from that and do what they want. If you are a LabVIEW OO expert, please chime in.

I am able to do Simple object wrapping

I wrapped the upper loop into a block. That's easy because it doesn't need inheritance or polymorphism. This is the original flow:

image

I wrapped that Producer Loop into a block, and added it to the driver lib. Here's what a flow looks like when using that block:

image

The whole Producer Loop functionality above is contained in that block. It makes the flow less busy, and takes care that that same logic can easily be reused - and kept consistent - in every process.
It's reuse, but not yet full OO. Here is the logic behind that block:

image

The keen eye will see that it is the same as the producer loop in the first and second  image, with all inputs and outputs turned into connectors. You can see it in use in the 3rd image.
I need to fix one side effect of wrapping this object: It breaks the Stop button functionality, because its status is now retrieved when entering the block. Not at each iteration.

  • Sign in to reply
  • Cancel

Top Replies

  • Andrew J
    Andrew J over 3 years ago +3
    I did something very similar a couple of years back when I believed NI’s marketing about NXG being the future. A “tester” just needs to create a couple of concrete subclasses to plug in to get it all to…
  • Jan Cumps
    Jan Cumps over 3 years ago in reply to Andrew J +2
    Andrew J said: when I believed NI’s marketing about NXG being the future That was rough for a lot of people. NI really pushed users to migrate their code base. Then canceled all. They must have had very…
Parents
  • DAB
    0 DAB over 3 years ago

    Interesting project Jan.

    Do you have an end application or are you just learning.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • DAB
    0 DAB over 3 years ago

    Interesting project Jan.

    Do you have an end application or are you just learning.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Jan Cumps
    0 Jan Cumps over 3 years ago in reply to DAB

    I want to learn, but I have a use case too: the LabVIEW driver for the Vibration DAQ HAT that I road tested.

    At this moment, I have 4 example flows for it. Everything in these flows is the same, except what I do with the acquired data.

    I'd like to make a very simple block, that just eats the data from the LabVIEW queue and does nothing with it, and allow the users to derive from that block and do interesting things (show the waveform on the screen, write the data to a spreadsheet, do FFT, calculate RMS, …)

    Here are a few of those examples, where the base functionality is always the same: dequeue data then do smart things with it. (click to enlarge)

    image image  image

    If I could make an abstract / simple class that handles that dequeuing, and the end user would only have to deal with what they want to do with that data - that's my dream.