NI LabVIEW Community
  • Products & Partners
  • Dev Tools
  • NI LabVIEW Community
  • More
  • Cancel
NI LabVIEW Community
NI Forum Resistance Value is Floting in Digital Potentiometer AD5293
  • Blog
  • LabVIEW Challenge Blogs
  • Forum
  • Documents
  • Quiz
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join NI LabVIEW Community to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 134 subscribers
  • Views 1157 views
  • Users 0 members are here
  • resistance
  • resistance measurement
  • Digital Potentiometer
  • ad5293
  • digipot
  • ad5292
Related

Resistance Value is Floting in Digital Potentiometer AD5293

umair1998
umair1998 over 3 years ago

Hi Everyone,

I am using digital potentiometer AD5293 and doing i2c communication using Labview. 

The only issue I have is that, when I measure the value at wiper and B terminal, for some reason it looks like it is floating at higher resistance, like if I apply 10kohm, it's 9.7kohm, no problem at this point until 40kOhm to 50kohm, I know the tolerances of resistors. 

But when I apply 60, 70 or 80kohm or in between them, then by using DMM I check the value it measures like

( 63, 63, 63. 8 etc, or 68, 67, 65 63 etc.)  if I applied 65kohm. For all higher values its show like this. Does it optimal or some fault in my circuit or digital potentiometer? I changed the potentiometers, and PCB but it's behavior is the same. 

Please help

  • Sign in to reply
  • Cancel

Top Replies

  • baldengineer
    baldengineer over 3 years ago +4
    A couple of things to note from the datasheet . 1. There is a "resistor performance mode" and a "normal' mode. Page 19 describes R-Perf Mode. 2. In normal mode, the tolerance for the 100K version is…
Parents
  • dougw
    0 dougw over 3 years ago

    Which version of that chip are you using? I think it that part number covers 20K, 50K and 100K versions.

    Is there anything else in the circuit that might affect the resistance?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dougw
    0 dougw over 3 years ago

    Which version of that chip are you using? I think it that part number covers 20K, 50K and 100K versions.

    Is there anything else in the circuit that might affect the resistance?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • umair1998
    0 umair1998 over 3 years ago in reply to dougw

    Thanks @dougw for your reply, I am using the 100K version. I am using these resistors for an analog PI Controller.  Do you know why this is happening?