PSOC 1, PSOC 3, PSOC 5, MINIPROG3, debugger / programmer kit

Manufactured By:Cypress
PSOC 1, PSOC 3, PSOC 5, MINIPROG3, debugger / programmer kit
Part Number:CY8CKIT-002

Cypress Semiconductor has completed a hardware update to the Miniprog3 to address hardware issues seen with programming, ESD, and power management. The Miniprog3 revision, either *A or *B, is indicated using sticker on the back of the programmer. The following are a list of updates made to the Miniprog3 *B programmer.

Updated Hardware to Improve Power Cycle Programming:

The Miniprog3 hardware has been updated to better improve power cycle programming for all PSoC devices. It was discovered that the Miniprog3 *A programmer revision did not correctly implement the power cycle programming methodology. Due to this issue the Miniprog3 *A programmer could not correctly support power cycle programming for PSoC 3, PSoC 4 and PSoC 5LP  devices. This specifically impacts customers who do not route out the XRES line to the programming connector or disable the optional XRES line on certain devices. The *B revision of the Miniprog3 will support power cycle programming for all PSoC 3, PSoC 4 and PSoC 5LP devices.

Over-current and Non-Polarized Connection Updates:

There are known electrical risks to the Miniprog3 *A revision that have been addressed with the *B update. To address the electrical issues the Miniprog3 *B programmer has added ESD over-current protection to the USB lines and has added electrical protection to the 5 and 10-pin connectors in case of a reverse polarity condition.

Improved Voltage Detection Capabilities:

The Miniprog3 *B programmer has been updated to improve the voltage detection capabilities. The Miniprog3 will measure the target voltage within an accuracy of 20 mV for a range of 1.8V – 5.0V.

Supported Software:

The Miniprog3 *B programmer is supported on the latest release of PSoC Programmer. To download the latest release, please navigate to the PSoC Programmer web page:

Features

  • PSoC® MiniProg3 is an all-in-one programmer for PSoC 1, PSoC 3, PSoC 4, and PSoC 5LP
    architectures
  • A debug tool for PSoC 3, PSoC 4, and PSoC 5LP architectures
  • A USB-I2C Bridge for debugging I2C serial connections and communicating with PSoC devices
  • The MiniProg3 programmer/debugger provides the flexibility to work with different programming and
    debugging interfaces, such as JTAG, SWD, ISSP, and I2C.
  • MiniProg3 supports the following debugging protocols for 8-bit and 32-bit PSoC devices:
    • SWD (PSoC 3, PSoC 4, PSoC 5LP)
    • JTAG (PSoC 3, PSoC 5LP)
    • I2C (limited PSoC 1 devices)
  • The MiniProg3 debugger is supported by the software tools PSoC Creator and PSoC Designer.

Ships With

  • MiniProg3 programmer/debugger
  • 10-pin ribbon cable
  • USB cable
  • Software CD
  • Quick start guide

Required Tools

Accessory Tools

Documents

User Manual/Guide

Downloads