Atmel Xplained Boards
  • Products & Partners
  • Dev Tools
  • Atmel Xplained Boards
  • More
  • Cancel
Atmel Xplained Boards
Forum 5V output on Arduino pins of SAMA5D3 Xplained?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Atmel Xplained Boards to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 4 subscribers
  • Views 792 views
  • Users 0 members are here
  • sama5d3_xplained
Related

5V output on Arduino pins of SAMA5D3 Xplained?

taichichuan
taichichuan over 12 years ago

Greetings!

 

  When I put a meter across any of the 5V output pins on the Arduino connectors, I don't see any voltage.  Do I have to power the board from the external power jack (J2)?  If I power from J2, it looks like I need to short R3 & R177.  Does that mean I need to remove resistors from the micro USB someplace?  I don't want to feed power back down my USB cable if I can avoid it.

 

TIA,

 

Mike

  • Sign in to reply
  • Cancel
  • taichichuan
    0 taichichuan over 12 years ago

    OK, since this forum seems dead and I want to help those who follow...  The 5V external connector (J2) has 2 sets of pads associated with it.  One is R177 the other is R176.  If you short (bridge, jumper, etc) R177, then the external 5V connector will be able to power the board.  There appears to be no conflict with the USB micro connector.  If you want to supply 5V on any of the Arduino pins, you then need to short R176.  Then the 5V will come out on the appropriate Arduino pins.  But, beware, the SAMA5D3 Xplained is a 3.3v card.  Don't put any 5V shields on the unit or you'll toast the CPU.  I just needed 5V for an external circuit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer