Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Blog Einride introduces futuristic self-driving trucks as part of new delivery service
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 17 Aug 2017 9:35 PM Date Created
  • Views 1768 views
  • Likes 3 likes
  • Comments 7 comments
  • research
  • transportation
  • autonomous
  • cabeatwell
  • trucking
  • Self-driving
  • innovation
Related
Recommended

Einride introduces futuristic self-driving trucks as part of new delivery service

Catwell
Catwell
17 Aug 2017

image

Swedish company Einride is looking to employ of fleet of 200 T-Pods by 2020 for a new autonomous delivery service. The T-Pod looks like something out of a sci-fi film (Photo via Einride)

 

We all heard the stories about self-driving cars and their unfortunate accidents, but ever think you’d see a self-driving delivery truck on the road? What kind of accidents do you imagine? One Swedish company is aiming to make this a reality. Einride recently showed off their prototype of T-Pod, an autonomous electric truck. Looking like a cross between a hilariously huge iPad and a kitchen appliance, the vehicle can move 15 standard pallets and can travel 124 miles on one charge. And it can hold a total weight of 20 tons when full. The truck doesn’t have cab space or windows, which explains its odd futuristic design.

 

For navigation, the truck employs a hybrid driverless system. T-Pod can steer itself while on the highway, but while on main roads a human will operate the vehicle remotely. There will also be people on hand to control several trucks at once when they’re on the highway if such a situation arizes.

Right now, T-Pod is still in its early prototype stage, but Einride is working on having the first truck completed by the fall. The company has bigger goals for the future. It wants to have a fleet of 200 T-Pods traveling between Gothenburg and Helsingborg. So far, Einride claims to have filled 60 percent of the 200 T-Pods they plan to build. Along with this, they’re also working on charging stations to power the trucks.

 

Einride isn’t the only company looking into autonomous delivery trucks. Waymo, Uber, and Daimler are also looking into similar technology. Volvo, also from Sweden, has been investing in self-driving technology for its own trucks. Last month, the company revealed their self-steering trucks that help out sugarcane framers improve their crop yield. While this vehicle isn’t totally autonomous, there’s still a driver inside, it drives alongside the harvester to deliver the crops off-site with minimal damage to the crop itself. Volvo ran similar tests in the mining industry and for garbage collection.

 

Even though these trucks sound cool, they should still be approached with some apprehension. Do we really want self-driving trucks delivering loads of cargo? What if something goes wrong? Hopefully, these companies are taking this into consideration. But chances are we won’t see anything like this in the States. We’re already getting a lot of push back just getting delivery bots on the sidewalk, so the idea of self-driving trucks on our highways probably won’t make it either.

 

I didn’t mention it in the review, but the movie “Logan” featured self-driving trucks that didn’t care one bit about pedestrians on the road. Perhaps an early prediction?

 

Either way, this is great inspiration for the IoT on Wheel Design Challenge.

 

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • the-dubster
    the-dubster over 9 years ago in reply to mcb1 +1
    mcb1 wrote: I have no doubt that driverless vehicles have a place, but I feel that these ideas are the hot air expelled by PR people when they've had a little too much cafine without an Engineer sitting…
  • mcb1
    mcb1 over 9 years ago in reply to the-dubster +1
    I have to print that out for work. Cheers Mark
  • mcb1
    mcb1 over 9 years ago in reply to the-dubster +1
    We had a large collection and strangely they seemed to be written about several of our middle management. We stopped because we ran out of room, and then they all went one day.
  • the-dubster
    the-dubster over 9 years ago in reply to mcb1

    mcb1 wrote:

     

    I have no doubt that driverless vehicles have a place, but I feel that these ideas are the hot air expelled by PR people when they've had a little too much cafine without an Engineer sitting in the corner bringing them back to reality.

     

     

    Mark

     

     

    I refer you to this! I might not 'dig' Mr Adams politics but I LOVE Dilbert comic strips!

     

    Dilbert Comic Strip on 2003-05-30 | Dilbert by Scott Adams

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago

    Cabe

    Thanks for bringing these to our attention. They do provide some interesting observations and provoke discussion.

     

     

    From my observations, the critical systems required to keep others safe are always written with the best intent, but it's that one thing that wasn't considered that usually makes it fail.

    It's only Tesla v truck you have to worry about, and since they are both electic they might communicate better ... image

     

    Driven vehicles do have accidents and some are driver error, or avoidable, but when the car in the opposite lane appears in yours, driver or not there will be a meeting.

     

    In those situations a driver may make choices, but what choices will an automated system make.?

    This is exactly that and well worth a go, I don't agree with some of the assumptions made (it's like judging a book by it's cover), but it was an eye-opener.

    Moral Machine

     

     

    Lets assume a sensor fails that the system deems is critical.

    Does the truck just stop where it is.?

    In a driven vehicle the driver might decide it is not the safest place to stop and instead continue 100m to clear the roadway or bend so that other road users are kept safe and not inconvienced.

     

     

     

    Here in NZ the poor truckies are not well paid, so the wages part of the freight bill is a very small percentage of total cost.

    I'm sure that economies in other areas might make more sense.

     

     

    I did a quick check and Gothenburg to Helsinborg is 217km or 134 miles.

    image

    So with a range of 124 miles it's going to be short.

    Also the 20 tonnes is a waste, since even here we're allowed 53 tonnes all up (on specified routes), but even 44 tonnes is more than 15 pallets.

     

     

    I have no doubt that driverless vehicles have a place, but I feel that these ideas are the hot air expelled by PR people when they've had a little too much cafine without an Engineer sitting in the corner bringing them back to reality.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<