Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Blog Nine bucks can net you a CHIP from Next Level Co that can fit in your pocket
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 5 Jun 2015 5:47 PM Date Created
  • Views 3047 views
  • Likes 2 likes
  • Comments 27 comments
  • chip
  • sbc
  • cheap
  • raspberry_pi
  • cabeatwell
  • gameboy
  • beagle_bone_black
  • innovation
Related
Recommended

Nine bucks can net you a CHIP from Next Level Co that can fit in your pocket

Catwell
Catwell
5 Jun 2015

image

Next Thing Co’s CHIP is a pocket-sized powerhouse that lets you code, play games and everything else a basic PC can do (via the CHIP kickstarter)

 

Small pocket-sized PCs can be found everywhere. Most come in the form of maker tools such as the Raspberry Pi, BeagleBoard or the Arduino (among loads of others), however these types of boards are typically used in DIY projects rather than used as stand-alone computer. Of course, there are other tiny computers that are used like a typical desktop (surfing the web, editing, Photoshop, etc.) including Intel’s NUC, ASUS’s Chromebox and Zotac’s Zbox Pico. The problem with those ultra-small PCs is the cost, which range anywhere from $100 and up- several times over what the Raspberry Pi costs.

 

Thankfully, high prices are not a factor with Next Thing Co’s CHIP- the world’s first $9 computer. The company recently launched a Kickstarter campaign to fund their insanely affordable PC and have surpassed their target goal of $50,000 by over 1.2-million with several weeks left to go. So what does nine-bucks net you? An Allwinner R8 processor (running @ 1GHz), 512Mb of RAM and 4Gb of storage. Strangely, there is no Allwinner R8 processor, rather Next Thing Co modified an Allwinner A13 SoC with integrated Flash and RAM, which helps keep the cost of the board down.

 

The board may be small (about the size of a credit card), however it isn’t lacking in the features department, which includes onboard Wi-Fi, Bluetooth 4.0, USB/micro-USB ports and an audio jack. It also has the capability to connect to any monitor from the very old VGA jack to the newer HDMI port through the use of add-on shields. CHIP also works with any USB-based keyboard and mouse without the need for drivers to be installed.

 

image

Pocket CHIP allows users to take their PC anywhere and is powered by a 3000 mAh battery.

 

Interestingly enough the board already has its first accessory add-on in the form of a Gameboy like housing known as Pocket CHIP. The board simply snaps into the housing, which features a 4.3" 470px x 272px screen with resistive touch, full QWERTY keyboard and a 3000 mAh battery. It also has a line of GPIO pins on the top edge for those who want to use the board in their projects. Next Thing Co preinstalled the mainline Linux as the board’s operating system along with several apps to get things running including the Chromium web browser, LibreOffice and the Scratch coding tool that helps users to learn how to program. Not bad for a PC that costs a mere $9, however the add-on shields will set you back an additional $10 to $15 depending on the board and the Pocket CHIP will set you back an additional $40- yep more than the PC itself.


Keep in mind.. $9 sounds great, but there is no community around this board yet. Raspberry Pi and Beaglebone have so much support, pre-written code troves, and countless projects. The CHIP is a while to go to hit this ease level.

 

C

See more news at:

http://twitter.com/Cabe_Atwell

  • Sign in to reply

Top Comments

  • johnbeetem
    johnbeetem over 11 years ago +3
    Actually, CHIP is a nice-looking board and nice form factor, very reminiscent of BeagleBone. The price is incredible and I agree with the Olimex analysis that this must be a promotional price, with losses…
  • fvan
    fvan over 11 years ago +2
    Don't forget the $20 shipping costs ... Also, will it continue to be sold at $9 after the KS campaign ?
  • clem57
    clem57 over 11 years ago +2
    fvan is write (right ). They tout low cost and add 50% or more for shipping? Bad marketing in my mind and so I canceled order. BTW you can get one and only one per account so shipping is per unit. What…
  • johnbeetem
    johnbeetem over 11 years ago

    Actually, CHIP is a nice-looking board and nice form factor, very reminiscent of  BeagleBone.  The price is incredible and I agree with the Olimex analysis that this must be a promotional price, with losses recovered through shipping costs.

     

    The main reason I didn't back CHIP is that boards won't be generally available until next year (May 2016 for systems with video) and by that time who knows what other boards will become available.  That, and I have enough boards to keep me busy for a long time.

     

    If CHIP does catch on, there's plenty of time to catch up.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to ntewinkel

    clem57 you should also consider - as you have started comparing to tablets - that these devices are with less claims than tablets, almost same price and seems too trying to put themselves to a sort of low-cost but elite market. This has no sense by any side you watch it: as a sort of PI / Arduino / BBB etc. competitor it has already lost (there is different history and different less experience beside) and as a sort of better tablet replacement less sense again, IMO. So, the only real point is that this is no more than a good advertised product. As less as you have to sell, as better should be your promotion. And this 9$ / pc is a real sensationalistic appeal image (until you don't investigare a bit in depth).

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 11 years ago in reply to clem57

    Clem Martins wrote:

     

    For around $70 dollars you get a quad, tablet (touch) kitkat wireless capable to 1080p and dual cameras to boot from http://www.amazon.com/Dragon-Touch-A93-Multi-touch-TabletExpress/dp/B00LVGIH7U

    John I cannot se the value for their pocket PC at $50???

    Clem

    I bought a dual core 7" tablet for $50 a few months ago. Except for io pins these little tablets seem to be the way to go instead of the SBCs.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 11 years ago in reply to mcb1

    Yes, I did back the Oak. Sounds like a nice product for a nice price. I won't be backing the so called $9 computer though, because of the steep shipping cost.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 11 years ago in reply to mcb1

    Yep, I've been backing every project Erik launched since the DigiSpark, and I will continue to do so for his future projects image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>