Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum I require BBView 7" setup help please.
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 57 subscribers
  • Views 1716 views
  • Users 0 members are here
Related

I require BBView 7" setup help please.

plawren1
plawren1 over 10 years ago

Can't get it to work..... Can't set it up.

Beagle Bone Black.

I don't want to use a new image.

I want a clear set of instructions on how to add/compile any drivers ontop of my current image.

Tried extending the SD memory to this:

Filesystem 1K-blocksUsed Available Use% Mounted on
rootfs       3360336 1863700   1322608  59% /
udev           10240   0 10240   0% /dev
tmpfs         101536 780100756   1% /run

/dev/mmcblk0p1   3360336 1863700   1322608  59% /

tmpfs         253836   0253836   0% /dev/shm
tmpfs         253836   0253836   0% /sys/fs/cgroup
tmpfs         102400   0102400   0% /run/user
tmpfs           5120   0  5120   0% /run/lock

/dev/mmcblk1p2   3610232 1843296   1580212  54% /media/rootfs

/dev/mmcblk1p1 98094   98092     2 100% /media/BEAGLEBONE

/dev/mmcblk0p2  10190136 1750108   7915740  19% /home/bbview

 

Ideally I want to set up BB View within /dev/mmcblk0p2.

 

Tried following instructions on numerous posts that simply don't work.

 

Thanks and regards

 

Paul.

  • Sign in to reply
  • Cancel
  • plawren1
    plawren1 over 10 years ago in reply to shabaz

    I'm happy with bone-debian-7.9-lxde-4gb-armhf-2015-11-12-4gb.img/bone-debian-7.9-lxde-4gb-armhf-2015-11-12-4gb.img in that I can update headers and extend memory. Lovely.

     

    I've updated the procedure to boot the BBView. Its definitely "talking" to it but now failing on f/w load

    [0.922633] bone-capemgr bone_capemgr.9: failed to load firmware 'BB-VIEW-LCD7-01-00A0.dtbo'

     

    But that's a new issue. Hope I'm heading in the right direction.....

    tea time. Thanks for nudging me.

    Paul.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • plawren1
    plawren1 over 10 years ago in reply to shabaz

    Hi Shabaz

     

    This is a standard released build.......

     

    root@beaglebone:/usr# apt-get -f install linux-headers-3.8.13-bone50

    Reading package lists... Done

    Building dependency tree      

    Reading state information... Done

    E: Unable to locate package linux-headers-3.8.13-bone50

    E: Couldn't find any package by regex 'linux-headers-3.8.13-bone50'

    root@beaglebone:/usr# uname -a

    Linux beaglebone 3.8.13-bone50 #1 SMP Tue May 13 13:24:52 UTC 2014 armv7l GNU/Linux

     

    I've almost given up on this thing.

     

    Cheers

     

    Paul.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<