Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Meet MinnowBoard MAX
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 14 replies
  • Subscribers 60 subscribers
  • Views 2342 views
  • Users 0 members are here
  • minnowboard
Related

Meet MinnowBoard MAX

e14 Contributor
e14 Contributor over 12 years ago

Meet MinnowBoard MAX | minnowboard.org

 

Maybe they've realised the original MinnowBoard was too little, too late, too expensive..  $99 for the base Max looks mildly more interesting, but it needs to be a lot faster and much less power hungry if it's to get close to the current Arm boards.

  • Sign in to reply
  • Cancel

Top Replies

  • johnbeetem
    johnbeetem over 12 years ago +1
    There's a good write-up of MinnowBoard Max at LinuxGizmos: http://linuxgizmos.com/intel-unveils-tiny-x86-minnowboard-max-open-sbc/ It sounds like MB Max has much better software support than the original…
  • prpplague
    prpplague over 12 years ago +1
    The original MinnowBoard was nothing more than a learning exercise for both Intel and Circuitco. Intel needed to learn a few things about open hardware, and circuitco needed to learn about x86 hardware…
  • prpplague
    prpplague over 12 years ago in reply to johnbeetem +1
    john, yes indeed the plains on the original minnow were swiss cheese..... you can download the gerbers for a view if you'd like, hehe the Max indeed supports more standard distributions such as ubuntu…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to prpplague

    David Anders wrote:

     

    Intel and circuitco have only been the x86 open hardware platform business for less that 18 months,

    You have a bit more experience at CircuitCo image

    Don't get me wrong, I think you're doing good things and I really do believe that Intel can do a lot in this area if they want to.

     

    So you've gone from $199 to $99 in not very long at all.. When do you think you'll get to $45 ? image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to e14 Contributor

    selsinork wrote:

     

    John Beetem wrote:

     

    There's a good write-up of MinnowBoard Max at LinuxGizmos: http://linuxgizmos.com/intel-unveils-tiny-x86-minnowboard-max-open-sbc/

     

    It sounds like MB Max has much better software support than the original Minnow.  It also has SATA: one dedicated connector and a second off the high-speed connector, which also provides PCIe.

    Actually I don't think that's a good write up at all. I have an original MinnowBoard. It has SATA, it has PCIe, it has uSD, it doesn't have NAND, it doesn't have micro-hdmi (does have normal hdmi though).

    Really, you'd have to think linuxgizmos have never even seen the original Minnow...

    My comment was misleading.  I didn't mean that LinuxGizmos' article said MB Max said SATA and PCIe were new.   I was in fact thinking about whether MB Max would be useful to me.  The fact that it has SATA puts it ahead of RasPi and Beagle as a PC replacement, and the fact that it has PCIe hooked up puts it ahead of RIoTboard.  I should have make this clear.  Sorry for the confusion.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to johnbeetem

    John Beetem wrote:

    My comment was misleading.  I didn't mean that LinuxGizmos' article said MB Max said SATA and PCIe were new.  

    Thing is, when you read the article that's more or less what they do say, along with the various other details they get wrong.

     

    The fact that it has SATA puts it ahead of RasPi and Beagle as a PC replacement, and the fact that it has PCIe hooked up puts it ahead of RIoTboard.

    For something with SATA, my choice is one of the Olimex A10/A20 boards. The LIME at 30euros is difficult to fault on anything apart from availability.

    The RIoT on the other hand has neither SATA or PCIe and I think can only be a BBB competitor when the BBB increases it's price.

     

    MinnowMax works out a bit more than RIoT while having both of the missing pieces, so there's certainly a place for it.

     

    Someone will no doubt be along shortly to ask if it runs windows too image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • rzr
    rzr over 11 years ago

    Give us a name of board supporting libre graphics drivers ?

     

    beside minnowmax which working amazingly nice

     

     

    https://www.youtube.com/watch?v=fP_L-ZJXOuA

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<