Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum I2C Slave?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 14 replies
  • Subscribers 60 subscribers
  • Views 4268 views
  • Users 0 members are here
Related

I2C Slave?

e14 Contributor
e14 Contributor over 11 years ago

Hi

I need to communicate with a I2C master with a BeagleBone black rev3 (Debian) as a slave.

I have search over the internet but not find anything. I'm new with BeagleBone.

I find a lot of example for master but not for the slave.

Can somebody please help me?

 

Regards Stefan

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to shabaz +1
    Thanks for the responses, Gary and shabaz! I had already done some surface level searches for Linux I2C drivers that also do slave-mode but didn't come up with anything conclusive. And I had almost forgot…
  • gdstew
    gdstew over 11 years ago in reply to clem57 +1
    "if you let the master "broadcast" a welcome message to see who responds with an address" The address used for this in the I2C specification is the general call address. I think your are correct that this…
  • e14 Contributor
    e14 Contributor over 11 years ago +1
    @ benett Linux 3.19 provides I2C slave mode kernel driver.
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    @benett

    Linux 3.19 provides I2C slave mode kernel driver. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • troyholt
    0 troyholt over 5 years ago in reply to e14 Contributor

    Well, I know this is a 5 year old post, but I was looking for a BBB i2c-slave driver and examples of how to use it.  Can anyone point me to such a thing or at least where to go look to find such information?  I have been running Debian 9.3 since it has LXQT and enough space to put gedit on a 8 GB uSD Card.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 5 years ago in reply to troyholt

    Hi Troy,

     

    I don't know the answer to your question, hopefully someone else can answer if they know, but just in case it helps, here is how I would go about working around such an issue.

    1. Determine if I2C slave is really the right thing - it's usually not for a processor. Usually the processor is the master. It's unusual enough to want to question the actual aim of this.

    2. If I2C slave really was essential, and I could not find a driver, then as a workaround I would write some code to bit-bang it, since I2C can run at speeds slow enough for this, and it doesn't need critical timing between bits/bytes for it to be successfully decoded by the remote device. Depending on the type of I/O that was available, it might need some external hardware (BJT or MOSFETs).

    To bit-bang it, the I2C specification could be used.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 5 years ago in reply to shabaz

    shabaz  wrote:

     

    ...

    To bit-bang it, the I2C specification could be used.

    The though thing with i2c is that it's way more complex to implement (bitbang) the slave state machine than a master.

    The master is not easy, but you can do that without too much hard timing and state criterea.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<