GIZMO 2
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • GIZMO 2
  • More
  • Cancel
GIZMO 2
Blog Hadron Vortex G2 - Light chaser mod
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join GIZMO 2 to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 12 May 2015 10:34 AM Date Created
  • Views 1726 views
  • Likes 5 likes
  • Comments 4 comments
  • RoadTest
  • vortex_g2
  • test_equipment
  • lucie_tozer
  • tektronix
  • gizmo2
  • tbs1202b-edu
  • test_and_measurement
Related
Recommended

Hadron Vortex G2 - Light chaser mod

e14 Contributor
e14 Contributor
12 May 2015

In it's initial build, the console is going to have a nightrider style light chaser on the top to act as a disk activity monitor. There are plenty of other animation styles that can be used but for the proof of concept, I stuck to just the light chaser that moves forwards and backwards.

 

The light monitor is being treat as an event driven animation. the first part of the video shows the animation being controlled independently by a setInterval function which in turn repeatedly calls another function that increments through the animation frames.

 

In the second part of the video, the animation being driven by the same signal that controls a single led on Gizmo2. This is achieved by making a connection from that led to an input pin on the Espruino. A setWatch function monitors the state of that pin and calls the function to increment the animation frames if it detects a change on the falling edge of the signal.

 

The system is using an Espruino that receives input from Gizmo2's disk activity led pin, handles the processing then communicates with an mcp23017 i/o port expander through an i2c bus to change the state of the led display.

 

Currently, the mcp23017 is connected to a bar graph led display for testing, but will be connected to a much larger display for the console build.

 

Throughout the video, I'm using a Tektronix TBS1202B oscilloscope to monitor the i2c bus in action (see how the i2c command sequence matches up to the led outputs). The oscilloscope is also used to capture the disk activity straight from the led output and investigate the signals.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 11 years ago +1
    I've yet to watch the entire video, but I looked through bits of it - very neat trick to get the animation from the Gizmo2 board like that!! It works very well!!
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to shabaz +1
    Thanks I'm thinking about capping the speed somehow, whether in software or with a hardware low pass filter I haven't decided yet... I also want to investigate tapping off usb signals through an opamp…
  • fustini
    fustini over 11 years ago +1
    Nifty! *all* computers should have LED bar graphs
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to fustini

    agreed! feedback on computers is boring!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fustini
    fustini over 11 years ago

    Nifty!

    *all* computers should have LED bar graphs image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to shabaz

    Thanks image I'm thinking about capping the speed somehow, whether in software or with a hardware low pass filter I haven't decided yet... I also want to investigate tapping off usb signals through an opamp buffer to do something similar, it might not work as elegantly but it's going to be fun trying!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago

    I've yet to watch the entire video, but I looked through bits of it - very neat trick to get the animation from the Gizmo2 board like that!!

    It works very well!!