GIZMO 2
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • GIZMO 2
  • More
  • Cancel
GIZMO 2
Forum setting up Ubuntu for embedded use (Gizmo2 as Media Player)
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join GIZMO 2 to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 12 subscribers
  • Views 1402 views
  • Users 0 members are here
Related

setting up Ubuntu for embedded use (Gizmo2 as Media Player)

e14 Contributor
e14 Contributor over 11 years ago

I've installed Ubuntu 14.04 on Gizmo 2 which is meant to sit inside a custom device case, run an OpenGL program (powered by the Panda3D library) and send video to a pico projector (based on this project: http://makezine.com/2011/09/19/pico-...rical-display/ )

 

For this I'll need to do few things:

 

1) Not start the desktop, but run the OpenGL program on startup which is the only program which should ever be running. How can I set up this?

 

2) Would be nice to disable the Ubuntu boot logo, or even better, control when the projector starts receiving HDMI signal. I'm sure the first thing is possible. But is the second possible to do? I'd like the projector to start displaying something after the OpenGL program has started. Otherwise I would probably need to add a mechanical shutter to block the projection for some time which isn't ideal...

 

3) Disable any kind of OS or included program notifications. The device needs Ubuntu just to start running the Panda3D library program, any interference might result in not working properly. This includes any "OS has restarted after some unexpected crash" or similar messages. How can all this be disabled?

 

I had originally asked this to ubuntu users but haven't gotten a response. Some people here seem to be using Ubuntu and is not unlikely they needed to do this too so I'm hoping some help from here.

  • Sign in to reply
  • Cancel

Top Replies

  • bobalexander
    bobalexander over 11 years ago +2 suggested
    1) I don't know if OpenGL can run outside of a desktop environment but you can get a very lightweight window manager such as FVWM2 to run X and just have it autolaunch OpenGL. 2) This should get you what…
  • bobalexander
    0 bobalexander over 11 years ago

    1)  I don't know if OpenGL can run outside of a desktop environment but you can get a very lightweight window manager such as FVWM2 to run X and just have it autolaunch OpenGL.

     

    2)  This should get you what you want with eliminating (setting the logo and background image to black):

         How To Customize The Ubuntu Boot Splash Screen & Logo [Linux] 

         I don't think you can turn off a display until a set point in Ubuntu. You might be able to hack something together Arduino-controlled HDMI switch : Install a transistor switch on the switcher PCB and replace the Arduino with an IO pin from the Gizmo2.

     

    3)  Disabling crash dumps can be done by editing /etc/default/apport and setting enabled=0 - if you are only running OpenGL and with a chopped down desktop environment you shouldn't see any other notifications...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to bobalexander

    Thank you.

     

    BTW, how is the OpenGL/DirectX performance of the device for you? Has anyone tested it? Minnowboard users have some stuff on Youtube.

    https://www.youtube.com/watch?v=j6RoF99T_TQ

    I currently have issues installing graphics driver and the overall performance is terrible.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to bobalexander

    Forgot, what about GRUB? It sometimes chooses automatically, sometimes makes you choose to start the OS or something else.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    This is what I did:

     

    8Zk8KOl.png

     

    flTIEXC.png

     

    Anything else that can be done?