GIZMO 2
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • GIZMO 2
  • More
  • Cancel
GIZMO 2
Forum GIZMO 2 no sound (Linux)
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join GIZMO 2 to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 13 subscribers
  • Views 2261 views
  • Users 0 members are here
Related

GIZMO 2 no sound (Linux)

e14 Contributor
e14 Contributor over 11 years ago

I get no sound on Linux Ubuntu 14.04 when plugging in a small speaker from the standard audio jack. But some noise is heard.

Also, when using a program using OpenAL for audio I get this error:

PrzxfRS.jpg

Thats all the info I can give. No error messages from the OS. Just no sound. Please tell me what else I can provide as info.

 

 

 

T

  • Sign in to reply
  • Cancel
Parents
  • balearicdynamics
    0 balearicdynamics over 11 years ago

    Welcome to the club!

     

    I am coming crazy by days on Gizmo2 to install OS and other stuff. Frankly I have not yet explored in depth the audio out but if you have a HDMI out put I suggest to try to see if the HDMI Audio out works. In this case maybe that it is a wrong output channel settings. The other thing I suggest if you haven not yet done it, is to install VLC as it gives many information on how the audio software is responding to the hardware of the board and you can make a lot of tests setting different parameters.

     

    In few time I will be back on a running Ubuntu version of the Ubuntu operating system and can make some test together with you.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to balearicdynamics

    I have the Gizmo connected to my TV via HDMI at the moment.

    I will try what you suggested.

    What do you mean by "output channel settings"? Where is that? I'm not very familiar with Linux.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to e14 Contributor

    Supposing you are using Ubuntu or Debian (until now these was the two better Linux I saw working on the Gizmo2) your audio will work with Alsa, where the audio out channel will work on several channels, the integrated audio output with the HDMI cable or the on-board audio processor sending and received audio signals through the jacks. With VLC you can configure the audio parameters as well as Alsa directly from the system configuration (all graphic user interfaces so I suppose these are better for you than the command line), selecting where the audio out should be directed.

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to balearicdynamics

    I know you can choose the audio and video output to use for VLC specifically, doesnt seem like it changes anything for other programs.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to e14 Contributor

    Sorry but let me ask you a question. What version of raspbian Linux did you installed? The standard version or the one with the Realtime Kernel specific for the audio card ?

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to balearicdynamics

    Raspbian? It's a standard Ubuntu 14.04 Desktop on Gizmo.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to e14 Contributor

    Sorry I wrote raspbian image

     

    I have not yet done tests in dept with audio only, but I saw that to get the better performances some users adopt the real-time kernel version of Ubuntu. AFAIK, there is not an RT version of the 14.04. This was only just a question about the operating system. And everywhere it is mentioned Ubuntu 14.04 LT as the best solution for the Gizmo2. When I installed it, during the installation process the OS asks for some non-open components related to the audio processor that should be installed. It is asked just because are not strictly open source so they note it. Excluding this detail I can't imagine what went wrong with your machine.In this moment I am using a version of debian but I have also a boot SSD disk with Ubuntu 14.04. If you can wait a while I can make specific tests then I will forward the working configuration (or report the same issue image )

     

    Enrico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • balearicdynamics
    0 balearicdynamics over 11 years ago in reply to e14 Contributor

    Sorry I wrote raspbian image

     

    I have not yet done tests in dept with audio only, but I saw that to get the better performances some users adopt the real-time kernel version of Ubuntu. AFAIK, there is not an RT version of the 14.04. This was only just a question about the operating system. And everywhere it is mentioned Ubuntu 14.04 LT as the best solution for the Gizmo2. When I installed it, during the installation process the OS asks for some non-open components related to the audio processor that should be installed. It is asked just because are not strictly open source so they note it. Excluding this detail I can't imagine what went wrong with your machine.In this moment I am using a version of debian but I have also a boot SSD disk with Ubuntu 14.04. If you can wait a while I can make specific tests then I will forward the working configuration (or report the same issue image )

     

    Enrico