GIZMO 2
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • GIZMO 2
  • More
  • Cancel
GIZMO 2
Forum GIZMO 2 no sound (Linux)
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join GIZMO 2 to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 13 subscribers
  • Views 2261 views
  • Users 0 members are here
Related

GIZMO 2 no sound (Linux)

e14 Contributor
e14 Contributor over 11 years ago

I get no sound on Linux Ubuntu 14.04 when plugging in a small speaker from the standard audio jack. But some noise is heard.

Also, when using a program using OpenAL for audio I get this error:

PrzxfRS.jpg

Thats all the info I can give. No error messages from the OS. Just no sound. Please tell me what else I can provide as info.

 

 

 

T

  • Sign in to reply
  • Cancel
Parents
  • monkeyman_stones
    0 monkeyman_stones over 10 years ago

    You need to change your alsa-base.conf file in /etc/modprobe.d/ to the device number (1, 2, 3, etc) your HDMI is/uses. You can find them from the terminal with command aplay -l which will define what number each sound device is. You can then change alsa-base.conf to target that device.  You can also go GUI and enter "alsamixergui" from the terminal, then click "File" (top left of window), then "Change Device" then select the HDMI option presented.  In /etc/modprobe.d/alsa-base.conf change everything (near the bottom of the page) from "options snd-(device type or name) index=-n" (where "n" is a number other than your HDMI) to the device id # of your HDMI (HDMI is often 0 or 3).

    Here is an exceptional resource and while it was created for/by Arch Linux, but it works for nearly all distros:  https://wiki.archlinux.org/index.php/Advanced_Linux_Sound_Architecture

    In addition, here is another excellent Arch Linux page defining the common codecs which are for all distro's (which you will need to install to have all sound file types play properly or at all): https://wiki.archlinux.org/index.php/codecs

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • monkeyman_stones
    0 monkeyman_stones over 10 years ago

    You need to change your alsa-base.conf file in /etc/modprobe.d/ to the device number (1, 2, 3, etc) your HDMI is/uses. You can find them from the terminal with command aplay -l which will define what number each sound device is. You can then change alsa-base.conf to target that device.  You can also go GUI and enter "alsamixergui" from the terminal, then click "File" (top left of window), then "Change Device" then select the HDMI option presented.  In /etc/modprobe.d/alsa-base.conf change everything (near the bottom of the page) from "options snd-(device type or name) index=-n" (where "n" is a number other than your HDMI) to the device id # of your HDMI (HDMI is often 0 or 3).

    Here is an exceptional resource and while it was created for/by Arch Linux, but it works for nearly all distros:  https://wiki.archlinux.org/index.php/Advanced_Linux_Sound_Architecture

    In addition, here is another excellent Arch Linux page defining the common codecs which are for all distro's (which you will need to install to have all sound file types play properly or at all): https://wiki.archlinux.org/index.php/codecs