GIZMO 2
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • GIZMO 2
  • More
  • Cancel
GIZMO 2
Forum Can Gizmo 2 use GX-420CA and 2GB chips w/o issues?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join GIZMO 2 to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 21 replies
  • Answers 4 answers
  • Subscribers 15 subscribers
  • Views 5972 views
  • Users 0 members are here
Related

Can Gizmo 2 use GX-420CA and 2GB chips w/o issues?

monkeyman_stones
monkeyman_stones over 9 years ago

I own a pair of GizmoSphere Gizmo 2 SBC's and with the first I also bought an AMD GX-420CA 4-Core, 2Ghz processor and more recently I purchased 5 (but only need 4 of them) Micron MT41K256M16HA-125E DDR3 RAM chips.  I'd like to install them all, but I want to make certain that I will not have an issue after having made such changes.

I know that GizmoSphere had intended to install 2GB of RAM chips from the start (but for $ savings did not), but I've seen no evidence that the 4-Core AMD GX-420CA 2Ghz processor had been intended, yet it's power usage is close enough to the AMD GX-210HA they did use that it should be fine so long as I don't overdo the use of the additional PCI slots through the High Speed Connector.

 

1) So, will the GizmoSphere Gizmo 2 work just fine and display all of the RAM of the 2GB RAM chips, or "No!"

2) Will the GizmoSphere Gizmo 2 work fine with the AMD GX-420CA, or is it too power hungry (or otherwise) to allow function of the SBC?

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • balearicdynamics
    balearicdynamics over 9 years ago in reply to shabaz +2 verified
    When I got the Gizmo2 for a project of a client I had a lot of issues ( helped me a lot) managing the options supported by the board. In the same period I have also explored with the guys of the GizmoSphere…
  • shabaz
    shabaz over 9 years ago +1
    Hi David, You should check with Gizmosphere directly if you can, but the answer for (1) was 'no' last time I checked the documentation or website - it stated somewhere that the board was capable of extra…
  • monkeyman_stones
    monkeyman_stones over 9 years ago in reply to shabaz +1 suggested
    It requires flashing the BIOS for the 2GB RAM to work. There's a source out there in which the user had already installed and created a BIOS file to flash for 2GB of RAM (it may have been through GitHub…
Parents
  • shabaz
    0 shabaz over 9 years ago

    Hi David,

     

    You should check with Gizmosphere directly if you can, but the answer for (1) was 'no' last time I checked the documentation or website - it stated somewhere that the board was capable of extra RAM, but it wasn't just a case of installing more (and I presumed this means other parts may need to be added too, e.g. capacitors). It isn't intended for user-modification to this extent anyway.

    For (2), I don't know the answer.

     

    EDIT: this is the text from the documentation (user guide) that I recalled:

    This is a manufacturing option only. It is not recommended that users attempt to remove or resolder the BGA memory components.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 9 years ago in reply to shabaz

    When I got the Gizmo2 for a project of a client I had a lot of issues ( helped me a lot) managing the options supported by the board. In the same period I have also explored with the guys of the GizmoSphere about the possibility to add memory easily but they told me that it was not needed - at least in theory - any extra hardware (the design includes the 2nd 1 GB RAM) but that they discovered unstability in the bios with more memory so decided to start the product with 1 Gb only. That's all what I know and it is a while I am not using this board (but I have in mind to use it in the near future for some local small server managing 3D printers.

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • monkeyman_stones
    0 monkeyman_stones over 9 years ago in reply to balearicdynamics

    How on Earth have you been able to work with people of a dead company? Their telephone number, address and email addresses are all dead. While the Gizmo 1 and 2 come with warranties, you cannot get any warranty coverage because they have killed the company. Questions asked here: http://www.gizmosphere.org/gizmoboard-support/  are never responded to.

    Here's some proof: https://youtu.be/N8OBgsgcfA4

    Phone #: https://drive.google.com/file/d/0B-1lAPlHMTDgNkpndDlVTGZhdzg/view?usp=drivesdk

    Fax #: https://drive.google.com/file/d/0B-1lAPlHMTDgcXgwOWVuZmZWMlU/view?usp=drivesdk

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • monkeyman_stones
    0 monkeyman_stones over 9 years ago in reply to balearicdynamics

    How on Earth have you been able to work with people of a dead company? Their telephone number, address and email addresses are all dead. While the Gizmo 1 and 2 come with warranties, you cannot get any warranty coverage because they have killed the company. Questions asked here: http://www.gizmosphere.org/gizmoboard-support/  are never responded to.

    Here's some proof: https://youtu.be/N8OBgsgcfA4

    Phone #: https://drive.google.com/file/d/0B-1lAPlHMTDgNkpndDlVTGZhdzg/view?usp=drivesdk

    Fax #: https://drive.google.com/file/d/0B-1lAPlHMTDgcXgwOWVuZmZWMlU/view?usp=drivesdk