GIZMO 2
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • GIZMO 2
  • More
  • Cancel
GIZMO 2
Forum Can Gizmo 2 use GX-420CA and 2GB chips w/o issues?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join GIZMO 2 to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 21 replies
  • Answers 4 answers
  • Subscribers 15 subscribers
  • Views 5972 views
  • Users 0 members are here
Related

Can Gizmo 2 use GX-420CA and 2GB chips w/o issues?

monkeyman_stones
monkeyman_stones over 9 years ago

I own a pair of GizmoSphere Gizmo 2 SBC's and with the first I also bought an AMD GX-420CA 4-Core, 2Ghz processor and more recently I purchased 5 (but only need 4 of them) Micron MT41K256M16HA-125E DDR3 RAM chips.  I'd like to install them all, but I want to make certain that I will not have an issue after having made such changes.

I know that GizmoSphere had intended to install 2GB of RAM chips from the start (but for $ savings did not), but I've seen no evidence that the 4-Core AMD GX-420CA 2Ghz processor had been intended, yet it's power usage is close enough to the AMD GX-210HA they did use that it should be fine so long as I don't overdo the use of the additional PCI slots through the High Speed Connector.

 

1) So, will the GizmoSphere Gizmo 2 work just fine and display all of the RAM of the 2GB RAM chips, or "No!"

2) Will the GizmoSphere Gizmo 2 work fine with the AMD GX-420CA, or is it too power hungry (or otherwise) to allow function of the SBC?

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • balearicdynamics
    balearicdynamics over 9 years ago in reply to shabaz +2 verified
    When I got the Gizmo2 for a project of a client I had a lot of issues ( helped me a lot) managing the options supported by the board. In the same period I have also explored with the guys of the GizmoSphere…
  • shabaz
    shabaz over 9 years ago +1
    Hi David, You should check with Gizmosphere directly if you can, but the answer for (1) was 'no' last time I checked the documentation or website - it stated somewhere that the board was capable of extra…
  • monkeyman_stones
    monkeyman_stones over 9 years ago in reply to shabaz +1 suggested
    It requires flashing the BIOS for the 2GB RAM to work. There's a source out there in which the user had already installed and created a BIOS file to flash for 2GB of RAM (it may have been through GitHub…
Parents
  • monkeyman_stones
    0 monkeyman_stones over 9 years ago

    Here: https://github.com/coreboot/coreboot/tree/master/src/mainboard/gizmosphere/gizmo2

     

    If you replace the Micron_MT41J128M16JT.spd.hex file with one specific to the Micron MT41K256M16HA such as Micron_MT41K256M16HA.spd.hex then there is no problem with the 2Gb chips.  They had intended it to have 2Gb from the start, but for the sake of profit margin dropped it to 1Gb.

     

    https://mail.coreboot.org/pipermail/coreboot-gerrit/2013-November/004302.html

     

    https://mail.coreboot.org/pipermail/coreboot-gerrit/2013-November/004198.html

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • monkeyman_stones
    0 monkeyman_stones over 9 years ago

    Here: https://github.com/coreboot/coreboot/tree/master/src/mainboard/gizmosphere/gizmo2

     

    If you replace the Micron_MT41J128M16JT.spd.hex file with one specific to the Micron MT41K256M16HA such as Micron_MT41K256M16HA.spd.hex then there is no problem with the 2Gb chips.  They had intended it to have 2Gb from the start, but for the sake of profit margin dropped it to 1Gb.

     

    https://mail.coreboot.org/pipermail/coreboot-gerrit/2013-November/004302.html

     

    https://mail.coreboot.org/pipermail/coreboot-gerrit/2013-November/004198.html