GIZMO 2
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • GIZMO 2
  • More
  • Cancel
GIZMO 2
Forum install windows 10
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join GIZMO 2 to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 12 subscribers
  • Views 1935 views
  • Users 0 members are here
  • gizmo_2
  • windows_10
Related

install windows 10

e14 Contributor
e14 Contributor over 11 years ago

I am attempting to install the latest Windows 10, build 10074, on a Gizmo 2.

 

The install starts fine, I select the Custom Install option and then get to a screen "Where do you want to install Windows" with the message "We couldn't find any drives.  To get a storage driver, click Load driver.

 

Does anyone know what driver  I need to use?

 

Interestingly if I browse fro a driver I can see the MicroSD that should be my hard drive, and I can also see its content.  So the card and interface is working.

 

I have tried using both NTFS and FAT32 for the file-system on the card.  I also tried using Diskpart to set up my MicroSD in the same way that I set up the Flash drive that I am using as the source of my Win 10 image, making it active etc.

 

Thoughts?

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 11 years ago

    Curious have you tried a true usb?

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Hi Clem

     

    I have not tried this.  The "HDD" on a Gizmo 2 is a MicroSD card slot, but I could attempt to use a second USB. 

     

    However, the USB drive that I am using for my OS installation media does not show up as a drive option for the Windows install, so I'm guessing this will not work.  No time to check it out right now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to clem57

    Hi Clem

     

    I have not tried this.  The "HDD" on a Gizmo 2 is a MicroSD card slot, but I could attempt to use a second USB. 

     

    However, the USB drive that I am using for my OS installation media does not show up as a drive option for the Windows install, so I'm guessing this will not work.  No time to check it out right now.