Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Blog Digispark, $12 dollar full-featured dev platform
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Catwell
  • Date Created: 22 Aug 2012 6:11 PM Date Created
  • Views 832 views
  • Likes 2 likes
  • Comments 3 comments
  • research
  • test
  • kickstarter
  • industry
  • hmi
  • sbc
  • embedded
  • cabeatwell
  • development
  • prototyping
  • measurement
  • dev
  • arduino
  • innovation
  • communication
Related
Recommended

Digispark, $12 dollar full-featured dev platform

Catwell
Catwell
22 Aug 2012

imageimage

Production Digisparks (via Kettenburg & Kickstarter)

 

Platforms like the Arduino or RPi offer infinite possibilities to create and invent — anything you can dream of or at least anything you can assemble and code. A large part of those possibilities do not require all of the features or power of those big name units. Once you finish a project, it is nice to keep it functional and start working on something else without dissecting old projects for those valued micro controllers.

 

 

With this in mind, hobbyist Erik Kettenburg decided he would take it upon himself to develop an affordable solution that could be used in less demanding applications. He wanted to take advantage of open source community contributions and Arduino's IDE (integrated development environment) that the Arduino model has already established as extremely effective.

 

 

His device is called the Digispark. It is a tiny (0.69in x 0.75in) microcontroller that can be plugged in via USB and is compatible with the Italian standard, Arduino's IDE and existing Arduino code.

 

 

Kettenburg started a Kickstarter for this idea and set the bar at a modest $5,000. With 20 days to go, the on-line community has shown their full support, contributing over $118,000!

 

 

Here is the list of notable features:

 

  • Support for the Arduino IDE 1.0+ (OSX/Win/Linux)
  • Power via USB or External Source - 5 V or 7-35 V (automatic selection)
  • On-board 500ma 5 V Regulator
  • Built-in USB (and serial debugging)
  • 6 I/O Pins (2 are used for USB only if your program actively communicates over USB, otherwise you can use all 6 even if you are programming via USB)
  • 8k Flash Memory (about 6k after bootloader)
  • I2C and SPI (USI)
  • PWM on 3 pins (more possible with Software PWM)
  • ADC on 4 pins
  • Power LED and Test/Status LED (on Pin0)

 

 

Regardless of the monetary success, Kettenburg says he wants to price the Digispark at just $12 a piece so developers do not feel the financial pressure to salvage them. He is also committed to making Digispark a piece of open source hardware. When the project is finalized, schematics, firmware and all necessary tools to hack the Digispark will be made available.

 

The heart is in the right place, and looks like the price is too.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Cabe

http://twitter.com/Cabe_e14

  • Sign in to reply
  • refaqtor
    refaqtor over 13 years ago

    Digisparks are nifty, if you prefer arduino.

     

    But the venerable MSP430 comes on these tiny boards @ ~$3/ea:

    http://www.ti.com/tool/ez430-t2012

     

    after getting this programmer w/ one board for $20:

    http://www.ti.com/tool/ez430-f2013

     

    These are my choice for small build-in-and-forget projects.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • awneil
    awneil over 13 years ago in reply to Workshopshed

    It's certainly a very neat little unit, but ...

     

    Andy Clark wrote:

     

     

    The one issue with this...

    I have another issue: the price - considering that you can get an STM32 Discovery board for under $10

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 13 years ago

    The one issue with this, and with the Arduino Mini Light is that they don't have an mounting points although you could have a dummy USB socket on the inside of your case for the Digispark. The Leonardo without headers is not much more so I'd be tempted to go for that option for deployment.