BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog BBB - PRU C compiler
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 30 Apr 2014 9:36 PM Date Created
  • Views 5674 views
  • Likes 5 likes
  • Comments 13 comments
  • beaglebone_black
  • sbc
  • beagleboneblack
  • bbb
  • BeagleBone
  • texas_instructments
  • ti
Related
Recommended

BBB - PRU C compiler

shabaz
shabaz
30 Apr 2014

Nice bit of information at this TI URL:

(My underlining below):

 

PRU Development

The Programmable Real-time Unit (PRU) is a low-latency microcontroller sub-system comprised of two or more 32-bit RISC processors, local instruction and data RAM, local peripherals and an interrupt controller. The PRU is efficient at handing events that have tight real-time constraints. The PRU is also known as the Industrial Communications Sub-System since it is used to enable industrial protocols such as EtherCATÂRegistered, EtherNet/IPâ„¢, PROFINET, PROFIBUS, POWERLINK, SERCOS III, and others. Each 32-bit processor runs at 200MHz, enabling 5ns instruction cycle. Local peripherals within the PRU sub-system include UART, eCAP, MII_RT, MDIO and IEP. The PRUâ€Tms fast input and output pins enable detection and reaction to I/O events within two PRU cycles.

Code Composer Studio provides a C compiler enabling users to add differentiation to their products.

 

(Downloading now! )

 

image

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 12 years ago in reply to e14 Contributor +1
    Hi Carlo, I did try the compiler, it worked well! I just did a simple loop, set it to unoptimized and visually inspected the assembler output. I have not yet tried to execute the code though. As you say…
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor +1
    In case anyone comes across this question, I noticed that while installing the Code Composer Studio, at least the Sitara 32-bit ARM Processors compilers should be selected, since the BeagleBone SoC is…
  • verminsky
    verminsky over 12 years ago

    This looks interesting indeed.  Have you had time to actually try the generated assembly code with a debian based BBB?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to e14 Contributor

    Hi Maddox,

     

    I don't recall doing anything special during the install, but I could be mistaken.:-( My version is 6.0.0.00190 (click on Help->About) and if I click on Project->New Project I see the screenshot shown above. All I can suggest is to uninstall, and try installing again, just double-checking all options as you install, in case there was anything BBB or PRU related in the options.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz

    Thanks - this is probably a newbie question, but I don't have the option to target the beaglebone_black with my installation of CCS v6 - after a fair amount of googling, I still come up empty - could you kindly point me in the right direction?  Did I miss something during the installation process?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to e14 Contributor

    Hi Maddox,

     

    If the PRU compiler is installed, then you can go to "Project"->"New CCS Project..."

    The window shown below will appear, select the PRU tab as shown:

    image

     

    You may have to explore a bit, I don't really have much in the way of instructions, I only had a chance to try a simple loop program, and will try something more intensive at a later date.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz

    How do create a CCS project with the PRU as the target?  In other words, how do I get CCS6.x to compile and generate PRU code?  I already clicked on the option to install the PRU compiler in CCS...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>