BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog BeagleBone Black Aluminium Enclosure
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 16 Jun 2015 9:40 PM Date Created
  • Views 2320 views
  • Likes 7 likes
  • Comments 7 comments
  • tem
  • tem_products
  • beagleboneblack
  • bbb
  • BeagleBone
  • beaglebone-black
  • texas_instruments
  • ti
Related
Recommended

BeagleBone Black Aluminium Enclosure

shabaz
shabaz
16 Jun 2015

I use the BeagleBone BlackBeagleBone Black for many projects, often they are bare but my latest BBB is housed in a very nice case from TEM Products.

This case is ideal if a project is going to be visible to an audience.


The case is quite different from others because it exposes the header connections on the BBB. It is also very accurately machined to act as a large heat sink.

Here it is with the BBB inside (the sticker is not included):


image


The enclosure is a very snug fit, I don't think a smaller case is possible! The finish is of a high quality, polished and nickel plated.

This is what the case looks like as purchased:

image

It is definitely an interesting enclosure design - very industrial looking, and it comes with hex bolts as seen here on the underside:

image

The inside of the enclosure shows a milled pattern except for the polished portion that makes thermal contact with the processor:

image

Assembly is straightforward, but a minor 'tweak' that I needed to do was to gently bend the leads of the polyswitch (orange blob close to the USB port on the right side of the photo below) down so that the other half of the enclosure could fit correctly; it was easy to do:

image

This is the final result, end views:

image

image

I'm very happy with this enclosure - there are also pre-drilled holes in the case for poking a toothpick or something in case the on-board buttons need pressing, and the console (serial) port header pins are exposed too (I use this wire-ended USB-serial adapterthis wire-ended USB-serial adapter and the connections on the BBB header 'J1' are: 1=Black, 2=Red, 4=Orange, 5=Yellow) :

image

The BBB on-board blue LEDs are not visible, but I might drill some tiny (1.5mm perhaps) holes for that if I feel the need at some point.

image

In summary the case is extremely unique, and I love the rugged look.

  • Sign in to reply

Top Comments

  • fvan
    fvan over 11 years ago +2
    Looks like a great enclosure. I like how it's so slim. $60 is a bit more than I'd care to spend on an enclosure though ...
  • fustini
    fustini over 11 years ago +1
    Thanks for posting the photos! It looks great!
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to fvan +1
    At least with a minion sticker on it, so the value will grow
  • clem57
    clem57 over 11 years ago

    If I had some $$ to spare, I would get it.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to balearicdynamics

    Hehe indeed, that's a rare sticker! It's not a low cost case but for project demo/exhibitions this is the case to use! Aluminium is nice to machine so I might make some custom modifications like holes for mounting.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gadget.iom
    gadget.iom over 11 years ago

    Looks like a solid piece of engineering there. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to fvan

    At least with a minion sticker on it, so the value will grow image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fvan
    fvan over 11 years ago

    Looks like a great enclosure. I like how it's so slim. $60 is a bit more than I'd care to spend on an enclosure though ...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
>