BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog Beaglebone Black with the BBView and the new Beaglebone Debian image
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 20 May 2015 9:16 AM Date Created
  • Views 8870 views
  • Likes 5 likes
  • Comments 27 comments
  • debian
  • bbview
  • Black
  • beaglebone_black
  • bbb
  • BeagleBone
  • screen
Related
Recommended

Beaglebone Black with the BBView and the new Beaglebone Debian image

e14 Contributor
e14 Contributor
20 May 2015

Fixing the problems with the BBView and the latest Beaglebone Debian image.

 

So since the new Debian update for the Beaglebone some problems have surfaced with using the BBView. Here I hope to help people fix those errors and get full use of their BBView.

 

Not many steps, and it is very easy to do.

 

     1.    Firstly we need to download the newest Debian Image from Here →http://beagleboard.org/latest-images

          Make sure you download the latest SD image (to boot from SD) or the flasher image (to reflash the EMMC with the new image)

 


     2.    Flash the image onto the SD card using your preferred means, dd command in linux /  win32DiskImager in windows are my preferred means.

 

 

     3.     Connect a an HDMI screen and keyboard, or or a TTL serial cable to the Beaglebone. If using the TTL cable you will also need a computer running a serial terminal program                (eg putty for windows)

 

 

     4.    Boot the Beaglebone Black from the new microSD card.

              Insert the microSD card.

               This will either boot the board from the microSD, or flash the new image onto the EMMC if you are using the flasher (This could take a while if using the flasher image)

 

 

     5.    When the board is booted, login using the username:root and password:debian

 

 

     6.     You will need some files to change the display output these files can be downloaded from HERE for Debian. Or from here.

               Just extract the downloaded zip file onto a USB stick and plug this into your Beaglebone Black

 

 

     7.    Now we need to change a few of the files to get the BBView to work

              In the terminal type....

root@beaglebone:~# mkdir /media/udisk
root@beaglebone:~# mount /dev/sda1 /media/udisk
root@beaglebone:~# cp -f /media/udisk/zImage /boot/vmlinuz-3.8.13-bone70 
root@beaglebone:~# cp -f /media/udisk/*.dtb  /boot/dtbs/3.8.13-bone70 
root@beaglebone:~# tar -xvf /media/udisk/kernel_modules.tar.gz -C /
root@beaglebone:~# cp -f /media/udisk/xorg.conf /etc/X11/
root@beaglebone:~# sync

 

 

              FOR 4 INCH DISPLAYS TYPE THIS

root@beaglebone:~# cd /boot/dtbs/3.8.13-bone70
root@beaglebone:~# cp am335x-boneblack-lcd4.dtb am335x-boneblack.dtb
root@beaglebone:~# sync

 

 

              FOR 7 INCH DISPLAYS TYPE THIS

root@beaglebone:~# cd /boot/dtbs/3.8.13-bone70
root@beaglebone:~# cp am335x-boneblack-lcd7.dtb am335x-boneblack.dtb
root@beaglebone:~# sync

 

 

     7.     Now shutdown your board. Connect your BBView and power it back up again.

 

Your BBView should now work as a screen for your Beaglebone Black. Have fun.

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to spletcher1 +1
    Hey Bill, I'm so sorry, I did miss that link out in my guide, the files are downloaded from this link. http://downloads.element14.com/downloads/bb-view/BB%20VIEW%20Debian%20Image.zip?COM=BeagleBoneBlack…
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to tomaja +1
    Hey Dragan, The latest " Debian 8.5 2016-05-13 4GB SD LXQT " image should have the image you're looking for just download it, extract it, then flash it. if that doesn't work then there is the old version…
  • tomaja
    tomaja over 9 years ago in reply to e14 Contributor

    Thanks!

    Sure, I will let you know image

     

    Dragan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to tomaja

    Hey Dragan,

    The latest "Debian 8.5 2016-05-13 4GB SD LXQT" image should have the image you're looking for just download it, extract it, then flash it. if that doesn't work then there is the old version from march 2015 available Debian 7.8 (BeagleBone, BeagleBone Black - 4GB SD) 2015-03-01

     

    both these links are taken straight from BeagleBoard.org - latest-images  under recommended versions, and older versions. Please get back to me to tell me whether this works or not and which one you ended up using  image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tomaja
    tomaja over 9 years ago in reply to e14 Contributor

    Hello

    I tried to find that Debian image but failed. Do you happen to have a link to it (Jan 2015)?

     

    Thanks in advance,

    Dragan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • imrank340@gmail.com
    imrank340@gmail.com over 10 years ago

    Hi Forum,

    I recently have BB-VIEW cape along with screen LCD7"  which has no brand name, but it work with

    "BBB-blank-debian-8.5-console-armhf-2016-06-19-2gb.img"  OS image with kernel 4.4.0rc via installing bb.org-overlay additional firmware which upgrade the dtc compiler 1.4.1.dfgehxx.  IT all work fine. But I have following problem:

    1/ BB Black using to BOOT from eMM memory instead of Micro SD  slot. Which I do not want it has to boot from Micro SD only

    2/ Since installing BB-View cape on the Beaglebone Black H Connectors A and B. The switch for "Boot Button" bas been obscure and cannot be able to reach. To have an access this switch surely to make BBB to boot from SD, which currently not possible.

    3/ I am trying to find GUI desktop for BBB under debian but I cannot able to locate so I can replace the current image with Debian GUI based desktop, if any one can share there experience will be much obliged.

     

    I will be grateful if any suitable solution can advise, please?

    Thank you,

    IK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Tried to install on 4.1.18

    First following the BBView Manual (copying zImage in /boot/uboot/ + dtbs in /boot/uboot/dtbs + untar kernel_modules.tar.gz + copy xorg.conf)

    Result : nothing

    Then followed this post (copying zImage in /boot/vmlinuz-4.1.18-ti-rt-r49 + dtbs in /boot/dtbs + untar kernel_modules.tar.gz + copy xorg.conf)

    Result : screen light up at startup and then shutdown (backlight visible)

     

    Any clue how to fix this ?

    Regards,

    Cam

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>