BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog Beaglebone Black with the BBView and the new Beaglebone Debian image
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 20 May 2015 9:16 AM Date Created
  • Views 8874 views
  • Likes 5 likes
  • Comments 27 comments
  • debian
  • bbview
  • Black
  • beaglebone_black
  • bbb
  • BeagleBone
  • screen
Related
Recommended

Beaglebone Black with the BBView and the new Beaglebone Debian image

e14 Contributor
e14 Contributor
20 May 2015

Fixing the problems with the BBView and the latest Beaglebone Debian image.

 

So since the new Debian update for the Beaglebone some problems have surfaced with using the BBView. Here I hope to help people fix those errors and get full use of their BBView.

 

Not many steps, and it is very easy to do.

 

     1.    Firstly we need to download the newest Debian Image from Here →http://beagleboard.org/latest-images

          Make sure you download the latest SD image (to boot from SD) or the flasher image (to reflash the EMMC with the new image)

 


     2.    Flash the image onto the SD card using your preferred means, dd command in linux /  win32DiskImager in windows are my preferred means.

 

 

     3.     Connect a an HDMI screen and keyboard, or or a TTL serial cable to the Beaglebone. If using the TTL cable you will also need a computer running a serial terminal program                (eg putty for windows)

 

 

     4.    Boot the Beaglebone Black from the new microSD card.

              Insert the microSD card.

               This will either boot the board from the microSD, or flash the new image onto the EMMC if you are using the flasher (This could take a while if using the flasher image)

 

 

     5.    When the board is booted, login using the username:root and password:debian

 

 

     6.     You will need some files to change the display output these files can be downloaded from HERE for Debian. Or from here.

               Just extract the downloaded zip file onto a USB stick and plug this into your Beaglebone Black

 

 

     7.    Now we need to change a few of the files to get the BBView to work

              In the terminal type....

root@beaglebone:~# mkdir /media/udisk
root@beaglebone:~# mount /dev/sda1 /media/udisk
root@beaglebone:~# cp -f /media/udisk/zImage /boot/vmlinuz-3.8.13-bone70 
root@beaglebone:~# cp -f /media/udisk/*.dtb  /boot/dtbs/3.8.13-bone70 
root@beaglebone:~# tar -xvf /media/udisk/kernel_modules.tar.gz -C /
root@beaglebone:~# cp -f /media/udisk/xorg.conf /etc/X11/
root@beaglebone:~# sync

 

 

              FOR 4 INCH DISPLAYS TYPE THIS

root@beaglebone:~# cd /boot/dtbs/3.8.13-bone70
root@beaglebone:~# cp am335x-boneblack-lcd4.dtb am335x-boneblack.dtb
root@beaglebone:~# sync

 

 

              FOR 7 INCH DISPLAYS TYPE THIS

root@beaglebone:~# cd /boot/dtbs/3.8.13-bone70
root@beaglebone:~# cp am335x-boneblack-lcd7.dtb am335x-boneblack.dtb
root@beaglebone:~# sync

 

 

     7.     Now shutdown your board. Connect your BBView and power it back up again.

 

Your BBView should now work as a screen for your Beaglebone Black. Have fun.

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 11 years ago in reply to spletcher1 +1
    Hey Bill, I'm so sorry, I did miss that link out in my guide, the files are downloaded from this link. http://downloads.element14.com/downloads/bb-view/BB%20VIEW%20Debian%20Image.zip?COM=BeagleBoneBlack…
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to tomaja +1
    Hey Dragan, The latest " Debian 8.5 2016-05-13 4GB SD LXQT " image should have the image you're looking for just download it, extract it, then flash it. if that doesn't work then there is the old version…
  • e14 Contributor
    e14 Contributor over 11 years ago

    After loading the newest BBB debian image and uploading your patched kernel along with modules and uploading dtb files, the ethernet (eth0) stops working. Tested with BBB revision C and BB View 7 inch.

    The ethernet looks like it works (it does detect whether the link is UP/DOWN, so PHY seems to work), but there is no communication over the network. It does not read DHCP packs. If I set the IP address to static, it does not communicate (no successful pings in either way).

    Once I load the old kernel back (along with the original modules) the LCD does not work (obviously) but ethernet works again. Tested with 3 devices (acquired from Polish and Australian suppliers).

     

    Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to randycarter2001

    Hi Randy,

     

    The Jan 2015 image is the correct one to use.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • randycarter2001
    randycarter2001 over 11 years ago

    Help!  Your instructions don't tell me which version of Debian I need in my BBB.  It just says "Firstly we need to download the newest Debian Image".  I have versions dated May 2014 and JAN 2015.  Which one is the right version for the BB-view-70?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to lotusf33t

    Hey Jack,

     

    See the comment I have just posted for Bill, above.

    This may help you.

    Any other problems please tell me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to spletcher1

    Hey Bill,

     

    I'm so sorry, I did miss that link out in my guide, the files are downloaded from this link.

    http://downloads.element14.com/downloads/bb-view/BB%20VIEW%20Debian%20Image.zip?COM=BeagleBoneBlack

     

    or if this doesn't work you can try get the files from here: element14: BB View LCD Cape Software Download Centre[1]

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>