BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog BeagleBone Web Server - LED Blinking
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: oneleggedredcow
  • Date Created: 22 Nov 2013 1:21 AM Date Created
  • Views 7265 views
  • Likes 2 likes
  • Comments 42 comments
Related
Recommended

BeagleBone Web Server - LED Blinking

oneleggedredcow
oneleggedredcow
22 Nov 2013

Table of Contents

Setup

LED Blinking

MySQL Installation

Temperature Sensor

Introduction

In the previous article, we set up the BeagleBone to be a webserver running Lighttpd and PHP.

 

In this article, we are going to build upon that foundation.  We are going to create a web site that lets the user turn on and off an LED on the BeagleBone.  This is a good example of how to create a simple web page that interacts with the BeagleBone and is a step towards our final goal of creating a website to show historical temperature information.

 

Turning a LED On/Off

BeagleBone LEDs can be turned on/off through command line, but in order to do this, we need to figure out what they are named.  The names can be found like this:

 

ls -1 /sys/class/leds

image

So, turning the usr2 LED on/off would look something like this:

image

1 will turn the LED on, and 0 will turn the LED off.

 

By default, some of the LEDs are used to display information to us about what is going on.  So, if you change the state of one of those LEDs, it will be quickly overwritten.  We can see this by looking at the trigger:

 

cat /sys/class/leds/beaglebone::usr0/trigger

image

To modify this so that the LED only changes when we tell it to, we can change the trigger to none:

 

echo none > /sys/class/leds/beaglebone::usr0/trigger

image

 

C Program

Now that we know how to turn on/off the LEDs, we can write a small C program to make it easier for us. The program will take in the number of the LED to change (0-4) and the state to change it to (off = 0, on = 1). Here’s the code:

 

#include <stdio.h>

#include <stdlib.h>

#include <fcntl.h>

#include <unistd.h>

 

int main(int argc, const char *argv[])

{

if (argc != 3)

{

printf("Usage:\n");

printf("\tledCtl <led> <on/off>\n");

printf("\n");

printf("<led>  : Number between 0-3\n");

printf("<on/off>: 1 = on, 0 = off\n");

 

return 1;

}

 

int ledNum = atoi(argv[1]);

if (ledNum < 0 || ledNum > 3)

{

printf("<led>  : Number between 0-3\n");

 

return 1;

}

 

char ledPath[1024];

sprintf(ledPath, "/sys/class/leds/beaglebone::usr%d/brightness", ledNum);

int fid = open(ledPath, O_WRONLY);

 

int onOff = atoi(argv[2]);

switch (onOff)

{

case 0:

write(fid, "0", 1);

break;

case 1:

write(fid, "1", 1);

break;

default:

printf("<on/off>: 1 = on, 0 = off\n");

return 1;

}

 

close(fid);

 

return 0;

}

 

Remember to change the path of the LED to the path that we found earlier.

 

For a simple task like this, we could have just used the command line to turn the LEDs on/off. However, I wanted to put it into a C program so that we set ourselves up better for the future.  When we take temperature measurements and put them into a MySQL database, it will require more logic that is better suited for a small program rather than the command line.

 

The code should be fairly clear.  It is mostly just checking the inputs that the user gave us to make sure that they are reasonable.

 

Before we compile it, we need to create a directory to store the scripts that we are going to be running on our web site:

 

mkdir /www/cgi-bin

 

To compile the code, type:

 

g++ ledctl.cpp -o /www/cgi-bin/ledctl

image

 

Then we can run some examples and make sure that it works:

 

/www/cgi-bin/ledCtl

/www/cgi-bin/ledCtl 2 1

/www/cgi-bin/ledCtl 2 0

image

 

Creating a Web Page

Awesome, now that we have a program to control the LEDs on the BeagleBone, let’s create a web page so that we can control the LEDs over the Internet.  Let’s call the web page ledCtl.php and place the following code in it:

 

<html>

<head>

<title>BeagleBone LED Changer</title>

<style type="text/css">

p { display: table-cell; }

button { width: 75px; margin: 2px auto; }

</style>

<?php

if (isset($_GET['led']) && isset($_GET['onOff']))

{

$led = $_GET['led'];

$onOff = $_GET['onOff'];

 

exec( "/www/cgi-bin/ledctl $led $onOff" );

}

?>

</head>

<body>

<div style="width: 200px; margin: 0px auto;">

<div style="width: 100px; float: left;">

<p>LED #2:</p>

<button type="button" onclick="location.href='ledCtl.php?led=2&onOff=1'">ON</button>

<button type="button" onclick="location.href='ledCtl.php?led=2&onOff=0'">OFF</button>

</div>

<div sytle="width: 100px; margin-left: 100px;">

<p>LED #3:</p>

<button type="button" onclick="location.href='ledCtl.php?led=3&onOff=1'">ON</button>

<button type="button" onclick="location.href='ledCtl.php?led=3&onOff=0'">OFF</button>

</div>

</div>

</body>

</html>

 

Note: We used LEDs #2 and #3 because LED #0 and #1 occasionally blink and override our on/off settings.

 

Then we can test our web page by going to a browser and using our new web page:

image

Pressing the buttons on the page should change the state of the LEDs on the BeagleBone!

 

Next Article

In the next article, we are going to get MySQL up and running on the BeagleBone.  We will use MySQL as a convenient place to store the temperature measurements that we take.  This will also make it easy to retrieve the data when the user requests historical temperature information through our web page.

Attachments:
ledctl.zip
  • Sign in to reply
  • robs7
    robs7 over 9 years ago

    Hello,

    I want to follow your tutorial but I'm having problems turning the led on and off, I've done the setup and now it's the led turn but i'm having problems with it. I am using python to switch the led and the code work just fine:

     

    import Adafruit_BBIO.GPIO as GPIO

    GPIO.setup("P9_12",GPIO.OUT)

    GPIO.output("P9_12"GPIO.HIGH)

     

    Now, in the web page I have this code:

     

    <body>

         <?php

              if(isset($_GET["on"])){

                   exec("python turnOn.py");}

         ?>

         <form method = "get">

              <button type = "button" onclick="location.href='on-off.php?on=true'">ON</button>

         </form>

    </body>

     

    According to my logic this should turn the led on since I use the button to run the python program directly, the web page refreshes correctly but there is no change on the led.

     

    If yoy can help I would really aprecciate it. Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor
    @Jaeeun Choi,

    Can you please upload your corrected code for turn on/off of External led?

     

    Thanks in advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    I'm using Rev C with Debian, after some changes on both CPP and PHP file they can be execute on BBB, but there is a broblem : in console ledctl app work correct only with "sudo" but in web page there isn't any effect on leds.

    I changed  permission of ledctl but still doesn't work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • oneleggedredcow
    oneleggedredcow over 12 years ago in reply to e14 Contributor

    Shucks, I've only tried using Angstrom, so I don't know about what would be different with Debian.

     

    Have you tried doing "chmod 4755 /www/cgi-bin/ledctl"?  this was mentioned earlier in the comments and I'm not sure if it fixes the problem or not.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    I am also having issues getting the LEDs to blink. The PHP page loads fine, clicking the buttons reloads the page just fine, and I'm nearly 100% that the PHP page is executing the program, but still, no blinking.

     

    The reason I'm so sure that the code is being executed, is that I replaced the suggested program here with one that toggles all 4 leds simultaneously for 20 seconds. When I run that particular php page, the reload takes exactly 20 seconds (as opposed to nearly instantaneously for the code that simply turns on or off a single LED).

     

    I originally had my programs in /var/www/cgi-bin, because that is where lighttpd created the /www/ folder. I gave the cgi-bin folder 777 permissions. No dice.

     

    So I moved the programs to /www/cgi-bin, and gave /www/, /cgi-bin/, and all the programs full permission. No dice. But really, executing the program is probably not the issue.

     

    So I went to each /sys/class/leds/beaglebone:green:usr* folder, and gave 666 permissions to each ones brightness. Then, I gave full permissions to each of the containing folders (/sys/class/leds/beaglebone:green:usr*/ . Still it does not work.

     

    I'm using Debian, if that helps.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>