BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog BeagleBone Web Server - LED Blinking
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: oneleggedredcow
  • Date Created: 22 Nov 2013 1:21 AM Date Created
  • Views 7265 views
  • Likes 2 likes
  • Comments 42 comments
Related
Recommended

BeagleBone Web Server - LED Blinking

oneleggedredcow
oneleggedredcow
22 Nov 2013

Table of Contents

Setup

LED Blinking

MySQL Installation

Temperature Sensor

Introduction

In the previous article, we set up the BeagleBone to be a webserver running Lighttpd and PHP.

 

In this article, we are going to build upon that foundation.  We are going to create a web site that lets the user turn on and off an LED on the BeagleBone.  This is a good example of how to create a simple web page that interacts with the BeagleBone and is a step towards our final goal of creating a website to show historical temperature information.

 

Turning a LED On/Off

BeagleBone LEDs can be turned on/off through command line, but in order to do this, we need to figure out what they are named.  The names can be found like this:

 

ls -1 /sys/class/leds

image

So, turning the usr2 LED on/off would look something like this:

image

1 will turn the LED on, and 0 will turn the LED off.

 

By default, some of the LEDs are used to display information to us about what is going on.  So, if you change the state of one of those LEDs, it will be quickly overwritten.  We can see this by looking at the trigger:

 

cat /sys/class/leds/beaglebone::usr0/trigger

image

To modify this so that the LED only changes when we tell it to, we can change the trigger to none:

 

echo none > /sys/class/leds/beaglebone::usr0/trigger

image

 

C Program

Now that we know how to turn on/off the LEDs, we can write a small C program to make it easier for us. The program will take in the number of the LED to change (0-4) and the state to change it to (off = 0, on = 1). Here’s the code:

 

#include <stdio.h>

#include <stdlib.h>

#include <fcntl.h>

#include <unistd.h>

 

int main(int argc, const char *argv[])

{

if (argc != 3)

{

printf("Usage:\n");

printf("\tledCtl <led> <on/off>\n");

printf("\n");

printf("<led>  : Number between 0-3\n");

printf("<on/off>: 1 = on, 0 = off\n");

 

return 1;

}

 

int ledNum = atoi(argv[1]);

if (ledNum < 0 || ledNum > 3)

{

printf("<led>  : Number between 0-3\n");

 

return 1;

}

 

char ledPath[1024];

sprintf(ledPath, "/sys/class/leds/beaglebone::usr%d/brightness", ledNum);

int fid = open(ledPath, O_WRONLY);

 

int onOff = atoi(argv[2]);

switch (onOff)

{

case 0:

write(fid, "0", 1);

break;

case 1:

write(fid, "1", 1);

break;

default:

printf("<on/off>: 1 = on, 0 = off\n");

return 1;

}

 

close(fid);

 

return 0;

}

 

Remember to change the path of the LED to the path that we found earlier.

 

For a simple task like this, we could have just used the command line to turn the LEDs on/off. However, I wanted to put it into a C program so that we set ourselves up better for the future.  When we take temperature measurements and put them into a MySQL database, it will require more logic that is better suited for a small program rather than the command line.

 

The code should be fairly clear.  It is mostly just checking the inputs that the user gave us to make sure that they are reasonable.

 

Before we compile it, we need to create a directory to store the scripts that we are going to be running on our web site:

 

mkdir /www/cgi-bin

 

To compile the code, type:

 

g++ ledctl.cpp -o /www/cgi-bin/ledctl

image

 

Then we can run some examples and make sure that it works:

 

/www/cgi-bin/ledCtl

/www/cgi-bin/ledCtl 2 1

/www/cgi-bin/ledCtl 2 0

image

 

Creating a Web Page

Awesome, now that we have a program to control the LEDs on the BeagleBone, let’s create a web page so that we can control the LEDs over the Internet.  Let’s call the web page ledCtl.php and place the following code in it:

 

<html>

<head>

<title>BeagleBone LED Changer</title>

<style type="text/css">

p { display: table-cell; }

button { width: 75px; margin: 2px auto; }

</style>

<?php

if (isset($_GET['led']) && isset($_GET['onOff']))

{

$led = $_GET['led'];

$onOff = $_GET['onOff'];

 

exec( "/www/cgi-bin/ledctl $led $onOff" );

}

?>

</head>

<body>

<div style="width: 200px; margin: 0px auto;">

<div style="width: 100px; float: left;">

<p>LED #2:</p>

<button type="button" onclick="location.href='ledCtl.php?led=2&onOff=1'">ON</button>

<button type="button" onclick="location.href='ledCtl.php?led=2&onOff=0'">OFF</button>

</div>

<div sytle="width: 100px; margin-left: 100px;">

<p>LED #3:</p>

<button type="button" onclick="location.href='ledCtl.php?led=3&onOff=1'">ON</button>

<button type="button" onclick="location.href='ledCtl.php?led=3&onOff=0'">OFF</button>

</div>

</div>

</body>

</html>

 

Note: We used LEDs #2 and #3 because LED #0 and #1 occasionally blink and override our on/off settings.

 

Then we can test our web page by going to a browser and using our new web page:

image

Pressing the buttons on the page should change the state of the LEDs on the BeagleBone!

 

Next Article

In the next article, we are going to get MySQL up and running on the BeagleBone.  We will use MySQL as a convenient place to store the temperature measurements that we take.  This will also make it easy to retrieve the data when the user requests historical temperature information through our web page.

Attachments:
ledctl.zip
  • Sign in to reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to oneleggedredcow

    If you know it's an LED you're connecting to a GPIO, then create an appropriate devicetree to define the gpio as a LED in the same fashion as the onboard LEDs.

    The advantage to doing that is that you get all the same features like triggers without needing to re-implement everything including the code you presented here from scratch. again.

    It's certainly valid to just twiddle a GPIO manually in various circumstances, but it seems strange not to take advantage of what linux provides.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • oneleggedredcow
    oneleggedredcow over 12 years ago in reply to oneleggedredcow

    C:\Users\user\Desktop is a Windows path.  So, the file isn't on the beaglebone.  You need to transfer it to the beaglebone using something like WinSCP.

     

    As far as using the GPIO, it is very similar.  You just need to change the ledPath variable to point to the pin that you want to control.  Here's an example:

    c++ - how to control beaglebone gpio pins - Stack Overflow

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • oneleggedredcow
    oneleggedredcow over 12 years ago in reply to e14 Contributor

    Based on your output, g++ is installed and looks like it is working.

     

    The steps in the tutorial assume that the file is in the home directory of the root user.  This is symbolized by the ~ character.  Honestly, it doesn't really matter what directory you run the command in though.  So, I would do an ls and make sure that ledctl.cpp is in the directory that you are currently in.  If not, then navigate to the directory that you put the file in and run the command there.  Since a full path is specified for the output (/www/cgi-bin/ledctl), it doesn't matter where you do the compilation, the output will go to the correct location.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to oneleggedredcow

    saved file as.cpp

    but the errors come out.

    so do i have to install g++ into baglebone black?

    and the other issue is do i put the directory where i saved .cpp file instead of /www/cgi-bin/ledctl?

    if i saved that file into desktop(C:\Users\user\Desktop) then put /qww/cgi-bin/desktop/ledctl ????

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • oneleggedredcow
    oneleggedredcow over 12 years ago in reply to e14 Contributor

    Sure, you could use your favorite text editor (vi, emacs, etc.) and create a new file and type it in through putty.

     

    Another way would be to download the file attached to this post using wget on the beaglebone:

         wget http://www.element14.com/community/servlet/JiveServlet/download/38-122477/ledctl.zip

    Then unzip the file and you should be good to go.

     

    Yet another option would be to copy/paste the code into notepad and save the file as ledctl.cpp.  The transfer the file to your beaglebone using WinSCP.  (This option works really well if you are planning on making additional changes to the code.  This lets you use your favorite IDE to program in and then transfer the code to the beaglebone.)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>