BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog PocketBeagle Photos and Graphics
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 23 Feb 2018 5:42 PM Date Created
  • Views 3017 views
  • Likes 17 likes
  • Comments 13 comments
  • pocketbeaglebone
  • bbb
  • pocket beagle
  • pocketbeagle
  • beagleboard
  • BeagleBone Black
  • pocket beaglebone
Related
Recommended

PocketBeagle Photos and Graphics

shabaz
shabaz
23 Feb 2018

I finally purchased a couple of PocketBeagles, I knew they would be small, but it is still amazing to see it close-up!

image

It is very thin too, it measured 4.60mm (the highest point is the surface of the Octavo module).

image

For connections, I purchased 2x9way total 18-way header pins2x9way total 18-way header pins because these are cheaper than 2x18way. A total of four of these are needed to fully connect to the PocketBeagle, although that might not be necessary for all projects. Note that the header pins are connected to the underside of the PocketBeagle, not to the top side like the larger BeagleBone Black. The pins won't fit on the top side, because the Octavo module hits the plastic surround of the header pins. It seems to make sense, that the PocketBeagle would be plugged on top of a larger board.

 

The very helpful silkscreen shows the pin descriptions on the underside:

image

Here are some graphics of the top and bottom side, perhaps useful for documenting projects:

image

image

Renders of the PCB:

image

image

  • Sign in to reply

Top Comments

  • bwelsby
    bwelsby over 8 years ago +4
    Nice. What have you got planned for them?
  • shabaz
    shabaz over 8 years ago in reply to bwelsby +4
    Hi Brian, I'm hoping to develop them as a kind of test tool. Still only a half-thought out idea : )
  • mcb1
    mcb1 over 8 years ago +4
    That is small.! No I don't need one, so I'm resisting
  • shabaz
    shabaz over 7 years ago in reply to cstanton

    It's a FLIR sensor, so not many distributors for it: model Lepton third gen, part code 500-0726-01 , Avnet has the breakout board for it so I guess they may have supplied the sensor at some point too, or maybe planning to.

    I used the sensor, plus the breakout board. The Lepton 3rd gen comes in two versions, the one I used, and another one which only costs an extra $10 - part code 500-0771-01

    That more expensive one is better, because it can be set to a wider temperature range mode, and also provides calibrated temperature values for each pixel, as well as pixel color.

    The version I used does not provide temperature value in degrees C, so I have to approximate or calibrate by pointing at a known temperature object first. I did not know that at the time I ordered it : (

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to shabaz

    Which thermal sensor was it?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to cstanton

    Hi Christopher,

     

    I ended up using it for a proof-of-concept device, in the photo here:

    There's a thermal camera behind it..

    image

    This is the type of thing it could do:

    image

     

    I'm thinking it could be worth taking the code, and making an open source portable thermal camera with it if there's interest.. since it can be handy for seeing where there are cold spots in the home, or for troubleshooting hot-spots on a PCB.

    I was thinking of using the Pi 3A for it perhaps, since that could be quicker (there are some reasonable-cost TFT LCD HATs for it). Or I could just wire the Pi TFT to the PocketBeagle, if the drivers work for that.

    Sadly I slightly damaged the thermal sensor (seems very static-sensitive : ( and now have some permanent failed image lines, but it still semi-functions enough to do a prototype.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 7 years ago in reply to shabaz

    Did you get any further with them? image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago

    That is small.!

    No I don't need one, so I'm resisting image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>