BeagleBoard
  • Products
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum USB 3.0 support for beagle bone AI.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 27 replies
  • Answers 11 answers
  • Subscribers 104 subscribers
  • Views 4724 views
  • Users 0 members are here
  • beagleboard_ai
Related

USB 3.0 support for beagle bone AI.

prathamesh12
prathamesh12 over 5 years ago

I want to use basler ace camera (acA1300-200um) with beagle bone AI board. It requires usb 3.0 host controller. As BB AI board provides only usb 2.0 , camera isn't working. Is there any way we can add usb 3.0 support to board? Like an external module with 3.0 support which can be further connected to AI board via UART....

  • Sign in to reply
  • Cancel

Top Replies

  • cstanton
    cstanton over 5 years ago in reply to prathamesh12 +3 verified
    The answer is simply hidden. sudo /opt/scripts/boot/bbai_usb_host.sh This executes: echo "host" > /sys/kernel/debug/48890000.usb/mode Which puts the USB-C 3.0 hub on the BeagleBone AI into 'USB Host Mode…
  • gdstew
    gdstew over 5 years ago +2 suggested
    The USB C connector used to power the AI is also connected to a USB 3 data interface on the SoC. The problem I've seen is that none of the power supplies for the AI make these signals available to use…
  • cstanton
    cstanton over 5 years ago in reply to gdstew +2 suggested
    Maybe a USB-C USB hub would work? If it allows backpowering. I may be able to test this.
  • shabaz
    0 shabaz over 5 years ago

    If it is an option, you could also consider GigE camera since the BB-AI has a high-throughput interface for it (Gigabit Ethernet). Many of these cameras are available in GigE variants too.

    However, I'd just like to point out that it can be an uphill struggle getting the open source software running for GigE cameras on ARM. I didn't succeed in my limited tests, I had some runtime errors I never managed to get to the bottom of..

    Is your camera supplied with software, and have you been successful installing it or compiling it on ARM and trying to run it, and see what happens with USB 2.0? (i.e. deliberately configure for a much lower frame rate or resolution).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • prathamesh12
    0 prathamesh12 over 5 years ago in reply to shabaz

    Yep.GigE may be another option. But in that case I need to change camera itself which is not feasible for me.

     

    Basler cameras run on pylon software. I have successfully installed it (Basler have provided separate arm image with c/c++ support). They have provided python wrapper for it as well.

    According to the company, USB 3.0 cameras will get detected on USB 2.0 ports but can't be used at all(There are different cameras with lower frame rate support for USB 2.0. One in the ACA category does not support it).

    I can compile the codes using their software and it gives me error like "USB 3.0 compatible port required."

     

    I have tested that camera with same software on my linux pc. It works absolutely fine with USB 3.0 and gives same error as of arm for USB 2.0 port.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton over 5 years ago in reply to prathamesh12

    The answer is simply hidden.

     

    sudo /opt/scripts/boot/bbai_usb_host.sh

     

    This executes:

     

    echo "host" > /sys/kernel/debug/48890000.usb/mode

     

    Which puts the USB-C 3.0 hub on the BeagleBone AI into 'USB Host Mode' and allows devices to be detected. While the HDMI isn't currently supported on my device, the USB ports are, and the devices connected were detected. So long as your USB hub back powers the ports, then set the right mode for the USB hub and it'll work fine. You may want to change the other modes as appropriate.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • prathamesh12
    0 prathamesh12 over 5 years ago in reply to cstanton

    This solves the problem. But now my usb hub is getting detected as 2.0

    On linux machine current usb hub is detected as both 2.0 and 3.0

    So is this due to fault in usb-hub?

    Or there is any mode other than host and drvice that can help?

     

    lsusb returns:

    debian@beaglebone:/opt/scripts/boot$ lsusb

    Bus 002 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub

    Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub

    Bus 004 Device 001: ID 1d6b:0003 Linux Foundation 3.0 root hub

    Bus 003 Device 003: ID 2676:ba02 Basler AG ace

    Bus 003 Device 002: ID 05e3:0610 Genesys Logic, Inc. 4-port hub

    Bus 003 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub

    debian@beaglebone:/opt/scripts/boot$

     

     

    dmesg on linux PC returns:

     

    [12846.476430] usb 2-3: new SuperSpeed USB device number 10 using xhci_hcd

    [12846.499861] usb 2-3: New USB device found, idVendor=05e3, idProduct=0616

    [12846.499863] usb 2-3: New USB device strings: Mfr=1, Product=2, SerialNumber=0

    [12846.499865] usb 2-3: Product: USB3.0 Hub

    [12846.499867] usb 2-3: Manufacturer: GenesysLogic

    [12846.502231] hub 2-3:1.0: USB hub found

    [12846.502606] hub 2-3:1.0: 4 ports detected

    [12846.624214] usb 1-8: new high-speed USB device number 18 using xhci_hcd

    [12846.783695] usb 1-8: New USB device found, idVendor=05e3, idProduct=0610

    [12846.783698] usb 1-8: New USB device strings: Mfr=1, Product=2, SerialNumber=0

    [12846.783700] usb 1-8: Product: USB2.0 Hub

    [12846.783701] usb 1-8: Manufacturer: GenesysLogic

    [12846.785064] hub 1-8:1.0: USB hub found

    [12846.786468] hub 1-8:1.0: 4 ports detected

     

    HERE HUB IS BEING DETECTED BOTH AS USB3.0 and USB2.0

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton over 5 years ago in reply to prathamesh12

    It may simply mean the USB 3.0 controller can negotiate USB 2.0 as well, depends how the driver works.

     

    Have you tried connecting a USB 3.0 hub to it, and then your camera? What does it negotiate at?

     

    Because the output provide shows you're connecting a GenesysLogic USB 2.0 hub. Which either means your connected hub is only USB 2.0 or the driver for the GenesysLogic chipset can only negotiate USB 2.0

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • prathamesh12
    0 prathamesh12 over 5 years ago in reply to cstanton

    Hi cstanton

     

    The hub which I am using is USB 3.0 and it is showing GenesysLogic USB 2.0 hub on BB and both 2.0 and 3.0 on linux.

    I did try it on windows. One thing I noticed is Camera does not show up when I connect hub with external power supply along with c type of PC.

     

    May be it's problem with the hub. When you tried connecting it with your hub, dis it show any problem on USB 3.0 except HDMI port? Have you actually tried connecting any USB3.0 device like hdd or something?

    Can you make sure that your hub is connected as USB3.0 host only? If yes then I ll change my hub itself....

     

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton over 5 years ago in reply to prathamesh12

    prathamesh12

    I'll check it out with the USB 3.0 hub and devices I have.

     

    Until then, have you ensured that your kernel is up to date, and the operating system? bbb.io/upgrade

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • prathamesh12
    0 prathamesh12 over 5 years ago in reply to cstanton

    debian@beaglebone:/opt/scripts$ git pull returns Already up to date.

     

    uname -r returns this  4.14.108-ti-r127

     

    Is this version okay?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • cstanton
    0 cstanton over 5 years ago in reply to prathamesh12

    Make sure you also run

    sudo tools/update_kernel.sh

     

    Your kernel looks like it may be out of date, or at least there are two more recent versions you can update to:

     

    https://rcn-ee.com/repos/latest/stretch-armhf/LATEST-ti

     

    ABI:1 LTS314 3.14.79-ti-r92

    ABI:1 LTS41 4.1.30-ti-r70

    ABI:1 LTS44 4.4.155-ti-r155

    ABI:1 LTS49 4.9.147-ti-r121

    ABI:1 LTS414 4.14.108-ti-r127

    ABI:1 LTS419 4.19.94-ti-r36

    ABI:1 LTS54 5.4.20-ti-r5

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • prathamesh12
    0 prathamesh12 over 5 years ago in reply to cstanton

    I run this command

    sudo tools/update_kernel.sh --lts-5_20.

    kernel got upgraded. Then I rebooted it but board is not booting at all..........

    D4 led is flashing constantly and nothing else.

    Did I crash os/kernel? What can I do now ?image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>