RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Blog Building Linux Kernel on RiotBoard for RiotBoard :)
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Nitin_Bhaskar
  • Date Created: 1 Aug 2014 5:54 PM Date Created
  • Views 855 views
  • Likes 0 likes
  • Comments 0 comments
  • riotboard
  • linux
Related
Recommended

Building Linux Kernel on RiotBoard for RiotBoard :)

Nitin_Bhaskar
Nitin_Bhaskar
1 Aug 2014

First thing first, I flashed images from Linux.zip under windows onto the eMMC of RiotBoard and then proceeded to build kernel on RiotBoard. By default, the oneiric rootfs contains toolchain for building the kernel. The only thing missing is the mkimage utility to obatin uImage. I have attached the mkimage executable below. Place this in "/usr/bin/".

 

Grab a copy of Linux kernel. I obtained one from embest. I used "embest_imx_3.0.35_4.0.0" branch.

 

git clone git://github.com/embest-tech/linux-imx.git -b embest_imx_3.0.35_4.0.0

 

Open Makefile and then modify CROSS_COMPILE (~line no. 196) to contain nothing

 

CROSS_COMPILE    ?=

 

Configure the kernel for RiotBoard by,

 

make imx6_defconfig

 

Build kernel sources by running

 

make uImage

 

After half an hour or so, following output can be seen on console

 

  LD  arch/arm/boot/compressed/vmlinux

  OBJCOPY arch/arm/boot/zImage

  Kernel: arch/arm/boot/zImage is ready

  UIMAGE  arch/arm/boot/uImage

Image Name:   Linux-3.0.35

Created:  Sun Oct  1 00:00:49 2017

Image Type:   ARM Linux Kernel Image (uncompressed)

Data Size:3908484 Bytes = 3816.88 kB = 3.73 MB

Load Address: 10008000

Entry Point:  10008000

  Image arch/arm/boot/uImage is ready

 

Next task is to flash the freshly built uImage. This can be done by issuing following command

 

dd if=uImage of=/dev/mmcblk0 bs=1M seek=1 conv=fsync

 

Reboot the RiotBoard and see the new kernel boot!!!

Attachments:
mkimage.zip