RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Blog Linux on the RIoTBoard Part 2: Kernel
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: radiatortwo
  • Date Created: 18 Sep 2014 5:21 PM Date Created
  • Views 2802 views
  • Likes 1 like
  • Comments 9 comments
Related
Recommended

Linux on the RIoTBoard Part 2: Kernel

radiatortwo
radiatortwo
18 Sep 2014

This series of blog posts contains the following parts:

1. The bootloader U-Boot

2. The Kernel (This part)

3. Debian Root File System

4. Flashing with MFGTool in Windows

5.Creating an SDCard Image

 

Part 2: Kernel

 

In this part we will be creating the kernel, the device tree as well as the modules and kernel headers from the mainline source code.

 

The build environment will be the same as the one for building u-boot.

So if you didn´t already do that, then you should do "Step 1. Essentials and Compiler" from Part 1.

 

1. Get the source code

 

If you´re not already in the right folder, cd into the folder you will be saving the code.

You should already have one i f you followed Part 1 of this series.

In my case:

 

cd /home/riotboard/linux
          

 

And now we´ll get the code from Linus Torvalds original Linux repository.

 

git clone git://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git
cd linux

 

 

2. Compile the Kernel

 

Before compiling make sure the environment variables are set correctly. (As described in Part 1)

Also make sure the OUTPUT variable is set to the correct folder.

 

export ARCH=arm
export CROSS_COMPILE=arm-linux-gnueabihf-
export OUTPUT=/home/riotboard/linux/output
          

 

First write the config to compile the kernel for our RIoTBoard.

(We now can use the config that´s integrated into the mainline code.)

 

make imx_v6_v7_defconfig
          

 

If you need to change the config. Like activating support for specific drivers or similar, you can execute menuconfig to edit the config file with a dialog.

(This is optional)

 

make menuconfig
          

 

Now we can compile the Kernel

(Adjust the parameter j to the number of threads it should use. Most likely one for each CPU.)

 

make -j4 bzImage
          

 

Now in the folder arch/arm/boot we have the Kernel file zImage

 

Copy that file into our Output boot folder.

 

mkdir $OUTPUT/boot
cp arch/arm/boot/zImage $OUTPUT/boot/zImage
          

 

3. Device Tree Blob

 

Next we need the Device Tree Blob file.

With the following command all DTB files will be created. But we copy only the one we need.

 

make dtbs
cp arch/arm/boot/dts/imx6dl-riotboard.dtb $OUTPUT/boot/imx6dl-riotboard.dtb
          

 

4. Modules and Headers

 

Now we need to create the modules.

And then copy them into our output folder.

 

make modules -j4
make modules_install INSTALL_MOD_PATH=$OUTPUT
          

 

Now the same thing for the Kernel headers.

This is optional, but sometimes you´ll need them to compile additional drivers on the board for example.

So let´s integrate them too. They belong into the usr folder.

 

make headers_install INSTALL_HDR_PATH=$OUTPUT/usr
          

 

Last thing to do now is just to pack everything into a tarball and remove the unneeded folders.

 

cd $OUTPUT
tar cvzf linux-kernel.tgz boot lib usr
rm -rf boot lib usr

 

That´s it for this part.

 

In the next part we will be creating a debian root file system from scratch.

 

Continue with Step 3

  • Sign in to reply
  • radiatortwo
    radiatortwo over 11 years ago in reply to schneebutzli

    As Tushar said, you can use the imx_v6_v7_defconfig instead.
    It´s already in the mainline kernel sources.

     

    I really have to update the blogs...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • schneebutzli
    schneebutzli over 11 years ago

    Hi Otto

     

    Could you tell me how you created this file or do you have an alternativ download?

     

    http://radisserver.ddns.net/riotboard/Linux/riot_defconfig 

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tusharp
    tusharp over 11 years ago in reply to e14 Contributor

    try the  imx_v6_v7_defconfig   present in the configs, it should work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hey Otto,

     

    I lost my copy of the riot_defconfig and your website doesn't appear to be up. Could you possibly reupload the file?

     

    Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<