RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Blog Linux on the RIoTBoard Part 3: Debian
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: radiatortwo
  • Date Created: 18 Sep 2014 5:22 PM Date Created
  • Views 1783 views
  • Likes 0 likes
  • Comments 3 comments
Related
Recommended

Linux on the RIoTBoard Part 3: Debian

radiatortwo
radiatortwo
18 Sep 2014

This series of blog posts contains the following parts:

1. The bootloader U-Boot

2. The Kernel

3. Debian Root File System (This part)

4. Flashing with MFGTool in Windows

5. Creating an SDCard Image

 

Part 3: Debian

 

So in this part we´ll create a debian file system completely from scratch.

You´re asking why you should do this, since there are downloadable images?

 

Well the reason I prefer this method is the following:

 

You can download a prebuilt image. But this image is most likely absolutely minimal.

There is nothing installed but the rare minimum so debian can start and work.

If you then use this image on the RIoTBoard you have to install everything directly on the board.

And depending on what you want to install, this can take a really long time.

If you´re installing a bigger desktop for example, this can take several hours.

 

But this method uses an emulator (qemu) to emulate an arm system on your x86 or x64 machine.

With this you can install everything you need right before even putting the image on the RIoTBoard.

And that´s a lot faster than to do this directly on the board.

 

For those who want a minimal image.

You can skip this step and just download one from http://www.armhf.com/

If needed they also have Ubuntu images there.

(Look in the download section for "Root File System")

 

Everyone else can follow these steps.

(Please note that this most likely won´t work on a virtual root server, since the kernels of these don´t provide proper chroot functionality. At least mine didn´t.)

 

Now let´s start.

 

Make sure you´re in the folder where you will save everything like in the previous parts of this series.

In my case:

 

cd /home/riotboard/linux

 

Step 1.

Get the needed packages.

 

apt-get install qemu-user-static debootstrap binfmt-support

 

Step 2.

Set some environment variables for the folder and the distro we want. Then create the directory and download the basic Debian system files.

At this point we only download the package files into the folder we defined.

(The distro used here is Debian "wheezy". In theory you can also use Debian "jessie". But I haven´t tested that at this point.)

 

export targetdir=rootfs
export distro=jessie

mkdir $targetdir
debootstrap --arch=armhf --foreign $distro $targetdir

 

Step 3.

Copy the qemu-arm-static-binary and the resolv.conf from your host into the created system folder.

This is needed so qemu can be startet within that folder.

The resolv.conf is needed, so we know which DNS Server to use because we need an internet connection inside the new system.

Normally it is created over DHCP. But since we haven´t done any network configuration yet, we have to use the same one as the one from the host.

 

cp /usr/bin/qemu-arm-static $targetdir/usr/bin/
cp /etc/resolv.conf $targetdir/etc

 

Step 4.

Now step into the new created system, and start configuring it from the inside.

That´s easily done by just chrooting into the folder.

 

chroot $targetdir

 

Step 5.

In the new rootfs system we need to set some variables again.

 

export distro=jessie
export LANG=C

 

Step 6.

By now we only downloaded the packages. But for installing them we need an ARM cpu.

Since the host is at x86 or x64 that wouldn´t work.

Luckily debootstrap has a function for that called second stage.

 

/debootstrap/debootstrap --second-stage

 

At this point we basically have a fresh fully installed debian system, that can be booted.

But only botting it won´t do much.

We have to configure some more stuff, so we also can use it.

 

Step 7.

We want to install stuff inside the new system over apt.

So we need a sources.list and some other settings

.

Change the locale in the URLs in the following script to the locale you want.

For example instead of http://ftp.de.debian.org/debian you´ll write http://ftp.uk.debian.org/debian for the uk server before executing this command.

 

cat <<EOT > /etc/apt/sources.list
deb http://ftp.de.debian.org/debian $distro main contrib non-free
deb-src http://ftp.de.debian.org/debian $distro main contrib non-free
deb http://ftp.de.debian.org/debian $distro-updates main contrib non-free
deb-src http://ftp.de.debian.org/debian $distro-updates main contrib non-free
deb http://security.debian.org/debian-security $distro/updates main contrib non-free
deb-src http://security.debian.org/debian-security $distro/updates main contrib non-free
EOT

cat <<EOT > /etc/apt/apt.conf.d/71-no-recommends
APT::Install-Recommends "0";
APT::Install-Suggests "0";
EOT

 

Step 8.

Update apt now.

(You´ll get some ignored lines because we didn´t setup the locales by now.)

 

apt-get update

 

Step 9.

Setup the missing locales and update again.

When the dialog comes up, select the locale you want.

I´m using "de_DE.UTF8". (Obviously)

 

apt-get install locales dialog
dpkg-reconfigure locales
apt-get update

 

Step 10.

Set the root password.

Don´t miss this step. Or your image will be useless since you can´t even login.

 

passwd

 

Step 11.

We need a network connection of course.

At this point you can also define wireless connections.

For other configurations, like a fixed IP, just google the how to do that in Linux.

There are a lot of explanations to find on this.

But in my example I only configure DHCP on eth0.

 

echo <<EOT >> /etc/network/interfaces
allow-hotplug eth0
iface eth0 inet dhcp
EOT

 

Step 12.

We need a hostname. (The name the board is reached in the network)

Just change "riotboard" to what you want.

 

echo riotboard > /etc/hostname

 

Step 13. (Obsolete in Debian 8 with Systemd)

Skip this step with Debian Jessie!

We want to access the riotboard over the serial port. (UART connection on J18)

The place to do this is the file "/etc/inittab".

Looking into that file, we find some examples on how to do that.

# Example how to put a getty on a serial line (for a terminal)

#

#T0:23:respawn:/sbin/getty -L ttyS0 9600 vt100

#T1:23:respawn:/sbin/getty -L ttyS1 9600 vt100

    

 

The serial port is accessed through "ttymxc1" and the standard baudrate is 115200.

So we execute this command to insert a line at the end of inittab.

 

echo T0:2345:respawn:/sbin/getty -L ttymxc1 115200 vt100 >> /etc/inittab

 

Step 14.

We now have a fully running minimal image of debian.

At this point you can install everything you want over apt.

And I always advise to install some usefull stuff like this.

 

apt-get install openssh-server ntpdate

 

Now after installing everything here is a little tip to reduce the size of the system.

 

apt-get clean

 

This only removes the downloaded packages for installing everything.

We don´t need them anymore since everything is already installed.

In this case here this reduces the size from around 150 MB to about 89 MB.

 

Step 15.

Now that we configured everything inside the system, we can quit the chroot shell and get back into our hosts shell.

 

exit

 

Step 16.

Because we don´t need to emulate ARM in an ARM system, we remove qemu as well as the resolv.conf we copied earlier into the new system.

 

rm $targetdir/usr/bin/qemu-arm-static
rm $targetdir/etc/resolv.conf

 

Step 17.

Everything we now need to do is just put all the files into a tarball.

So get into the folder and pack everything in a package.

 

By the way:

Notice the parameter p in the tar command. This means the permissions stay like they are on all files and folders inside the new tarball.

This is very important! If you miss that you will have a lot of problems with false set permissions on all system files.

 

cd $targetdir
tar cvzpf oneiric.tgz *

 

Now we have a file called oneiric.tgz.

Copy this file into our output folder where our other stuff is lying, so we find it again.

 

cp oneiric.tgz /home/riotboard/linux/output/oneiric.tgz

 

This file we now can use to flash our system on the board.

 

And that´s it for this part.

In the next part we will be putting everything together to get it running on the board with Windows and MFGTool.

 

Continue with Part 4

  • Sign in to reply
  • e14 Contributor
    e14 Contributor over 11 years ago

    Do you know how i can i install a cross compile toolchain so i can compile natively from this debian ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • radiatortwo
    radiatortwo over 11 years ago in reply to toonamo

    My first experience with Jessie was...

     

    I didn' t try it in the RIoTBoard but I wanted to install a new virtual machine as my build system. Just to geht used to it. With systemd for example. Didn't use that before.


    Installation went fine. But then when installing the Compiler and everything else I had so many dependency errors. I just deleted the vm and now use my wheezy build system again.


    Maybe I should try it again. But at the Moment I don't know why I should.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • toonamo
    toonamo over 11 years ago

    are there any known reasons to not install jessie?