RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Blog RIoTboard: Building a TFT LCD Display and Digitizer - Part 1: Introduction
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 9 Jul 2014 2:44 AM Date Created
  • Views 4396 views
  • Likes 4 likes
  • Comments 19 comments
  • lcd
  • ioe
  • internet_of_everything
  • lvds
  • tft
  • internet_of_things
  • riotboard
  • digitizer
  • iot
Related
Recommended

RIoTboard: Building a TFT LCD Display and Digitizer - Part 1: Introduction

shabaz
shabaz
9 Jul 2014

Part 1: Introduction

(Click here for Part 2).

Thanks so much to doctorcdf and nlarson at element14 for always inspiring me and others, I was very proud to receive two free RIoTboards for a couple of projects. The RIoTboardRIoTboard is one of the latest very low cost single board computers (SBC) with a decent processor capable of running Android or Linux.

 

This first project is to connect it up to a Thin Film Transistor (TFT) LCD display as found on old laptops, with a view to eventually converting it all into a microscope viewer. The RIoTboad has two video output options; HDMI video output for connecting to a TV or monitor, and an interface with low-voltage differential signalling (LVDS) for connecting to TFT LCD panels (i.e. laptop LCD panels!).

 

When I received the RIoTboard, I immediately plugged it into a TV using the HDMI video connector, an Ethernet connector into my router, and then powered up the board. It straight away displayed the Android startup screen and was instantly usable. I was browsing the web immediately, and BBC news website and videos played out-of-the-box. Android runs quite fast on the RIoTboard.

 

After some discussions with the amazing all-round Guru/Oracle (agrahambell ) it was clear the RIoTboard should in theory work with many old laptop LCD displays, and so this project was conceived.

 

For those not wishing to construct their own, there is a pre-built display available that is designed for the RIoTboard. The project described here takes quite some effort (not hard, just some time/patience) and is likely to be no cheaper than a pre-built display. Nevertheless the build-it-yourself approach is documented here. The resultant image quality is good. A 1024x768 display was used, here is a photo of a video being played:

image

 

Here is an example video, showing general snappiness of response and high video quality. Video output was smooth in real life:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

This is what the mock-up looks like! It's not pretty. It is supported by wood and adhesive tape. I just taped the RIoTboard and other parts onto the back of the LCD panel (using the yellow card that you can see for insulation), for verifying functionality. Eventually it will be disassembled and fitted in a nice case. The wood supports and tape are just for testing purposes so that I can access both sides.

image

Here it is from the front, displaying an Android home screen. The coke can is for size comparison:

image

Another video - I think it would make a great music and video player:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Full construction details and circuit diagrams will be in the next post (in the next day or so [part 2 now available by clicking here]). In the meantime, this is what the RIoTboard looks like, it is about half the size of a compact disk case. It is about 120x75mm.

image

image

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 12 years ago +2
    and I think it looks fine on it's wooden stand, stuck together with double sided sticky tape in the best Blue Peter tradition
  • Problemchild
    Problemchild over 12 years ago +2
    Laser cutting of case to follow shortly then Shabaz! !
  • bwelsby
    bwelsby over 12 years ago +1
    Great project, I have a stack of old laptops waiting for something like this. I will get stuck in when I get back from holiday.
  • tusharp
    tusharp over 12 years ago in reply to e14 Contributor

    Discontinuation ... image

     

    No plans of discontinuation of LCD 8000-97c.

    Its the one we are officially supporting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tusharp
    tusharp over 12 years ago in reply to bwelsby

    I can see its available in UK farnell  check here.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to e14 Contributor

    Yes, a higher-res would be interesting. I avoided anything too high-res in case the wiring would not stomach it (since I don't have controlled impedance all the way) but also because I want to exploit a feature of this particular panel which is a digitizer pane (I've not investigated any aspect of that yet though!).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to bwelsby

    It does seem odd that it's been discontinued, especially as it's only recently been added as a RIoTboard accessory both here on the shiny new e14 Design Center and on uk.farnell.com.

    I can only imagine that either it's a mistake, or there's a replacement due soon.

     

    Given it's basically twice the cost of the board for the LCD8000-97C, I've never thought they'd sell many for use with the RIoT anyway. tusharp any idea what's going through their minds?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bwelsby
    bwelsby over 12 years ago in reply to e14 Contributor

    I have had problems getting Android working on my HDMI monitor which works fine with Linux, I have tried all resolutions in the "bootargs" but timings are off.

    I also just noticed that the LCD8000-97C is flagged as obsolete and no longer stocked at Farnell in the UK.   Still available as US stock but much more expensive £115.11 + shipping ( £15.95) + VAT  was  £97.73 + VAT

    Definitely time to dig out the old laptops.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>