RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Blog RIoTboard: Building a TFT LCD Display and Digitizer - Part 1: Introduction
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 9 Jul 2014 2:44 AM Date Created
  • Views 4459 views
  • Likes 4 likes
  • Comments 19 comments
  • lcd
  • ioe
  • internet_of_everything
  • lvds
  • tft
  • internet_of_things
  • riotboard
  • digitizer
  • iot
Related
Recommended

RIoTboard: Building a TFT LCD Display and Digitizer - Part 1: Introduction

shabaz
shabaz
9 Jul 2014

Part 1: Introduction

(Click here for Part 2).

Thanks so much to doctorcdf and nlarson at element14 for always inspiring me and others, I was very proud to receive two free RIoTboards for a couple of projects. The RIoTboardRIoTboard is one of the latest very low cost single board computers (SBC) with a decent processor capable of running Android or Linux.

 

This first project is to connect it up to a Thin Film Transistor (TFT) LCD display as found on old laptops, with a view to eventually converting it all into a microscope viewer. The RIoTboad has two video output options; HDMI video output for connecting to a TV or monitor, and an interface with low-voltage differential signalling (LVDS) for connecting to TFT LCD panels (i.e. laptop LCD panels!).

 

When I received the RIoTboard, I immediately plugged it into a TV using the HDMI video connector, an Ethernet connector into my router, and then powered up the board. It straight away displayed the Android startup screen and was instantly usable. I was browsing the web immediately, and BBC news website and videos played out-of-the-box. Android runs quite fast on the RIoTboard.

 

After some discussions with the amazing all-round Guru/Oracle (agrahambell ) it was clear the RIoTboard should in theory work with many old laptop LCD displays, and so this project was conceived.

 

For those not wishing to construct their own, there is a pre-built display available that is designed for the RIoTboard. The project described here takes quite some effort (not hard, just some time/patience) and is likely to be no cheaper than a pre-built display. Nevertheless the build-it-yourself approach is documented here. The resultant image quality is good. A 1024x768 display was used, here is a photo of a video being played:

image

 

Here is an example video, showing general snappiness of response and high video quality. Video output was smooth in real life:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

This is what the mock-up looks like! It's not pretty. It is supported by wood and adhesive tape. I just taped the RIoTboard and other parts onto the back of the LCD panel (using the yellow card that you can see for insulation), for verifying functionality. Eventually it will be disassembled and fitted in a nice case. The wood supports and tape are just for testing purposes so that I can access both sides.

image

Here it is from the front, displaying an Android home screen. The coke can is for size comparison:

image

Another video - I think it would make a great music and video player:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Full construction details and circuit diagrams will be in the next post (in the next day or so [part 2 now available by clicking here]). In the meantime, this is what the RIoTboard looks like, it is about half the size of a compact disk case. It is about 120x75mm.

image

image

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 12 years ago +2
    and I think it looks fine on it's wooden stand, stuck together with double sided sticky tape in the best Blue Peter tradition
  • Problemchild
    Problemchild over 12 years ago +2
    Laser cutting of case to follow shortly then Shabaz! !
  • bwelsby
    bwelsby over 12 years ago +1
    Great project, I have a stack of old laptops waiting for something like this. I will get stuck in when I get back from holiday.
  • tusharp
    tusharp over 12 years ago in reply to bwelsby

    the product is currently unavailable in UK stock, we have stock only in US as of now.

    a bug might have replaced Out of Stock with Obsolete image.

     

    will notify web dev team on this .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to shabaz

    I see the Laptops that have the display that Shabaz used (Thinkpad X41) are available from Ebay for £50 ish. Another way of getting the Spares!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to DAB

    Hi DAB,

     

    Oh! That's unfortunate about the tablet. Hopefully the rear of the LCD panel will have a model number, there is a possibility that a datasheet can be found on the Internet for it, to confirm if it is likely to work.

     

    A good thing about the RIoTboard is that it is ready-to-go out of the box (for Android) - just plug in HDMI, a keyboard/mouse, and power (and Ethernet to access stuff). It's a nice user experience. I placed some music/video files onto a microSD and it detected it fine and played them, so this was great.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago

    I have been eyeing a dead tablet that I bought.

    My wife plugged in the wrong power cord and blasted the charging circuit, but the display should be fine.

     

    Definitely on my to do list once I get the RioT board up and running.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bwelsby
    bwelsby over 12 years ago in reply to tusharp

     

    tushar panda wrote:

     

    I can see its available in UK farnell  check here.

    Yes that's the US stock with added shipping charges.

    FYI if I go to the E14 site here RIoTboardand click on the BUY NOW link for LCD8000-97C  I get this pop-up

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>