RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Blog RIoTboard: Building a TFT LCD Display and Digitizer - Part 1: Introduction
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: shabaz
  • Date Created: 9 Jul 2014 2:44 AM Date Created
  • Views 4391 views
  • Likes 4 likes
  • Comments 19 comments
  • lcd
  • ioe
  • internet_of_everything
  • lvds
  • tft
  • internet_of_things
  • riotboard
  • digitizer
  • iot
Related
Recommended

RIoTboard: Building a TFT LCD Display and Digitizer - Part 1: Introduction

shabaz
shabaz
9 Jul 2014

Part 1: Introduction

(Click here for Part 2).

Thanks so much to doctorcdf and nlarson at element14 for always inspiring me and others, I was very proud to receive two free RIoTboards for a couple of projects. The RIoTboardRIoTboard is one of the latest very low cost single board computers (SBC) with a decent processor capable of running Android or Linux.

 

This first project is to connect it up to a Thin Film Transistor (TFT) LCD display as found on old laptops, with a view to eventually converting it all into a microscope viewer. The RIoTboad has two video output options; HDMI video output for connecting to a TV or monitor, and an interface with low-voltage differential signalling (LVDS) for connecting to TFT LCD panels (i.e. laptop LCD panels!).

 

When I received the RIoTboard, I immediately plugged it into a TV using the HDMI video connector, an Ethernet connector into my router, and then powered up the board. It straight away displayed the Android startup screen and was instantly usable. I was browsing the web immediately, and BBC news website and videos played out-of-the-box. Android runs quite fast on the RIoTboard.

 

After some discussions with the amazing all-round Guru/Oracle (agrahambell ) it was clear the RIoTboard should in theory work with many old laptop LCD displays, and so this project was conceived.

 

For those not wishing to construct their own, there is a pre-built display available that is designed for the RIoTboard. The project described here takes quite some effort (not hard, just some time/patience) and is likely to be no cheaper than a pre-built display. Nevertheless the build-it-yourself approach is documented here. The resultant image quality is good. A 1024x768 display was used, here is a photo of a video being played:

image

 

Here is an example video, showing general snappiness of response and high video quality. Video output was smooth in real life:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

This is what the mock-up looks like! It's not pretty. It is supported by wood and adhesive tape. I just taped the RIoTboard and other parts onto the back of the LCD panel (using the yellow card that you can see for insulation), for verifying functionality. Eventually it will be disassembled and fitted in a nice case. The wood supports and tape are just for testing purposes so that I can access both sides.

image

Here it is from the front, displaying an Android home screen. The coke can is for size comparison:

image

Another video - I think it would make a great music and video player:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Full construction details and circuit diagrams will be in the next post (in the next day or so [part 2 now available by clicking here]). In the meantime, this is what the RIoTboard looks like, it is about half the size of a compact disk case. It is about 120x75mm.

image

image

  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 12 years ago +2
    and I think it looks fine on it's wooden stand, stuck together with double sided sticky tape in the best Blue Peter tradition
  • Problemchild
    Problemchild over 12 years ago +2
    Laser cutting of case to follow shortly then Shabaz! !
  • bwelsby
    bwelsby over 12 years ago +1
    Great project, I have a stack of old laptops waiting for something like this. I will get stuck in when I get back from holiday.
  • shabaz
    shabaz over 12 years ago in reply to e14 Contributor

    I did the same thing, I purchased a mini-HDMI cable but couldn't quite bring myself to cut it : ) In the end I made a custom breakout PCB, one end to be soldered to a mini-HDMI plug, and the other end to accept wires. I also needed to create an breakout board at the LCD panel end too. What kind of connector is on your LCD panel? Mine had a HIROSE connector, which while of large pitch (1mm), was difficult to use a plug with, because I didn't have any crimp tool that can do such tiny crimps. So, I was forced to create a breakout board. For the wires in-between, I used the insides of a SATA cable (Ethernet is also a possibility but I didn't try it).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bwelsby
    bwelsby over 12 years ago

    Great project, I have a stack of old laptops waiting for something like this.  I will get stuck in when I get back from holiday.

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    and I think it looks fine on it's wooden stand, stuck together with double sided sticky tape in the best Blue Peter tradition image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    aarrgghh.....   you beat me to it image

     

    Where did you get the mini-hdmi adapter board I see connected to the riot board in the photo ?   I'd bought a normal mini-hdmi cable with the intention of butchering it to use for this, but an adapter like that could be a better idea..  The display I have is also a 1024x768 and seems to only use a single link, however another slightly newer 1024x768 seems to want a dual-link. So while it'll certainly be possible with some panels, I'm no longer sure the necessary panels will be quite as common as I originally thought.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<