RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Blog RioTboard Power Consumption
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 23 Jun 2014 7:33 PM Date Created
  • Views 977 views
  • Likes 0 likes
  • Comments 3 comments
Related
Recommended

RioTboard Power Consumption

e14 Contributor
e14 Contributor
23 Jun 2014

Does anyone know the typical power consumption of the RioTboard? 

  • Sign in to reply
  • dragonstyne
    dragonstyne over 12 years ago in reply to e14 Contributor

    The board itself without any other connected devices consumes about 600ma. When you add additional peripherals and accessories, it goes up from there. Which is what selsnork was telling you.

     

    Regards.

    -Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Those are very useful meaningless numbers.  Thanks Selsinork...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    Can I start by suggesting posting a discussion rather than a blog post. Blog posts tend to be less visible here, so often less likely to get you any answers.

     

    Anyhow...  'Typical' is an almost meaningless starting point, without knowing what it'll be doing, what peripherals you'll have connected etc. it's an almost impossible question to answer. So here's some meaningless numbers to give you some idea:

     

    linux, 3.15 kernel, cli only, idle, no peripherals, no network, ~180mA

    as above, with gigabit network connection, ~250mA

    adding HDMI monitor, 395mA

    as above with a task running (time echo "scale=2000;4*a(1)" | bc -l), ~520mA

     

    debian with no peripherals attached other than a usb wifi adapter, approx 410mA....   410-180 gives 230mA for the wifi adapter alone!

     

    android with lvds display, up to 850mA during boot, 660mA at lock screen

    adding gigabit network connection, ~720mA

    with activity and the lvds display I can get android up to just over 1A, disconnecting the display sees a drop of approx 450mA

     

    So with a range from 180mA right up to 1A, what do you think is 'typical' ?