RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Blog Riotboard webserver : Part2 - Monitering Temperature with Xtrinsic Sensor
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: tusharp
  • Date Created: 27 Aug 2014 2:35 PM Date Created
  • Views 1286 views
  • Likes 1 like
  • Comments 2 comments
  • tusharp
  • Ubuntu
  • mpl3115
  • freescale
  • imx6
  • temperature
  • riotboard
  • embedded
  • xtrinsic
  • cortex-a9
  • bsp
  • arm9
  • sensor
  • linux
Related
Recommended

Riotboard webserver : Part2 - Monitering Temperature with Xtrinsic Sensor

tusharp
tusharp
27 Aug 2014

Contents:

Part1: Environment Setup

Part2: Monitering Temperature with Xtrinsic Sensor   <-- You are here

Part3: Capture sensor data to database ..

Part4: Remote datalogger

 

Once done with webserver i was looking out to measure temperature.

I found one xtrinsic sensor from a previous setup.

The  Xtrinsic sensorXtrinsic sensor  is available in community and has good support freescale MCUs.

2lvd30h.jpg

Its an overkill image  to use xtrinsic for just temperature, but i thought to give it a try.

 

In fact its not an overkill, the Sensor board comes with multiple sensing stuff

MPL3115A2  - high-precision sensor used to provide accurate pressure and altitude data

MAG3110     - small, low-power, digital 3-axis magnetometer

MMA8491Q  - low voltage, 3-axis low-g accelerometer

 

 

Setting up the Hardware

 

Lets start with the pin mapping of Xtrinsic and Riotboard.

For this setup we need 7 pins in Xtrinsic to be connected to Riotboard .

 

Pin Mapping

2rf4p75.jpg

I am using Male-to-Female jumpers to connect Pins in Riotboard Expansion connector to Xtrinsic.

We will be bypassing the breadboard connection stuff to keep this simple.

 

Connecting female headers in Xtrinsic CN2 Connector.

 

2gwhxxi.jpg


Connecting female headers in CN1 Connector.

2iac3v7.jpg

 

 

Connecting Male headers in Riotboard (J13)

id56wx.jpg

 

1628guh.jpg


My setup looks something like this ..

fjdys5.jpg


I wrote a small user-space driver  to access the temperature sensor.

 

 

#include <stdio.h>
#include <stdint.h>
#include <linux/i2c.h>
#include <linux/i2c-dev.h>
#include <fcntl.h>
#include <stdlib.h>
#include <unistd.h>
#include <sys/ioctl.h>
#include <string.h>

static int write_register(int file,unsigned char address,unsigned char reg,unsigned char data)
{

   unsigned char output_buffer[2];
   struct i2c_rdwr_ioctl_data packets;
   struct i2c_msg messages[1];

    messages[0].addr  = address;
    messages[0].flags = 0;
    messages[0].len   = sizeof(output_buffer);
    messages[0].buf   = output_buffer;

    output_buffer[0] = reg;
    output_buffer[1] = data;

    packets.msgs  = messages;
    packets.nmsgs = 1;

    if(ioctl(file, I2C_RDWR, &packets) < 0) {
        perror("Error sending data");
        return 1;
    }

    return 0;
}


static int read_register(int file, unsigned char address, unsigned char reg, unsigned char *data)
{
    unsigned char input_buffer, output_buffer;
    struct i2c_rdwr_ioctl_data packets;
    struct i2c_msg messages[2];


    output_buffer = reg;
    messages[0].addr  = address;
    messages[0].flags = 0;
    messages[0].len   = sizeof(output_buffer);
    messages[0].buf   = &output_buffer;

    messages[1].addr  = address;
    messages[1].flags = I2C_M_RD;
    messages[1].len   = sizeof(input_buffer);
    messages[1].buf   = &input_buffer;


    packets.msgs      = messages;
    packets.nmsgs     = 2;
    if(ioctl(file, I2C_RDWR, &packets) < 0) {
        perror("Error sending data");
        return 1;
    }
    *data = input_buffer;

    return 0;
}


int main() {
    int file, i;
    unsigned char data;
    int val1;
    int val2;
    int t_m;
    int choice;
    int DBG_ENABLE = 0;
    char string[200];

printf("Enable Debugging [1-Enable/0-Disable] :");
scanf("%d",&choice);

    if (choice == 1)
        DBG_ENABLE = 1;
    else if (choice == 0)
        DBG_ENABLE = 0;
    else
        {
            printf("Unknown choice \n Exiting... \n");
            exit(1);
        }

if ((file = open("/dev/i2c-3", O_RDWR)) < 0)
{
    perror("Error openning file!");
    exit(1);
  }

if(DBG_ENABLE == 0)
printf("Debugging Disabled \n");
else if(DBG_ENABLE == 1)
printf("Debugging Enabled \n");
else
printf("No idea");


//0x0C who_am_i , factory programmed device id
   if(read_register(file, 0x60, 0x0C, &data))
    exit(1);
   else
   {
    if(DBG_ENABLE == 1)
     { printf("GET:Register[0x%02X]: 0x%02X\n" , 12 , data);
     }
   }
//0x26 set ctrlreg1 ACTIVE
   if(read_register(file, 0x60, 0x26, &data))
      exit(1);
   else
   {
    if(DBG_ENABLE == 1)
     { printf("GET:Register[0x%02X]: 0x%02X\n" , 38 , data);
     }
   }


   if(write_register(file, 0x60, 0x26, 0x03))
     exit(1);
   else
     {
        if(read_register(file, 0x60, 0x26, &data))
           exit(1);
        else
       {
    if(DBG_ENABLE == 1)
        {  printf("SET/GET:Register[0x%02X]: 0x%02X\n" , 38 , data);
        }
       }

     }

while(1)
{
//read temperature MSB/LSB
   if(read_register(file, 0x60, 0x04, &data))
     exit(1);
   else
    { if(DBG_ENABLE == 1)
        {   printf("Register[0x%02X]: 0x%02X\n" , 4 , data);
        }
    }

        val2 = (int)data;
        if(DBG_ENABLE == 1) printf("val2: initial :%d:\n",val2);
        val2 <<=8;
        if(DBG_ENABLE == 1) printf("val2: shift :%d:\n",val2);


   if(read_register(file, 0x60, 0x05, &data))
    exit(1);
   else
   {
     if(DBG_ENABLE == 1)
     printf("Register[0x%02X]: 0x%02X\n" , 5 , data);
   }

    val2 = val2+ (int)data;

    if(DBG_ENABLE == 1)
    { printf("val2 :%d:\n",val2);
    }

    t_m = (val2 >> 8) & 0xff;

   printf("temperature :%d: \n",t_m);

  system(string);


   sleep(1);
}
    close(file);
    return 0;
}

 

A delay of 1 sec has been introduced to prevent ouput msgs flooding terminal window .

 

Compiling the program :

On Riotboard:

gcc xtrinsic_temp.c -o xtrinsic_temp

 

 

On PC:

<PATH_TO_TOOLCHAIN>/fsl-linaro-toolchain/bin/arm-fsl-linux-gnueabi-gcc xtrinsic_temp.c -o xtrinsic_temp

 

 

There are two ways to use the program:

1. Get Temperature as only output.

2. Enable debug to check register values (Just for fun) image..

 

Once Compiled we will execute . To access a device file "/dev/i2c-3" (check line 92 above ) we need to be root.

# ./xtrinsic_temp

 

It will ask for debug option.

Enter 0 to disable debugging  (recommended)

28v93d0.jpg

 

Enter 1 to enable debugging.

1zv4sqe.jpg

 

 

 

Ok seems like we got the setup right image

 

Testing a bit more.

 

We need :

  1. something very hot (I got a Soldering Iron)
  2. above setup

 

Identify the MPL3115 Sensor ( U1 - at centre of board)

5k29gj.jpg

 

Power on the Solder Iron and place near the MPL3115 Sensor

 

You can see a rapid rise in the Temperature

 

[Click on below pic to see temp rise]

image

 

So we completed integration of xtrinsic temperature sensor with Riotboard

Next time we shall see how to capture sensor data in a database.

  • Sign in to reply
  • mcb1
    mcb1 over 12 years ago

    Thanks for the informative post.

    A1 use of animated GIF.  image

     

     

    mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago

    Good post and display of connecting devices to the RioT board.

     

    DAB