RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Blog Riotboard Yocto  : Part2 : Build u-boot using Yocto
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: tusharp
  • Date Created: 24 Sep 2014 3:48 PM Date Created
  • Views 3784 views
  • Likes 0 likes
  • Comments 0 comments
  • tusharp
  • Ubuntu
  • yocto
  • uboot
  • image
  • bitbake
  • freescale
  • imx6
  • riotboard
  • setup
  • riot
  • cortex-a9
  • poky
  • bsp
  • arm
  • linux
Related
Recommended

Riotboard Yocto  : Part2 : Build u-boot using Yocto

tusharp
tusharp
24 Sep 2014

Contents:

Part1 : Environment setup and initial build
Part2 : Build u-boot using Yocto     <-- You are here
Part3 : Build Kernel using Yocto
Part4 : Package Development using Yocto
Part5 : Application Development using ADT


In the previous blog we have build & flashed a basic sdcard image and booted with Riotboard.

 

In this blog we shall manually fetch, configure, compile and build uboot using yocto bitbake tool .

 

Setting up yocto for Riotboard:

~$ cd fsl-arm-yocto-bsp

~/fsl-arm-yocto-bsp$  MACHINE=riotboard source fsl-setup-release.sh -b build -e fb

~/fsl-arm-yocto-bsp/build$

 

Checking for the available uboot recipes:

~/fsl-arm-yocto-bsp/build$ bitbake -s | grep  u-boot

24vtdhh.jpg

we will be using the last one u-boot-riotboard  (2013.04)

 

 

 

Bootloader source directory:
build/tmp/work/riotboard-poky-linux-gnueabi/u-boot-riotboard/2013.04-r0/git

 

Locating source directory through bitbake, this command can be used to locate source directory for other recipes also.

It will open the recipe source directory in a new terminal window with yocto variables defined.

~/fsl-arm-yocto-bsp/build$ bitbake -c devshell u-boot-riotboard


mhg7e0.jpg

 

 

Bootloader recipe location:
sources/meta-fsl-arm-extra/recipes-bsp/u-boot/u-boot-riotboard_2013.04.bb

14e5q3c.jpg

 

 

Lets build...

 

Clean up the previous build (if any)

~/fsl-arm-yocto-bsp/build$ bitbake u-boot-riotboard -c clean -f

This will remove everything (except log directory - temp) from the uboot build directory.

It is necessary as we want to have a fresh build from source.

 

Fetch uboot from source:

~/fsl-arm-yocto-bsp/build$ bitbake u-boot-riotboard -c fetch

The Riotboard has mainline uboot support.
So we can customise the recipe (check SRC_URI & bbappend in yocto) and get the latest support from mainline uboot.

If you are planning to modify uboot, Yocto has details steps for patching new recipes, check here.

 

 

Compiling uboot:

~/fsl-arm-yocto-bsp/build$ bitbake u-boot-riotboard -c compile

This will generate u-boot.imx file here :
/tmp/work/riotboard-poky-linux-gnueabi/u-boot-riotboard/2013.04-r0/image/boot

 

 

Deploy u-boot image files:

~/fsl-arm-yocto-bsp/build$ bitbake u-boot-riotboard -c deploy

This will make u-boot.imx available in deploy directories to be bundled with sdcard image.

 

If you get something like below but still want to rebuild it, force a rebuild by adding -f  to above commands.

104onf9.jpg

 

You can directly build the uboot directly and may not need above manual steps.

~/fsl-arm-yocto-bsp/build$ bitbake u-boot-riotboard -c deploy

 

After build procedure completed you will get uboot image in deploy/images folder.

2mq3sxz.jpg

 

I hope the above gives fair idea into the yocto recipe & directories and shows how a package (like uboot) is manually build.

Next time we shall see how the kernel is setup, build , configure and patched using yocto.