RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Blog Upgrading RIoTboard with Yocto BSP and Kernel 3.10.17 (Linux Host)
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: tusharp
  • Date Created: 31 Jul 2014 2:34 PM Date Created
  • Views 3818 views
  • Likes 1 like
  • Comments 17 comments
  • tusharp
  • Ubuntu
  • kernel3.10
  • freescale
  • imx6
  • rootfs
  • mx-6
  • riotboard
  • embedded
  • riot
  • root
  • cortex-a9
  • bsp
  • mx-6s
  • glossary
  • arm
  • arm9
  • linux
Related
Recommended

Upgrading RIoTboard with Yocto BSP and Kernel 3.10.17 (Linux Host)

tusharp
tusharp
31 Jul 2014

Announcing the availability of an updated 3.10.17 kernel for RIoTboard.It has been available for quite some time in github repository.

https://github.com/embest-tech/linux-imx/tree/embest_imx_3.10.17_1.0.0_ga

 

The release has been in sync with official i.MX releases.

 

All the commits can be found in the repository providing support for LCD and other accessories.

 

We made our major release on this heavily tested and optimised kernel which carries number of advancements over the older releases.

With new kernel we get the most sought feature, the Device Tree, which contributes to smaller amount of BSP code to merge and greater ability to customise physical devices on new boards.

 

To setup we need to download a SDCARD image with an updated kernel first.

The updated kernel source can be found here.

 

We will be downloading the fsl-image-fb-riotboard.sdcard image.

https://www.dropbox.com/sh/8ebbtcork0l2cua/AACH4U7ovJYIJvge1VLdWueJa/image.rar

 

image

The SVN2652 has

 

Image NameDescription

fsl-image-fb-riotboard.sdcard

SDCARD image for RIoTboard

fsl-image-fb-riotboard.tar.bz2

Root File System bundle.

imx6solo_RIoTboard.dtb

Device Tree Binary

u-boot.imx

Bootloader

uImage3.10.17 kernel

 

 

First we need to detect the memory device.

I am using in built-in SDCARD adapter in my laptop and it shows SD card as mmcblk device.

 

# ll /dev/mmc*

brw-rw---- 1 root disk 179, 0 Jul 29 17:19 /dev/mmcblk0

 

Using a USB-SD adapter shows a sdb device .

 

 

image

 

# ll /dev/sd*

brw-rw---- 1 root disk 8, 0 Jul 29 11:26 /dev/sda

brw-rw---- 1 root disk 8, 3 Jul 29 11:26 /dev/sda3

brw-rw---- 1 root disk 8, 5 Jul 29 11:26 /dev/sda5

brw-rw---- 1 root disk 8, 6 Jul 29 11:26 /dev/sda6

brw-rw---- 1 root disk 8, 7 Jul 29 11:26 /dev/sda7

brw-rw---- 1 root disk 8, 8 Jul 29 11:26 /dev/sda8

brw-rw---- 1 root disk 8, 16 Jul 29 16:45 /dev/sdb

 

 

CAUTION: Most Linux machines shows harddisk as sda. Our device will be mostly something like sdb,sdc ....

                       We will be carefully selecting our device so that we don't wipe out our SDA harddisk partition

 

to confirm our device name, plug in and plug out the card reader and execute the command ( ll /dev/sd* )  to determine the device number.

 

If the device is mounted by default , manually unmount the device  before proceeding.

 

# umount /dev/sdb

 

Once we have completed the device detection , we will use below command to setup a kernel 3.10.17 based bootable sdcard.

 

# sudo dd if=fsl-image-fb-riotboard.sdcard of=/dev/sdX bs=1M

      (where sdX is the detected sdcard device)

 

Once the command completes, power down the card, remove it, plug it into J6 of RIoTboard and power on the board.

 

Make sure the boot switch are in SDCARD mode before powering on.

2a4xxlx.jpg

 

1111gz9.jpg

 

Once Powered on it will boot with Kernel 3.10.17.

You will see a boot log as below:

U-Boot 2013.04 (Jul 04 2014 - 09:45:23)

 

CPU:   Freescale i.MX6SOLO rev1.1 at 792 MHz

CPU:   Temperature 42 C, calibration data: 0x5a151a5f

Reset cause: POR

Board: MX6SOLO RIoTboard

I2C:   ready

DRAM:  1 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

*** Warning - bad CRC, using default environment

 

No panel detected: default to HDMI

Display: HDMI (640x480)

In:    serial

Out:   serial

Err:   serial

mmc0 is current device

Net:   FEC [PRIME]

Warning: failed to set MAC address

 

Normal Boot

Hit any key to stop autoboot:  0

mmc0 is current device

reading boot.scr

** Unable to read file boot.scr **

reading uImage

5275824 bytes read in 250 ms (20.1 MiB/s)

Booting from mmc ...

reading imx6solo_RIoTboard.dtb

43553 bytes read in 21 ms (2 MiB/s)

## Booting kernel from Legacy Image at 12000000 ...

   Image Name:   Linux-3.10.17_1.0.0_RIoTboard+g1

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    5275760 Bytes = 5 MiB

   Load Address: 10008000

   Entry Point:  10008000

   Verifying Checksum ... OK

## Flattened Device Tree blob at 18000000

   Booting using the fdt blob at 0x18000000

   Loading Kernel Image ... OK

OK

   Using Device Tree in place at 18000000, end 1800da20

 

Starting kernel ...

 

 

It will stop at login promt

riotboard login:

Enter root as the username , no password is required.

 

riotboard login: root

root@riotboard:~#

 

Verifying the kernel version details:

root@riotboard:~# uname -a

 

Linux riotboard 3.10.17_1.0.0_RIoTboard+g14571fa #1 SMP PREEMPT Fri Jul 4 09:49:22 CST 2014 armv7l GNU/Linux


So we got an updated 3.10 kernel for RIoTboard .


A video guide :

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image



  • Sign in to reply
  • tusharp
    tusharp over 10 years ago in reply to e14 Contributor
    I have tried svn3000 image also..but apt-get and gcc wont work with this..

    This is not a debian distro so no apt-get present.

     

    plz go through yocto project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to tusharp

    thanks Tushar sir,

     

    I have tried svn3000 image also..but apt-get and gcc wont work with this..

    wat should i do so that i will be able to run USB uvccapture program on riotboard.

     

    For the yocto project, i will study the documentation and try to work accordingly.

     

    Regards,

    Rashmi

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tusharp
    tusharp over 10 years ago in reply to e14 Contributor
    is there any way to upgrade the linaro image 2591

     

    linaro 2591 is not hardware accelerated so GUI will be slow and camera mostly won't work.

    yocto svn3000 supports hardware acceleration for display and camera works perfect, check this blog.

     

    also pls tell me the difference between yocto and ubuntu images, as I am new to this field.

    yocto is build framework that builds uboot,kernel and packages all from source.

    ubuntu/debian are OS when it comes to PC but root file systems when it comes to embedded.

     

    yocto will build everything(uboot,kernel & libraries - except gpu binaries) from scratch  while ubuntu can be used along with a standalone kernel & rootfs to form a BSP.

     

    not sure if my above "3 lines of yocto documentation" have helped much but this will definitely help you.

     

     

    Thanks

    Tushar

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago
    Hello Tusharp,

     

     

    I want to know is there any way to upgrade the linaro image 2591 which i downloaded. because this particular image is having apt-get and gcc installed and also it is allowing my board to boot successfully.

     

    As i want to use a usb camera and do image capture and also do video streaming with this board, kindly help me. I have tried to build images from several ways from last 2-3 months but of no use.

     

    also pls tell me the difference between yocto and ubuntu images, as I am new to this field.

    Regards,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to tusharp

    I tried with SVN3000 and as as the image linked on this page.

    With both I get no signal on HDMI on my tv screen - I am going to try it with another screen when I have time.

     

    Apart from that - why are there android parameters in your boot args ( androidboot.console=ttymxc1 androidboot.hardware=freescale)?

    Is that a typo?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>