RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Linux : Where is UART's
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 25 subscribers
  • Views 2994 views
  • Users 0 members are here
Related

Linux : Where is UART's

e14 Contributor
e14 Contributor over 12 years ago

Hi,

I have installed Linux in the RiotBoard.

i would like use UART's in Expansion Port (UART3, UART4 and UART5)

 

I have found :

- UART3 on / dev/ttymxc2

- Debug port on /dev/ttymxc1

 

I don't know where is connected /dev/ttymxc0 and search others Serial port : UART4 & 5

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hello,

     

    Today I was trying to connect my two RS485 to RiotBoard but I'm stuck were you are. I was able to connect one RS485 to UART3 (ttymxc2), but I can't see UART4 & 5 and ttymxc0 seems to be not connect to neither of them.

     

    In dmesg is just this about Serial IMX drivers:

    Serial: IMX driver
    imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
    imx-uart.1: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX
    console [ttymxc1] enabled, bootconsole disabled
    console [ttymxc1] enabled, bootconsole disabled
    imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX

     

    So if anyone knows how to make it working I will be very glad.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago

    Hello,

     

    Today I was trying to connect my two RS485 to RiotBoard but I'm stuck were you are. I was able to connect one RS485 to UART3 (ttymxc2), but I can't see UART4 & 5 and ttymxc0 seems to be not connect to neither of them.

     

    In dmesg is just this about Serial IMX drivers:

    Serial: IMX driver
    imx-uart.0: ttymxc0 at MMIO 0x2020000 (irq = 58) is a IMX
    imx-uart.1: ttymxc1 at MMIO 0x21e8000 (irq = 59) is a IMX
    console [ttymxc1] enabled, bootconsole disabled
    console [ttymxc1] enabled, bootconsole disabled
    imx-uart.2: ttymxc2 at MMIO 0x21ec000 (irq = 60) is a IMX

     

    So if anyone knows how to make it working I will be very glad.