RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Linux : Where is UART's
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 25 subscribers
  • Views 2994 views
  • Users 0 members are here
Related

Linux : Where is UART's

e14 Contributor
e14 Contributor over 12 years ago

Hi,

I have installed Linux in the RiotBoard.

i would like use UART's in Expansion Port (UART3, UART4 and UART5)

 

I have found :

- UART3 on / dev/ttymxc2

- Debug port on /dev/ttymxc1

 

I don't know where is connected /dev/ttymxc0 and search others Serial port : UART4 & 5

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    I'm interested in the UARTS myself.  I need RS232 support with CTS,RTS,DCD,and DTR.  Are these UARTS TTL or RS232 levels?  Is there support for the hardware control signals?

     

    Thanks,

    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    i don't found support with CTS,RTS,DCD,and DTR (maybe by GPIO)

     

    however, I can confirm that the signal level is TTL for all UART

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Hello,

     

    Finaly I foud a solution to make UART 4&5 working.

    I will try to write simple guide, how to achieve that.

     

    Thanks to xizhou wang I was able to find the way how to do that.

     

    1. In schematics http://www.element14.com/community/servlet/JiveServlet/previewBody/65504-102-1-287949/RIoTboard_Schematics.pdf on page 8 you can find how the UART 4&5 are pinned.  

     

    So in file /linux-imx/arch/arm/mach-mx6/board-mx6dl_riot.h you have to add UART4&5

     

    #if 0
            /* UART1 for debug */
            MX6DL_PAD_CSI0_DAT10__UART1_TXD,
            MX6DL_PAD_CSI0_DAT11__UART1_RXD,
    #else
            /* UART2 for debug */
            MX6DL_PAD_EIM_D26__UART2_TXD,
            MX6DL_PAD_EIM_D27__UART2_RXD,
    #endif
            /* UART3 */
            MX6DL_PAD_EIM_D24__UART3_TXD,
            MX6DL_PAD_EIM_D25__UART3_RXD,
    
            /********************** ADDED ***********************/
            /* UART4 */
            MX6DL_PAD_KEY_COL0__UART4_TXD,
            MX6DL_PAD_KEY_ROW0__UART4_RXD,
    
            /* UART5 */
            MX6DL_PAD_KEY_COL1__UART5_TXD,
            MX6DL_PAD_KEY_ROW1__UART5_RXD,
            /***************************************************/

           

    2. Then in /linux-imx/arch/arm/mach-mx6/board-mx6q_riot.c you have to initialize UART 4&5

     

    static inline void mx6q_riot_init_uart(void)
    {
            imx6q_add_imx_uart(0, NULL);
            imx6q_add_imx_uart(1, NULL);
            imx6q_add_imx_uart(2, NULL);
             
    /********************** ADDED ***********************/
            imx6q_add_imx_uart(3, NULL);
            imx6q_add_imx_uart(4, NULL);
    /***************************************************/
    }

     

    And now you have to recompile the kernel and flash it to your RiotBoard.

    After that you will have:

     

    /dev/ttymxc0 - still don't know what is for image

    /dev/ttymxc1 - debug serial port

    /dev/ttymxc2 - UART3

    /dev/ttymxc3 - UART4

    /dev/ttymxc4 - UART5

     

    Hope it will help

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Marek Czudek wrote:

     

    /dev/ttymxc0 - still don't know what is for

    it's hooked up to the OpenSDA debugger via U26 on p20 of the schematics.  Some info on OpenSDA is available here https://www.pemicro.com/opensda/ and the user guide http://cache.freescale.com/files/32bit/doc/user_guide/OPENSDAUG.pdf

     

    It's briefly mentioned on p33 of the user manual with the note at the bottom of the page that says

    The RIoTboard has hardware to support Freescale’s OpenSDA interface. Currently this

    interface has not been enabled in software

    so apparently ttymxc0 is unusable as the OpenSDA hardware appears to be the only way to get to it and for some unknown reason it has no software support.

     

    Indeed, following the instructions from the OpenSDA user manual gets no response. No usb storage device appears. You'd have to assume therefore that whatever firmware is supposed to be loaded onto the Kinetis K20 is missing.  Only a guess, but loading it may take jtag onto the un-populated J17.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    do you have tutorial to rebuild kernel linux for riotboard  ? or just image binary file included UART 4 & 5 ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • radiatortwo
    radiatortwo over 12 years ago in reply to e14 Contributor

    Here is how I compiled the older RiotBoard Kernel from the git Repo. Everthing done in a Debian Virtual Machine.

    I don´t use the toolchain from the repos. because of that you have to install some essential stuff.

     

    apt-get install git build-essential fakeroot kernel-package u-boot-tools zlib1g-dev libncurses5-dev

     

    To get the gcc compiler with armhf put this line into /etc/apt/sources.list

    deb http://www.emdebian.org/debian/ unstable main

     

    Then type the following commands:

    apt-get update
    apt-get install emdebian-archive-keyring
    apt-get update
    apt-get install gcc-4.7-arm-linux-gnueabihf
    ln -sf `which arm-linux-gnueabihf-gcc-4.7 ` /usr/local/bin/arm-linux-gnueabihf-gcc

     

    Now you can checkout the Kernel code from git

    git clone git://github.com/embest-tech/linux-imx.git -b embest_imx_3.0.35_4.1.0

     

    At this point you can make the changes as described in this thread to activate UART 4 & 5.

     

    Then to configure and compile everything.

    cd linux-imx
    make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- imx6_defconfig
    make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- uImage

     

    If it compiles without errors you find the images under arch/arm/boot

     

    Tell me please if I missed something or you get any errors.

    I´ve written this directly out of my head. So it could be wrong in some point.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • radiatortwo
    radiatortwo over 12 years ago in reply to e14 Contributor

    Here is how I compiled the older RiotBoard Kernel from the git Repo. Everthing done in a Debian Virtual Machine.

    I don´t use the toolchain from the repos. because of that you have to install some essential stuff.

     

    apt-get install git build-essential fakeroot kernel-package u-boot-tools zlib1g-dev libncurses5-dev

     

    To get the gcc compiler with armhf put this line into /etc/apt/sources.list

    deb http://www.emdebian.org/debian/ unstable main

     

    Then type the following commands:

    apt-get update
    apt-get install emdebian-archive-keyring
    apt-get update
    apt-get install gcc-4.7-arm-linux-gnueabihf
    ln -sf `which arm-linux-gnueabihf-gcc-4.7 ` /usr/local/bin/arm-linux-gnueabihf-gcc

     

    Now you can checkout the Kernel code from git

    git clone git://github.com/embest-tech/linux-imx.git -b embest_imx_3.0.35_4.1.0

     

    At this point you can make the changes as described in this thread to activate UART 4 & 5.

     

    Then to configure and compile everything.

    cd linux-imx
    make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- imx6_defconfig
    make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- uImage

     

    If it compiles without errors you find the images under arch/arm/boot

     

    Tell me please if I missed something or you get any errors.

    I´ve written this directly out of my head. So it could be wrong in some point.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to radiatortwo

    Otto, thank you for your instructions. It was very helpful and much appreciated. Much better than using the toolchain. However, the symbolic link didn't work for me (using Debian 7.5 VM) and I had to change it to:

     

    ln -sf arm-linux-gnueabihf-gcc-4.7 /usr/bin/arm-linux-gnueabihf-gcc

     

    Just in case others are having the same problems I did. After that everything worked great, not only for the original kernel but also for selsinork's new u-boot and kernel. (Thank you selsinork!).