RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Ubuntu 14.04
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 23 replies
  • Subscribers 27 subscribers
  • Views 4087 views
  • Users 0 members are here
Related

Ubuntu 14.04

e14 Contributor
e14 Contributor over 12 years ago

How can I install an the actual Ubuntu 14.04 or at least how can i fix the reboot problem at ubuntu 12.04.

Has anybody a finished image available for download, in order to use with the riotboard.?

  • Sign in to reply
  • Cancel

Top Replies

  • radiatortwo
    radiatortwo over 12 years ago in reply to e14 Contributor +1
    Just came home but selsinork did help already. I´m glad it´s working now.
  • e14 Contributor
    e14 Contributor over 12 years ago

    Perhaps post details of your reboot problem and see if someone can help?

     

    The only images that are currently available (here) are the Android and 12.04.  You may be able to install the 12.04 and then upgrade it all the way to 14.04, but I don't know if that would be successful or not.

    If the problem you're having is related to the kernel then it's unlikely an upgrade like this would help anyway as you'll need a specific kernel for this board and there likely isn't one other than the original one in the 12.04 image at this point.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • radiatortwo
    radiatortwo over 12 years ago

    Only alternative right now is compiling the Kernel yourself.

    There is a branch of the original Kernel in which the reboot error is corrected.

     

    I described here how to compile the Kernel.

    Re: Linux : Where is UART's

     

    You then just have to replace the Kernel image file when flashing Ubuntu.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tusharp
    tusharp over 12 years ago

    how can i fix the reboot problem at ubuntu 12.04.

    can you share the boot logs or snapshot of the reboot issue you are facing.

     

    Has anybody a finished image available for download, in order to use with the riotboard.?

    there is a linaro ubuntu 11.10 image available, you can also build it from source

     

    after flashing (Linux) you can update it to get the supported armel packages.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to radiatortwo

    Hallo Mr. Römer sadly copy and paste didn't work at all.

    I always receive following error

    linaro@linaro-ubuntu-desktop:~/linux-imx$ sudo make ARCH=arm CROS_COMPILE=arm-linux-gnueabihf- uImage

    make: arm-fsl-linux-gnueabi-gcc: Command not found

    scripts/kconfig/conf --silentoldconfig Kconfig

    make: arm-fsl-linux-gnueabi-gcc: Command not found

      CHK     include/linux/version.h

      CHK     include/generated/utsrelease.h

    make[1]: `include/generated/mach-types.h' is up to date.

      CC      kernel/bounds.s

    /bin/sh: 1: arm-fsl-linux-gnueabi-gcc: not found

    make[1]: *** [kernel/bounds.s] Error 127

    make: *** [prepare0] Error 2

    linaro@linaro-ubuntu-desktop:~/linux-imx$

     

     

    I tried to do i tby manual and replaced u-boot and linux to embest_imx_3.0.35_4.1.0. and also downloaded the compiler from toochain.

    Make u-boot worked fine, but creating kernel image delivered still the same error.

    I tried on ubuntu 11. now on 12.11 but still the same problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • radiatortwo
    radiatortwo over 12 years ago in reply to e14 Contributor

    I have a typo in the text it´s not "CROS_COMPILE=..." it´s "CROSS_COMPILE=...".

    Sorry for that.

    I´ll correct it in that post.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to radiatortwo

    Yes I've seen.

    But this didn't solve.

    May you could dd your RIoTboard, so I'd be able to place it on mine? or to replace the existing Linux and burn with the mergetool.

    I am gonna to use it in commercial way. Have already running 10 Pi's successfully with gsm and RS485 transmission since a year (a little workaround with GPIO, reboot..) and they still work.

    But want to get more stable, for example without sd card. But actually it's sad to provide an old version on the official website.,

    which can't once reboot or shutdown.

    So please hurry up:). RioTBoardTeam.

     

    P.S in the Usermanual is described make mx6solo_riot_config,

    but the boards name has been changed. I just not remember how. Pls.correct.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • radiatortwo
    radiatortwo over 12 years ago in reply to e14 Contributor

    If you can wait some more:
    Selsinork is going to post a description on how to compile the newest mainline kernel.

    What I described to compile is a rather old Kernel 3.0.35.

    He already posted the description of compiling and using the mainline u-boot yesterday.

     

    I will then also compile and test the new Kernel. I could also provide some space for an image on my server.

    I can´t provide an image myself. Just because it would take mo too damn long to upload it...

    I have a really slow connection.

    If someone wants to upload it I could give a ftp account for that.

     

    What I can do is to provide the Kernel Image file itself. I made no changes in the kernel code and I only tested it with a minimal debian rootfs so far.

    But it should work with an Ubuntu rootfs I think.

     

    I can upload it as soon as I´m back from work, because it´s on my notebook and I don´t have it with me right now. This will take a few hours from now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • radiatortwo
    radiatortwo over 12 years ago in reply to radiatortwo

    Here is the Kernel Image in which the reboot should be fixed.
    Just replace your old image with this one.

     

    Like I said.

    Only tested with Debian rootfs.

    Attachments:
    uImage3.0.35_4.1.0.working.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to radiatortwo

    Hallo Herr Römlich,

    i replaced the file in the boot directory?

    uname -a shows

    Linux linaro-ubuntu-desktop 3.0.35-02871-ga35ffe3 #1 SMP PREEMPT Wed Oct 30 15:27:47 CST 2013 armv7l armv7l armv7l GNU/Linux

     

    is this now the updated version?

    Reboot still don't work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    It appears that Ottos working version is Linux-3.0.35-03023-ga0660f4

     

    Unfortunately, the file in the boot directory is never used.

    Assuming you're using the MFG_Tool, you'd need to replace the uimage in the correct subdirectory and reflash completely. (I don't have a windows machine, so really can't help with MFG_Tool)

     

    The reason it doesn't use the file in the boot directory can be found in the embedded script in u-boot which does this:

     

    bootdelay=3
    baudrate=115200
    ipaddr=192.168.1.103
    serverip=192.168.1.101
    netmask=255.255.255.0
    loadaddr=0x10800000
    rd_loadaddr=(0x10800000 + 0x300000)
    netdev=eth0
    ethprime=FEC0
    uboot=u-boot.bin
    kernel=uImage
    nfsroot=/opt/eldk/arm
    bootargs=console=ttymxc1,115200 nosmp video=mxcfb0:dev=hdmi,1280x720M@60,bpp=32 video=mxcfb1:off
    bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp
    bootcmd_net=run bootargs_nfs; tftpboot ${loadaddr} ${kernel}; bootm
    bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait
    bootcmd_mmc=run bootargs_mmc; mmc dev 3; mmc read ${loadaddr} 0x800 0x2000; bootm
    bootcmd=run bootcmd_mmc

    the bit in bold is what loads the kernel and what it's doing is reading raw data directly from the mmc card starting at  1,048,576 bytes into the card, and a length of 4,194,304 bytes.

     

    Theoretically you could use dd to write the new uimage to the card in the correct location with something like:

    dd if=/boot/uImage of=/dev/mmcblk0 bs=1M seek=1

    However, I've never done that and can't guarantee it'll work, so you should be prepared to have to reflash using the MFG_Tool

     

    Note that there's an implicit problem with the u-boot setup that's being used - if you recompile a kernel and it ends up being bigger than 4MB then it won't be able to boot since u-boot will only partially load the kernel image.  I'm sure it's obvious why the way this is currently being done is a bad idea.  The worst part is that there's no need to do this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>