RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum A newcomer asks about Riotboard HDMI...
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 51 replies
  • Subscribers 26 subscribers
  • Views 6333 views
  • Users 0 members are here
  • hdmi
  • riotboard
  • tablet
Related

A newcomer asks about Riotboard HDMI...

mubase
mubase over 12 years ago

Hi all. My name is Steve. I am from London. I am a newbie to the Forum. image

I found out yesterday about the Riotboard through an email from Farnell. I was so turned on I bought one today. I am not an experienced Android programmer but have experience with Processing for Android, Arduino, AVR ATMEGA and XMEGA. I haven't got my board yet but thought I'd ask about HDMI.

I have a couple of Android tablets with HDMI sockets.

One is a PIPO M9 and the other a CnM 9" tablet.

Is it possible to connect the Riotboard to a tablet screen using the HDMI sockets?

Or does it have to be a monitor?

  • Sign in to reply
  • Cancel

Top Replies

  • mubase
    mubase over 12 years ago in reply to e14 Contributor +1
    Hi selsinork. Hmmm. Nice but a bit out of my price range ATM. ;s.
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to mubase +1
    seems like that should work, although I'm always slightly skeptical of things like that on ebay serial console is fairly simple to get going, worry more that the post office won't deliver it
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to mubase +1
    steven scutt wrote: OK. The time and date on my board was set to 1970... I kept getting a message during the compile about some process or other being in 2012... Ah yes... various things stupidly…
Parents
  • mubase
    mubase over 12 years ago

    Hello . image

     

    Well I got the HDMI to VGA cable today. (As mentioned above..)

    Plugged it into the HDMI connector of the board and plugged a dell LCD monitor into the VGA end of the adapter...

    Turned on the board and!!!!!

    NOTHING!!!

    I also tried plugging it into my laptop VGA socket. The laptop screen border changes but TIA... hmmm....

    Anyone have any ideas or experience of what I can do?

    (apart from spending hundreds of punds on something I don't have the moolah for at the moment...?)

     

    Cheers,

    Steve.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tusharp
    tusharp over 12 years ago in reply to mubase
    plugged a dell LCD monitor into the VGA end of the adapter

    HDMI interfaces are highly supported but with vga connectors may not work.

    apart from spending hundreds of pounds ...

    serial console is nice and good if there is no display specfic work.

    I mentioned the software setup here and hardware connection here.

     

    Hope that helps for the moment.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • radiatortwo
    radiatortwo over 12 years ago in reply to mubase

    Yes same thing.

     

    But instead you´ll need the Android Image and Tools.

    http://downloads.element14.com/riotboard/Android/Android%20Image.zip?ICID=knode-riotboard-quick&COM=RIoTboard

    http://downloads.element14.com/riotboard/Android/tools.zip?ICID=knode-riotboard-quick&COM=RIoTboard

     

    Maybe only the tools. If I remember right there was already an Image inside the zip.

    You´ll have to look in the folder "Mfgtools-Rel-4.1.0_130816_MX6DL_UPDATER\Profiles\MX6DL Linux Update\OS Firmware\files\android"

     

    If theres an boot.img, recovery.img, system.img and u-boot-mx6solo-riot.bin, then you already have all the files needed.

    But also here you have to rename the ucl2.txt to ucl2.xml.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to mubase

    There's a possible alternative - if you have another linux machine to work from.

    I detailed here

    http://www.element14.com/community/community/knode/single-board_computers/riotboard/blog/2014/05/16/riotboard-ubuntu-image-on-sd-card

    how to put the ubuntu image onto an SD card. Doing that would mean you don't have to wipe android and replace it with linux on the eMMC. You can just change the boot switches to boot from SD and boot linux.

    Unfortunately, you really do need a linux machine to be able to setup the card.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • radiatortwo
    radiatortwo over 12 years ago in reply to e14 Contributor

    Didn´t think of that.

    If there is already something done in Android that´s a good idea.

     

    A virtual machine with Linux wouldn´t work, because you´d need direct access to the SD-Card through the reader.

    My choice would be a live Linux system from CD/DVD/USB. Or a RIoTBoard with Linux and its SDCard slot.image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mubase
    mubase over 12 years ago in reply to mubase

    OK! I've manaed to flash the image onto the board.

     

    Using terminal again I get a scrawl of bootup data. A couple of things I am concerned about.

     

    Should one of the LEDs be flashing? (the one nearest the power jack)..

     

    I get this message...

     

    modprobe: FATAL: Could not load /lib/modules/3.0.35-02871-ga35ffe3/modules.dep: No such file or directory

     

    Anyone know What it means?

    Also this:

    ERROR: HDMI is not ready!

    asoc: can't open platform imx-hdmi-soc-audio.0

     

    So now I have "root@linaro-ubuntu-desktop:~#"

    Where can I go from here?

    Can I install Python? Or how do I go about starting the exciting journey of programming on the Riotboard??

    (I did say I was a noob with some Android, Arduino & Microcontroller experience.. image  )

     

    Cheers,

    Steve.

     

    oh, p.s. did I tell you I was interested in mainly Audio, synthesis and control..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • radiatortwo
    radiatortwo over 12 years ago in reply to mubase

    That modprobe error means that the modules.dep file is missing.

    That´s only a problem if you want to use some external hardware like USB-Wifi or similar.

    The Linux Image isn´t the best and is rather old. That´s why selsinork put that much effort into creating patches for the mainline Kernel.

     

    The HDMI Error is something I also get, when I don´t have a HDMI device connected. So I assume the HDMI to VGA adapter isn´t recognized.

     

    When you´re on the console you´re now able to do everything you could do in ubuntu Linux. (Except start the GUI because you don´t have a picture...)

     

    If you want to install python you could go like this.

    (This is for python 3.3 for example)

     

    sudo apt-get build-dep python3.2
    sudo apt-get install build-essential libreadline-dev libncurses5-dev libssl1.0.0 tk8.5-dev zlib1g-dev liblzma-dev
    
    wget http://python.org/ftp/python/3.3.0/Python-3.3.0.tgz
    
    tar xvfz Python-3.3.0.tgz
    
    cd Python-3.3.0
    ./configure --prefix=/opt/python3.3
    make  
    sudo make install

     

    And to test if it´s really installed

     

    /opt/python3.3/bin/python3

     

    After that you can google for python tutorials. There is a lot of stuff for this.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mubase
    mubase over 12 years ago in reply to radiatortwo

    I've just found out that Python 2.7 is installed already! image  (i typed python and it started..)

    There seems to be a heap of stuff in the distribution which I will thouroughly enjoy looking through...image

    Just one more tiny tiiiiny question???  image

    Is it possible the peripherals (GPIO, USART, Audio etc...) can be programmed using Python?? Ir even a C/C++ extension?? Or will I have to write them ?? 

     

     

    I haven't had any luck with the HDMI. After some digging around I found out about there existing a problem with the R-pi and HDMI to VGA converters due to there not being enough current..:   

    http://creativityslashdesign.blogspot.it/2013/06/hdmi-current-booster-for-raspberrypi-by.html

    is it possible it could be this??

    If not I'll just have to get a monitor or save up for the LVDS monitor selsinork & tusharp suggested.

     

    Thanks again again. I owe you guys a few pints.

    Cheers,

    Steve.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • radiatortwo
    radiatortwo over 12 years ago in reply to mubase

    I can´t tell you much about the GPIO ports. I´m more of a software guy and don´t use them.

    I don´t think that there´s already a python class or similar for this.

     

    Here´s been a discussion about them. Don´t know if it´ll help you though.

    GPIO Ports on RIoT Board

     

    The HDMI problem could be because of the current. That´s why I suggested a converter with external power supply.

    But no guarantee that it´s then working. I don´t have VGA devices anymore and couldn´t even test it...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to radiatortwo

    Depends on the VM, some will let you do passthrough for a particular usb device.. So a usb SD card reader could be used.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to mubase

    GPIO can, theoretically, be programmed using any language you like. /sys/class/gpio being the starting point. However some folks had problems with that on the ubuntu image early on.  There's a thread around here somewhere where I tried to show how to decipher the gpios, but unfortunately used the addresses from the i.MX6 Quad instead of the Solo. The method works, you just need to use the right datasheet.

    Unfortunately the setup in the default 3.0.35 kernel appears to be less than useful for using gpio.

    Hopefully I'll get time to do another blog post or two soon that will finish off setting up Debian, at which point things like gpios basically just work on the 3.15-rc* kernel. Even so, you will need some sort of linux machine in order to build all the pieces. Ideally I'll try to produce an image that can be easily written to an SD card so that people who don't have the confidence to do it themselves can just write the image and go..  Right now I don't have anywhere to host a large image, so how to make it available is still a problem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to mubase

    ERROR: HDMI is not ready!

    doesn't sound particularly good.

     

    asoc: can't open platform imx-hdmi-soc-audio.0

    don't think I'd worry too much about that... native HDMI can do audio as part of the stream to something like an HDTV. but a DVI monitor doesn't do audio while the video format is essentially identical. So you're likely seeing a message that indicates the driver can't detect that the connected device has audio capabilities - which is probably ok for an HDMI-VGA converter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to mubase

    ERROR: HDMI is not ready!

    doesn't sound particularly good.

     

    asoc: can't open platform imx-hdmi-soc-audio.0

    don't think I'd worry too much about that... native HDMI can do audio as part of the stream to something like an HDTV. but a DVI monitor doesn't do audio while the video format is essentially identical. So you're likely seeing a message that indicates the driver can't detect that the connected device has audio capabilities - which is probably ok for an HDMI-VGA converter