RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum A newcomer asks about Riotboard HDMI...
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 51 replies
  • Subscribers 26 subscribers
  • Views 6345 views
  • Users 0 members are here
  • hdmi
  • riotboard
  • tablet
Related

A newcomer asks about Riotboard HDMI...

mubase
mubase over 12 years ago

Hi all. My name is Steve. I am from London. I am a newbie to the Forum. image

I found out yesterday about the Riotboard through an email from Farnell. I was so turned on I bought one today. I am not an experienced Android programmer but have experience with Processing for Android, Arduino, AVR ATMEGA and XMEGA. I haven't got my board yet but thought I'd ask about HDMI.

I have a couple of Android tablets with HDMI sockets.

One is a PIPO M9 and the other a CnM 9" tablet.

Is it possible to connect the Riotboard to a tablet screen using the HDMI sockets?

Or does it have to be a monitor?

  • Sign in to reply
  • Cancel

Top Replies

  • mubase
    mubase over 12 years ago in reply to e14 Contributor +1
    Hi selsinork. Hmmm. Nice but a bit out of my price range ATM. ;s.
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to mubase +1
    seems like that should work, although I'm always slightly skeptical of things like that on ebay serial console is fairly simple to get going, worry more that the post office won't deliver it
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to mubase +1
    steven scutt wrote: OK. The time and date on my board was set to 1970... I kept getting a message during the compile about some process or other being in 2012... Ah yes... various things stupidly…
Parents
  • mubase
    mubase over 12 years ago

    Hello . image

     

    Well I got the HDMI to VGA cable today. (As mentioned above..)

    Plugged it into the HDMI connector of the board and plugged a dell LCD monitor into the VGA end of the adapter...

    Turned on the board and!!!!!

    NOTHING!!!

    I also tried plugging it into my laptop VGA socket. The laptop screen border changes but TIA... hmmm....

    Anyone have any ideas or experience of what I can do?

    (apart from spending hundreds of punds on something I don't have the moolah for at the moment...?)

     

    Cheers,

    Steve.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tusharp
    tusharp over 12 years ago in reply to mubase
    plugged a dell LCD monitor into the VGA end of the adapter

    HDMI interfaces are highly supported but with vga connectors may not work.

    apart from spending hundreds of pounds ...

    serial console is nice and good if there is no display specfic work.

    I mentioned the software setup here and hardware connection here.

     

    Hope that helps for the moment.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mubase
    mubase over 12 years ago in reply to radiatortwo

    I'm installing python 3.3.0 as per Otto's instructions above.

    I've got to running "make"

     

    1. sudo apt-get build-dep python3.2 
    2. sudo apt-get install build-essential libreadline-dev libncurses5-dev libssl1.0.0 tk8.5-dev zlib1g-dev liblzma-dev 
    3.  
    4. wget http://python.org/ftp/python/3.3.0/Python-3.3.0.tgz 
    5.  
    6. tar xvfz Python-3.3.0.tgz 
    7.  
    8. cd Python-3.3.0 
    9. ./configure --prefix=/opt/python3.3 
    10. make   


    its been running for about 45 minutes now... should it be taking this long????


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • radiatortwo
    radiatortwo over 12 years ago in reply to mubase

    45 minutes is a bit long...

    What is he showing right now?

     

    By the way you can cancel it with Ctrl + C.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mubase
    mubase over 12 years ago in reply to radiatortwo

    it was going through something like this:

     

    By default, distutils will build C++ extension modules with "g++".

     

     

      If this is not intended, then set CXX on the configure command line.

     

     

     

     

     

     

    checking for -Wl,--no-as-needed... yes

     

     

    checking how to run the C preprocessor... gcc -E

     

     

    checking for grep that handles long lines and -e... /bin/grep

     

     

    checking for egrep... /bin/grep -E

     

     

    checking for ANSI C header files... yes

     

     

    checking for sys/types.h... yes

     

     

    checking for sys/stat.h... yes

     

     

    checking for stdlib.h... yes

     

     

    checking for string.h... yes

     

     

    checking for memory.h... yes

     

     

    checking for strings.h... yes

     

     

    checking for inttypes.h... yes

     

     

    checking for stdint.h... yes

     

     

    checking for unistd.h... yes

     

     

    checking minix/config.h usability... no

     

     

    checking minix/config.h presence... no

     

     

    checking for minix/config.h... no

     

     

    checking whether it is safe to define __EXTENSIONS__... yes

     

     

    checking for --with-suffix...

     

     

    checking for case-insensitive build directory... no

     

     

    checking LIBRARY... libpython$(VERSION)$(ABIFLAGS).a

     

     

    checking LINKCC... $(PURIFY) $(MAINCC)

     

     

    checking for GNU ld... yes

     

     

    checking for inline... inline

     

     

    checking for --enable-shared... no

     

     

    checking for --enable-profiling... no

     

     

    checking LDLIBRARY... libpython$(VERSION)$(ABIFLAGS).a

     

     

    checking for ranlib... ranlib

     

     

    checking for ar... ar

     

     

    checking for readelf... readelf

     

     

    checking for python... found

     

     

    checking for a BSD-compatible install... /usr/bin/install -c

     

     

    checking for a thread-safe mkdir -p... /bin/mkdir -p

     

     

    checking for --with-pydebug... no

     

     

    checking whether gcc accepts and needs -fno-strict-aliasing... no

     

     

    checking if we can turn off gcc unused result warning... yes

     

     

    checking whether gcc supports ParseTuple __format__... no

     

     

    checking whether pthreads are available without options... no

     

     

    checking whether gcc accepts -Kpthread... no

     

     

    checking whether gcc accepts -Kthread... no

     

     

    checking whether gcc accepts -pthread... yes

     

     

    checking whether g++ also accepts flags for thread support... yes

     

     

    checking for ANSI C header files... (cached) yes

     

     

    checking asm/types.h usability... yes

     

     

    checking asm/types.h presence... yes

     

     

    checking for asm/types.h... yes

     

     

    checking conio.h usability... no

     

     

    checking conio.h presence... no

     

     

    checking for conio.h... no

     

     

    checking curses.h usability... yes

     

     

    checking curses.h presence... yes

     

     

    checking for curses.h... yes

     

     

     

    over and over again... I've pressed cntrl c now... ???

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to mubase

    45 minutes is relative....  cross compiling on a fast multi-core x86 machine will go a lot quicker than compiling natively on the RIoT, but it does add other complications to the equation.

     

    A reasonably large part of the delay with doing this stuff natively on the board can be down to the simple fact thes eMMC and SD cards are slow. A USB hard drive of the spinning rust variety can speed things up a lot.

    I build most of my stuff on a Sabre-Lite, or Wandboard, or CubieTruck. The reason is simple, those all have SATA so I'm not limited by slow SD card speeds.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • radiatortwo
    radiatortwo over 12 years ago in reply to e14 Contributor

    Yes but 45 minutes for Python is really long.

    Even on the RaspberryPi that compiles a lot slower than the RIoTBoard it doesn´t take that long.

     

    I´ll install the Image on my RIoTBoard and will look if I can reproduce the problem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mubase
    mubase over 12 years ago in reply to radiatortwo

    OK. The time and date on my board was set to 1970... I kept getting a message during the compile about some process or other being in 2012...

    I've updated the time to now and tried make again,

    now i'm getting stuff like this:

    gcc -pthread -c -Wno-unused-result -DNDEBUG -g -fwrapv -O3 -Wall -Wstrict-prototypes    -I. -I./Include    -DPy_BUILD_CORE -o Objects/bytearrayobject.o Objects/bytearrayobject.c

     

    which looks more promising,,,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tusharp
    tusharp over 12 years ago in reply to mubase

    its been running for about 45 minutes now... should it be taking this long????

    should take that long, may be it has something to do with the eMMC latency.

    did you try using apt-get, i guess 2.7 based armel packages will be available.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • radiatortwo
    radiatortwo over 12 years ago in reply to mubase

    Yup that´s looking good the compiler actually compiles something now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tusharp
    tusharp over 12 years ago in reply to radiatortwo

    Even i want to give it a try and check if its that slow .

    I am away so can't do it now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tusharp
    tusharp over 12 years ago in reply to mubase

    to keep away the time stuff set your clock to current time using below

    date +%Y%m%d -s "20140526"

    date +T -s "23:55:00"

     

    this will set the clock and hopefully not give any future date warnings  or annoying 1970s stuff.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • tusharp
    tusharp over 12 years ago in reply to mubase

    to keep away the time stuff set your clock to current time using below

    date +%Y%m%d -s "20140526"

    date +T -s "23:55:00"

     

    this will set the clock and hopefully not give any future date warnings  or annoying 1970s stuff.