RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Trying to start: Android + Ubuntu image defect
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 24 subscribers
  • Views 960 views
  • Users 0 members are here
Related

Trying to start: Android + Ubuntu image defect

e14 Contributor
e14 Contributor over 12 years ago

Hey everyone,

 

I just got a Riotboard a few days ago - I really like it's concept - but have some real trouble to get started. First of the preinstalled Android obviously has some problems with my HDMI adapter - my monitor does not have an HDMI input, so I bought an active HDMI->VGA adapter. However, I do not get any screen output - on the serial it says:

error: v4l2 capture: slave not found!

error: HDMI not ready!

 

Then I tried to flash the Linux image... But once again I ran into an error (disregarding the fact that to flash I can't use my Mac but need to use a Windows machine) as obviously the .tgz file in the Linux image is incorrect (I cannot extract it - something along tar magic number error).

 

I then thought of compiling Android 4.2.2 by myself and flashing it. As it turned out, the manifest file for Android 4.2.2 obviously has an error and I cannot continue. Now I try to compile Android 4.3 and see if that does change anything (I'm afraid it won't).

 

So... Is anyone able to provide working images or some other kind of help, please? I _really_ want to get started and experiment with the board but I do not know how image

 

Thanks for your efforts and best regards

Michael Rose

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    So today I got my HDMI-VGA adapter with external power-source and - It works image Well at least the screen image

     

    I flashed the original Android 4.3 image, plugged in my mouse... but my mouse does not behave as expected. First, I cannot see the pointer (is that always the case?). If I click and move / drag around anywhere - nothing happens. However, the scroll wheel seems to be working as it switches between the time display and the "add widget" thingy in the lock screen. Any tips on that?

     

    Edit: Probably a bad mouse - used my Logitech mouse (which has a little wireless connector) and that one worked like a charm! Now it's time to start playing - Thanks for all your help!

     

    Regards

    Michael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago

    So today I got my HDMI-VGA adapter with external power-source and - It works image Well at least the screen image

     

    I flashed the original Android 4.3 image, plugged in my mouse... but my mouse does not behave as expected. First, I cannot see the pointer (is that always the case?). If I click and move / drag around anywhere - nothing happens. However, the scroll wheel seems to be working as it switches between the time display and the "add widget" thingy in the lock screen. Any tips on that?

     

    Edit: Probably a bad mouse - used my Logitech mouse (which has a little wireless connector) and that one worked like a charm! Now it's time to start playing - Thanks for all your help!

     

    Regards

    Michael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • tusharp
    tusharp over 12 years ago in reply to e14 Contributor

    so you were able to set it up on mac image , great going.