RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum To everyone visiting this site
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 17 replies
  • Subscribers 29 subscribers
  • Views 2029 views
  • Users 0 members are here
Related

To everyone visiting this site

radiatortwo
radiatortwo over 12 years ago

I figured that here are always the same questions asked.

Since downloads are still down at this time and all the information is scattered all over the place, a lot of people here are having problems on getting the board to run with a Linux system.

 

So I thought I´d write a series of Blog Posts on how to get everything together, for those who want to get the board running with Linux.

 

I know it´s an Android development board. However most people here seem to want to use it with Linux.

Also now there seems to be some focus on yocto.

 

What I would write would be on how to get the mainline stuff running. (Mainline u-boot, kernel and Debian)
Basically what selsinork already did and then was deleted, but with more recent and correct info. (Like the correct git repos for example.)

 

That then would include the following points:

1. Building the bootloader U-Boot

2. Building the Kernel and Device Tree

3. Creating an Debian Root File System

4. Flashing everything on the board with MFGTool in Windows

5. Flashing everything on a SDCard with Linux

 

I have some time next week for this. But I wanted to ask first if that´s really needed.

 

If so then you can also tell me to include stuff I forgot or anything you want to know.

 

Hope I get some feedback on this. If so I will write and post everything during the next week.

  • Sign in to reply
  • Cancel

Top Replies

  • FreescaleTools_and_Software
    FreescaleTools_and_Software over 12 years ago +1
    Hi Otto First of all, thank you for your precious contribution on the community. Thanks to generous users like you, sharing their experience about a solution, other community users can quickly educate…
  • radiatortwo
    radiatortwo over 12 years ago in reply to radiatortwo +1
    Well first 4 parts are out. Last one is coming tomorrow. Since I had the one or other beer in between I hope there are no big mistakes. So if you find some errors please tell me. Linux on the RIoTBoard…
Parents
  • omeier
    omeier over 12 years ago

    Hello,

     

    I work on the RIoT with the ubuntu Image (image_SVN2591_001).

    It works for now, but it has a large footprint. I develop an embedded application that don't use the Desktop (and much more of the Ubuntu configuration).

    -> So I am VERY interested in an Debian or Yocto build that can be easyly customized.

     

    I don't try the to build a Yocto myself since there is no BSP on the Yocto page that supports the I.MX6 or RIoT.

     

    -> Is the sourcecode for the LVDS- and Touchscreen-Driver available?

    I need the LVDS and Touch support und I plan to change the Display-Type in future. So I think I must eventually modify the driver...

     

    Regards,

    Oliver

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • FreescaleTools_and_Software
    FreescaleTools_and_Software over 12 years ago in reply to omeier

    Hi Oliver

    Are you sure that there is no i.MX6 support in the Yocto BSP tool ? The latest Freescale official release should be linux 3.10.

    According to the information that I have, Yocto tool includes i.MX6 support and other i.MX6 board profiles like Wandboard.
    Element14 is currently working to get the RiOT available in the board profiles which have already been precompiled (which means that user will not have to recompile all the kernel when they just change some options which is really time consuming).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • FreescaleTools_and_Software
    FreescaleTools_and_Software over 12 years ago in reply to omeier

    Hi Oliver

    Are you sure that there is no i.MX6 support in the Yocto BSP tool ? The latest Freescale official release should be linux 3.10.

    According to the information that I have, Yocto tool includes i.MX6 support and other i.MX6 board profiles like Wandboard.
    Element14 is currently working to get the RiOT available in the board profiles which have already been precompiled (which means that user will not have to recompile all the kernel when they just change some options which is really time consuming).