RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Ubuntu Linux UART3 issue
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 24 subscribers
  • Views 785 views
  • Users 0 members are here
Related

Ubuntu Linux UART3 issue

omeier
omeier over 11 years ago

The UARTS of the RIoTboard mapped as:

-  /dev/ttymxc0     probably OpenSDA

- /dev/ttymxc1     Debug port

- /dev/ttymxc2     UART3

This was also discussed here: Linux : Where is UART's

 

So it should be possible to use the UART3 from command line with the following commands:

 

 

     configure:   stty -F /dev/ttymxc2 11125

     transmit:     echo Hello World > /dev/ttymxc2  

     receive:      cat /dev/ttymxc2

 

 

I have discovered that UART3 is is not working in the Ubuntu build "image_SVN2591_001".

UART3 seems to accept the data, but there is no signal on the expension port. It seems that UART3 is just not mapped to the expansion port.

This image comes with Kernel 3.0.35-02881-g2ca0807-dirty.

 

Then I made a downgrade to Kernel 3.0.35-02871-ga35ffe3 (image_SVN2487).

-> With the older Kernel UART3 works as expected!

 

Does someone know the difference between the 2 kernels?

Is it possible to get UART3 in Kernel 3.0.35-02881-g2ca0807-dirty to work?

 

 

This is the full kernel-version:

Linux version 3.0.35-02881-g2ca0807-dirty (luofc@embest-tech) (gcc version 4.6.2 20110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) ) #2 SMP PREEMPT Fri Apr 4 10:59:35 CST 2014

 

and

 

Linux version 3.0.35-02871-ga35ffe3 (luofc@embest-tech) (gcc version 4.6.2 20110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20) ) #1 SMP PREEMPT Wed Oct 30 15:27:47 CST 2013

  • Sign in to reply
  • Cancel
Parents
  • tusharp
    tusharp over 11 years ago

    there may be a commit mismatch in the releases.

    let me check ..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • tusharp
    tusharp over 11 years ago

    there may be a commit mismatch in the releases.

    let me check ..