RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum DDR calibraiton
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 24 subscribers
  • Views 638 views
  • Users 0 members are here
Related

DDR calibraiton

tjmerics
tjmerics over 11 years ago

Is the DDRstress tester program for the riot board available?

  • Sign in to reply
  • Cancel
Parents
  • radiatortwo
    radiatortwo over 11 years ago

    Don´t know what it´s for. (RAM Stress test I suppose).

     

    But after a quick glance I think it should be possible with MFGTool to get the board into OTG Mode, then send the binary for iMX6S and then execute the command.
    Only thing I dont know right now is how to get the results. (Maybe copy the output into a file and then copy that onto a partition so you can read it afterwards.)

     

    But I think it would be easier to do this in u-boot I think?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • radiatortwo
    radiatortwo over 11 years ago

    Don´t know what it´s for. (RAM Stress test I suppose).

     

    But after a quick glance I think it should be possible with MFGTool to get the board into OTG Mode, then send the binary for iMX6S and then execute the command.
    Only thing I dont know right now is how to get the results. (Maybe copy the output into a file and then copy that onto a partition so you can read it afterwards.)

     

    But I think it would be easier to do this in u-boot I think?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • tjmerics
    tjmerics over 11 years ago in reply to radiatortwo

    The program not only tests the DDR but is used generate all the calibrations which are used in the DCD for the DDR. The output is dumped to a serial port. The default program uses uart1. This is connected to the K20 for OpenSDA. The console here is uart2. This requires a custom program. I was looking for the version which would have been used to bring up the RiotBoard.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • radiatortwo
    radiatortwo over 11 years ago in reply to tjmerics

    I´ve been looking at the documentation of i.MX6 DDR Stress Tester 1.03 right now.

     

    There in the user guide it says to put the board into serial download mode so it is recognized as a HID Device in Windows.

    And then execute the following command on the console:

    DDR_Stress_Tester.exe  -t  mx6x  -df  mx6x_ddr_script_filename

     

    Didn´t see anything that you´d need a serial port as output. As far as I can tell you can do all the calibration and stress testing right there.

     

    Only thing I don´t see is a script for the RIoTBoard. But there is a reference script for the iMX6Solo.
    Don´t know if it needs changes though.