RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum uSD boot
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 23 subscribers
  • Views 989 views
  • Users 0 members are here
  • riotboard
Related

uSD boot

e14 Contributor
e14 Contributor over 11 years ago

Dear all,

I have flashed SVN3000 image to an SD card. When I boot it from SD connector (J6, bottom) it works perfectly, however, when I boot the riotboard from uSD (J7, top) image stored in eMMC is booted.

I have checked a hundred times the boot switches and it is correct:

                         D1 D2 D3 D4 D5 D6 D7 D8

SD (J6, bottom)    1   0   1    0    0    1    0    1

uSD (J7, top)        1   0   1    0    0    1    1    0

 

could you please give me any advice?

 

Thank you in advance!

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I have found the solution by chance ... after having written my question. This is what I have done, just in case somebody else has the same problem:

    I read somewhere: "if you use a MicroSD, make sure to change boot script to use device 1 instead of 0" and this is what I have done:

    In u-boot I have written:

    > setenv mmcdev 1

    > saveenv

    change the switches, insert the sd in the usd connector and restart.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer