RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum unable to read file boot.scr
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 23 subscribers
  • Views 1692 views
  • Users 0 members are here
  • hdmi
  • riotboard
Related

unable to read file boot.scr

e14 Contributor
e14 Contributor over 10 years ago

Dear all,

I am able to bitbake a core-image-sato with yocto 1.8 for my riotboard and I am able to copy it to an sd card and connect normally with the terminal.

However, I can not make the video output work for the HDMI.

I have tested SVN_3000 image and it works perfectly and I can visualize the graphical environment in my monitor, so that I guess that hardware is ok!

I have modified u-boot by setting:

bootargs=console=ttymxc1,115200 nosmp video=mxcfb0:dev=hdmi,1280x720@60m, bpp=32 video=mxcfb1:off fbmem=10M

as it is in the SVN_3000 image, but unfortunately it does not work.

I don't know what's going on, I just don't know if the error "Unable to read file boot.scr" has something to do with it

 

I am stuck at this for two days now and any feedback is completely welcome.

Thank you very much in advance!

 

U-Boot 2015.04+fslc+g5d9ffd2 (Oct 10 2015 - 04:00:11)

 

CPU:   Freescale i.MX6SOLO rev1.1 996 MHz (running at 792 MHz)

CPU:   Commercial temperature grade (0C to 95C) at 43C

Reset cause: POR

Board: RIoTboard

I2C:   ready

DRAM:  1 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

auto-detected panel HDMI

Display: HDMI (1024x768)

In:    serial

Out:   serial

Err:   serial

Net:   FEC [PRIME]

Error: FEC address not set.

 

Hit any key to stop autoboot:  0

switch to partitions #0, OK

mmc0 is current device

reading boot.scr

** Unable to read file boot.scr **

reading zImage

6219248 bytes read in 338 ms (17.5 MiB/s)

Booting from mmc ...

reading imx6dl-riotboard.dtb

30758 bytes read in 18 ms (1.6 MiB/s)

Kernel image @ 0x12000000 [ 0x000000 - 0x5ee5f0 ]

## Flattened Device Tree blob at 18000000

   Booting using the fdt blob at 0x18000000

   Using Device Tree in place at 18000000, end 1800a825

 

Starting kernel ...

  • Sign in to reply
  • Cancel
  • tusharp
    0 tusharp over 10 years ago

    Hi Alvaro,

     

    do you need support or is it fixed.

     

    reply incase you need help.

     

     

    Tushar