RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum Riotboard doesn't recognize Wi-Pi
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 23 subscribers
  • Views 1369 views
  • Users 0 members are here
  • wi-pi
  • Ubuntu
  • riotboard,
  • wireless_connectivity
Related

Riotboard doesn't recognize Wi-Pi

jorgerito
jorgerito over 8 years ago

Hi, I have a Riotboard with Ubuntu booted from an SD card, I been trying to use a wifi connection with the Wi-Pi module but it doesn't work.

 

 

When I plug it in and run the lsusb command on terminal it shows this:

 

 

Bus 002 Device 008 ID 148f:5370 Ralink Technology, Corp.

 

 

I tried doing some configurations to the file /etc/network/interfaces but it does nothing.

 

 

It would be great if somebody could help me. I'm new on Linux

  • Sign in to reply
  • Cancel
Parents
  • stmorgan
    0 stmorgan over 8 years ago

    You might want to see Tushar Panda's post on this topic:

     

    https://www.element14.com/community/community/designcenter/single-board-computers/riotboard/blog/2015/01/27/setup-mediatek-rt5370-wifi-on-riotboard-ubuntu-platform

     

    The Wi-Fi dongle described in that post uses the same Ralink RT5370 chip/chipset.

     

    Erich Styger's post on using the Wi-Pi with RIoTboard under Android may also be useful if you want to test that Wi-Pi is actually functional:

     

    https://mcuoneclipse.com/2014/07/24/adding-the-wi-pi-wifi-dongle-to-the-riot-android-board/

     

    I found out  a week ago that it is possible for a Wi-Pi to be damaged but still appear to function in some respects.  When using the Wi-Pi as part of an ADS-B receiver, we had a series of very strong thunderstorms pass through the area.  I managed to shut the system's Raspberry Pi 2 MCU down, but only after we had several lightning strikes within a mile/couple of kilometers.  I started the receiver up after the storm, and the Wi-Pi dongle made a connection to the router and was successfully assigned an IP address, but it is apparently damaged in such a way that it will no longer pass data.  If I substitute an identical Wi-Pi in the system and restart it, it works just fine.  So can use an Android RIoTboard image to test that your Wi-Pi dongle is fully functional if you have doubts on that topic.


    Good luck.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • stmorgan
    0 stmorgan over 8 years ago

    You might want to see Tushar Panda's post on this topic:

     

    https://www.element14.com/community/community/designcenter/single-board-computers/riotboard/blog/2015/01/27/setup-mediatek-rt5370-wifi-on-riotboard-ubuntu-platform

     

    The Wi-Fi dongle described in that post uses the same Ralink RT5370 chip/chipset.

     

    Erich Styger's post on using the Wi-Pi with RIoTboard under Android may also be useful if you want to test that Wi-Pi is actually functional:

     

    https://mcuoneclipse.com/2014/07/24/adding-the-wi-pi-wifi-dongle-to-the-riot-android-board/

     

    I found out  a week ago that it is possible for a Wi-Pi to be damaged but still appear to function in some respects.  When using the Wi-Pi as part of an ADS-B receiver, we had a series of very strong thunderstorms pass through the area.  I managed to shut the system's Raspberry Pi 2 MCU down, but only after we had several lightning strikes within a mile/couple of kilometers.  I started the receiver up after the storm, and the Wi-Pi dongle made a connection to the router and was successfully assigned an IP address, but it is apparently damaged in such a way that it will no longer pass data.  If I substitute an identical Wi-Pi in the system and restart it, it works just fine.  So can use an Android RIoTboard image to test that your Wi-Pi dongle is fully functional if you have doubts on that topic.


    Good luck.