RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum How can i flash using Linux?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 32 replies
  • Subscribers 24 subscribers
  • Views 4003 views
  • Users 0 members are here
  • flash
  • linux
Related

How can i flash using Linux?

e14 Contributor
e14 Contributor over 12 years ago

Hi,

 

there is no method described in the manual. I guess many (most?) people interested in an open

hardware development device are using linux.

 

I hope there are any tools available and the documentation can be extended.

 

Thanks

 

Steffen

  • Sign in to reply
  • Cancel

Top Replies

  • vandana
    vandana over 12 years ago in reply to e14 Contributor +2
    We will be uploading the actual gerbers very soon - and it will be truly open source. Based on some of the community feedback, we are also looking into CAD library support with other tools. Thanks
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    community.element14.com/.../contentimage_5F00_176409.html It's on Page 44 of the UM that it mentions that Linux currently only boots from eMMC. Though maybe that means eventually it'll have an SD option…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    anthony_h wrote: It's on Page 44 of the UM that it mentions that Linux currently only boots from eMMC. Unfortunately that's so vague as to be pointless.. From a Linux point of view eMMC and SD are…
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Remember that the RIoT board is targeted specifically for Android development, not mainline linux.

     

    It's also not a truly open hardware design as the actual CAD files are not provided. There are Gerbers available now which allow you to produce an exact copy, but the Mentor/KiCad/Eagle/whatever source files are not available so you can't easily modify it.

    There are better choices if you want an open hardware board, for eaxmple the Olimex OLinuXino boards.

     

    However, the user manual has section 5 on how to build linux kernel images and you'll find a linux download on this page RIoTboard

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Thanks for the reply. You are right - it's maybe not that open.

     

    I have seen the linux image. My problem is, that i don't see a way to upload it to the riotboards eMMc. The mfg tool is not

    running on my linux desktop.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    I don't have a board, but can't you just write it to an SD card and boot from that ?  Assuming the sizes work out it's probably possible to just dd the image to the eMMC afterwards.

     

    There's no real requirement for the mfgtools, but if you're stuck on doing it that way, you can try https://github.com/boundarydevices/imx_usb_loader which is what's used for other i.MX6 boards. I've used it successfully on sabre-lite

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    AFAIK you can only boot Linux from the internal eMMC — not from the external.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    James Carruthers wrote:

     

    AFAIK you can only boot Linux from the internal eMMC — not from the external.

    Where did you get that information ?

    The user manual says otherwise (and other i.MX6 systems can boot from varying places)

    image

    So once you set the boot switches to SD you can boot whatever you like from SD.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Fullscreen contentimage_176409.html Download
    <html><head><title>Jive SBS</title></head>
    <body><font face="arial,helvetica,sans-serif">
    <b>Error</b><br><font size="-1">
    An general error occurred while processing your request.
    </font></font></body></html>
    

     

    It's on Page 44 of the UM that it mentions that Linux currently only boots from eMMC. Though maybe that means eventually it'll have an SD option. As you stated, the chip can boot from either interface, so it seems to be a software configuration thing for Linux.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    anthony_h wrote:

     

    It's on Page 44 of the UM that it mentions that Linux currently only boots from eMMC.

    Unfortunately that's so vague as to be pointless..  From a Linux point of view eMMC and SD are identical as they use the same driver. If u-boot can load android from eMMC there's no reason to believe it can't load Linux - since android is based on a linux kernel.

    The wording seems strange too "Currently the Linux system on the RIoTboard supports only booting from the eMMC" but as we all know it arrives with Android installed, so 'currently' there is no linux on the board... If there was, it wouldn't be an issue image

     

    I'm wondering if what it really means is that the ancient 3.0.35 based image from the download page is brain-damaged enough that it's incapable of doing so.  In a different thread there's a devicetree file for the 3.13 kernel which should effectively remove any kernel based obstacles. The only remaining problem would be if u-boot or the ubuntu image have hard-coded something and any of those should be fixable.

     

    It's a pity there's no SPI rom like the Sabre-Lite. A decent version of u-boot in SPI essentially makes it possible to easily boot from anywhere.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    anthony_h wrote:

     

    It's on Page 44 of the UM that it mentions that Linux currently only boots from eMMC.

    Unfortunately that's so vague as to be pointless..  From a Linux point of view eMMC and SD are identical as they use the same driver. If u-boot can load android from eMMC there's no reason to believe it can't load Linux - since android is based on a linux kernel.

    The wording seems strange too "Currently the Linux system on the RIoTboard supports only booting from the eMMC" but as we all know it arrives with Android installed, so 'currently' there is no linux on the board... If there was, it wouldn't be an issue image

     

    I'm wondering if what it really means is that the ancient 3.0.35 based image from the download page is brain-damaged enough that it's incapable of doing so.  In a different thread there's a devicetree file for the 3.13 kernel which should effectively remove any kernel based obstacles. The only remaining problem would be if u-boot or the ubuntu image have hard-coded something and any of those should be fixable.

     

    It's a pity there's no SPI rom like the Sabre-Lite. A decent version of u-boot in SPI essentially makes it possible to easily boot from anywhere.