RIoTboard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum How can i create an image of my linux configuration and flash it into emcc
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 24 subscribers
  • Views 3818 views
  • Users 0 members are here
Related

How can i create an image of my linux configuration and flash it into emcc

e14 Contributor
e14 Contributor over 12 years ago

I want to copy the same configuration on more riotboards. How can i handle this with the emcc-flash not the sd-card?.

  • Sign in to reply
  • Cancel
Parents
  • tusharp
    0 tusharp over 12 years ago

    just for records:

     

    block size can be determined using below command

    blockdev --getbsz /dev/mmcblk1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tusharp
    0 tusharp over 12 years ago

    just for records:

     

    block size can be determined using below command

    blockdev --getbsz /dev/mmcblk1

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jiapei100
    0 jiapei100 over 5 years ago in reply to tusharp

    In my case:

     

    ➜  ~ df -h

    Filesystem      Size  Used Avail Use% Mounted on

    /dev/mmcblk0p1   28G   18G  8.8G  67% /

    none             16G     0   16G   0% /dev

    tmpfs            16G   88K   16G   1% /dev/shm

    tmpfs            16G   31M   16G   1% /run

    tmpfs           5.0M  4.0K  5.0M   1% /run/lock

    tmpfs            16G     0   16G   0% /sys/fs/cgroup

    tmpfs           3.2G   12K  3.2G   1% /run/user/120

    tmpfs           3.2G  116K  3.2G   1% /run/user/1000

    /dev/mmcblk1p1   29G   29G     0 100% /media/lvision/AGX-SD

     

     

    And I got the following No space left on device ERROR

     

    ➜  ~ sudo dd bs=1024 if=/dev/mmcblk0 of=/dev/mmcblk1

    [sudo] password for lvision:

    dd: error writing '/dev/mmcblk1': No space left on device

    30318593+0 records in

    30318592+0 records out

    31046238208 bytes (31 GB, 29 GiB) copied, 4605.66 s, 6.7 MB/s

     

    while I tried to dd mmcblk0 which is ONLY used 18G to mmcblk1 which is of 29G size.