RIoTboard
  • Products
  • Dev Tools
  • Single-Board Computers
  • RIoTboard
  • More
  • Cancel
RIoTboard
Forum How to add module usbserial
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join RIoTboard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 24 subscribers
  • Views 1146 views
  • Users 0 members are here
Related

How to add module usbserial

e14 Contributor
e14 Contributor over 12 years ago

I want to attach the mobile-modem Huawei E-169 and an USB-RS485 adapter.

Both devices are listed in lsusb.

but no one will be mounted correctly

The Huawei Modem should be mounted at /dev/ttyUSB*.

dmesg delivers output only mounted as storage.

 

usb 2-1.2: new high speed USB device number 8 using fsl-ehci

scsi7 : usb-storage 2-1.2:1.2

scsi8 : usb-storage 2-1.2:1.3

scsi 7:0:0:0: CD-ROM            HUAWEI   Mass Storage     2.31 PQ: 0 ANSI: 2

scsi 8:0:0:0: Direct-Access     HUAWEI   MMC Storage      2.31 PQ: 0 ANSI: 2

sd 8:0:0:0: [sda] Attached SCSI removable disk

linaro@linaro-ubuntu-desktop:~$

 

I tried to modeswitch the device with modeprobe usbserial with following error.

FATAL: Module usb_serial not found.

 

How can i load module usb_serial?

 

linaro@linaro-ubuntu-desktop:~$ modprobe -l | grep serial

kernel/drivers/usb/gadget/g_serial.ko

already tried to /boot/linux.config

CONFIG_USB_SERIAL=y and

CONFIG_USB_SERIAL=m

 

Working on Ubuntu 12.11

Linux linaro-ubuntu-desktop 3.0.35-03023-ga0660f4 #1 SMP PREEMPT Tue Mar 25 21:17:12 CET 2014 armv7l armv7l armv7l GNU/Linux

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    There appears to be very few modules included in the default image. I don't see the usbserial one.

     

    So you're left with following the instructions radiatortwo posted on recompiling that kernel, but while you're configuring it you can add any missing modules you think you'll need

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    There appears to be very few modules included in the default image. I don't see the usbserial one.

     

    So you're left with following the instructions radiatortwo posted on recompiling that kernel, but while you're configuring it you can add any missing modules you think you'll need